LED
Description
Sample API funtions for controlling LEDs.
When specifying an LED to use, always use the BOARDLEDx definitions that are defined within the BOARD_HEADER.
See led.h for source code.
Functions |
|
| void | halInternalInitLed (void) |
|
Configures GPIOs pertaining to the control of LEDs.
|
|
| void | halToggleLed ( HalBoardLed led) |
|
Atomically wraps an XOR or similar operation for a single GPIO pin attached to an LED.
|
|
| void | halSetLed ( HalBoardLed led) |
|
Turns on (sets) a GPIO pin connected to an LED so that the LED turns on.
|
|
| void | halClearLed ( HalBoardLed led) |
|
Turns off (clears) a GPIO pin connected to an LED, which turns off the LED.
|
|
| void | halStackIndicateActivity (bool turnOn) |
|
Called by the stack to indicate activity over the radio (for both transmission and reception).
|
|
Typedefs |
|
| typedef enum HalBoardLedPins | HalBoardLed |
|
Ensures that the definitions from the BOARD_HEADER are always used as parameters to the LED functions.
|
|
Function Documentation
◆ halInternalInitLed()
| void halInternalInitLed | ( | void |
|
) |
Configures GPIOs pertaining to the control of LEDs.
◆ halToggleLed()
| void halToggleLed | ( | HalBoardLed |
led
|
) |
Atomically wraps an XOR or similar operation for a single GPIO pin attached to an LED.
- Parameters
-
ledIdentifier (from BOARD_HEADER) for the LED to be toggled.
◆ halSetLed()
| void halSetLed | ( | HalBoardLed |
led
|
) |
Turns on (sets) a GPIO pin connected to an LED so that the LED turns on.
- Parameters
-
ledIdentifier (from BOARD_HEADER) for the LED to turn on.
◆ halClearLed()
| void halClearLed | ( | HalBoardLed |
led
|
) |
Turns off (clears) a GPIO pin connected to an LED, which turns off the LED.
- Parameters
-
ledIdentifier (from BOARD_HEADER) for the LED to turn off.
◆ halStackIndicateActivity()
| void halStackIndicateActivity | ( | bool |
turnOn
|
) |
Called by the stack to indicate activity over the radio (for both transmission and reception).
It is called once with
turnOn
true and shortly thereafter with
turnOn
false.
Typically does something interesting, such as change the state of an LED.
- Parameters
-
turnOnSee Usage.
Typedef Documentation
◆ HalBoardLed
| typedef enum HalBoardLedPins HalBoardLed |
Ensures that the definitions from the BOARD_HEADER are always used as parameters to the LED functions.