CLI Commands in RAM
Description
Support for CLI commands stored in and executed from RAM.
Data Structures |
|
| struct | cli_storage_ram_t |
|
Struct representing an instance of the CLI storage RAM.
|
|
Functions |
|
| void | sl_cli_storage_ram_clear ( sl_cli_command_arg_t *arguments) |
|
Clear the command lines stored in ram.
|
|
| void | sl_cli_storage_ram_list ( sl_cli_command_arg_t *arguments) |
|
Print the contet of the command lines stored in ram.
|
|
| void | sl_cli_storage_ram_define ( sl_cli_command_arg_t *arguments) |
|
Start defining new command lines that will be stored in ram.
|
|
| void | sl_cli_storage_ram_execute ( sl_cli_command_arg_t *arguments) |
|
Execute command lines stored in ram.
|
|
| size_t | sl_cli_storage_ram_count (sl_cli_handle_t cli_handle) |
|
Get the number of command lines stored in ram.
|
|
| void | sl_cli_storage_ram_init ( cli_storage_ram_handle_t handle) |
|
Initialize the cli_storage_ram instance.
|
|
Typedefs |
|
| typedef cli_storage_ram_t * | cli_storage_ram_handle_t |
|
Definition of the CLI storage RAM handle.
|
|
Function Documentation
◆ sl_cli_storage_ram_clear()
| void sl_cli_storage_ram_clear | ( | sl_cli_command_arg_t * |
arguments
|
) |
Clear the command lines stored in ram.
This function can be used directly as a cli command handler.
- Parameters
-
[in] argumentsA pointer to the command arguments.
◆ sl_cli_storage_ram_list()
| void sl_cli_storage_ram_list | ( | sl_cli_command_arg_t * |
arguments
|
) |
Print the contet of the command lines stored in ram.
This function can be used directly as a cli command handler.
- Parameters
-
[in] argumentsA pointer to the command arguments.
◆ sl_cli_storage_ram_define()
| void sl_cli_storage_ram_define | ( | sl_cli_command_arg_t * |
arguments
|
) |
Start defining new command lines that will be stored in ram.
This function can be used directly as a cli command handler.
- Parameters
-
[in] argumentsA pointer to the command arguments.
◆ sl_cli_storage_ram_execute()
| void sl_cli_storage_ram_execute | ( | sl_cli_command_arg_t * |
arguments
|
) |
Execute command lines stored in ram.
This function can be used directly as a cli command handler.
- Note
- The function has a different implementation in a bare-metal vs. kernel configurations. In a bare-metal configuration, this function will signal that stored commands shall be run by the sl_cli_storage_ram_tick function. One stored command is executed for each call to the sl_cli_storage_ram_tick function. In a kernel configuration, all stored commands will be executed before this function returns.
- Parameters
-
[in] argumentsA pointer to the command arguments.
◆ sl_cli_storage_ram_count()
| size_t sl_cli_storage_ram_count | ( | sl_cli_handle_t |
cli_handle
|
) |
Get the number of command lines stored in ram.
- Parameters
-
[in] cli_handleHandle to the CLI where the cli_storage_ram component is connected.
- Returns
- The number of command lines stored in ram.
◆ sl_cli_storage_ram_init()
| void sl_cli_storage_ram_init | ( | cli_storage_ram_handle_t |
handle
|
) |
Initialize the cli_storage_ram instance.
- Parameters
-
[in] handleA handle to the cli_storage_ram instance.
Typedef Documentation
◆ cli_storage_ram_handle_t
| typedef cli_storage_ram_t * cli_storage_ram_handle_t |
Definition of the CLI storage RAM handle.