sl_se_command_context_t Struct Reference
SE mailbox command context.
#include <sl_se_manager_types.h>
Data Fields |
|
| SE_Command_t | command |
|
SE mailbox command struct.
|
|
| bool | yield |
|
If true, yield the CPU core while waiting for the SE mailbox command to complete.
|
|
SE mailbox command context.
This structure defines the common SE mailbox command context used for all SE Manager API functions that execute SE mailbox commands. The members of this context structure should be considered internal to the SE Manager and should not be read or written directly by the user application. For members that are relevant for the user, the user can access them via corresponding set and get API functions, e.g. sl_se_set_yield() .
Field Documentation
◆ command
| SE_Command_t sl_se_command_context_t::command |
SE mailbox command struct.
◆ yield
| bool sl_se_command_context_t::yield |
If true, yield the CPU core while waiting for the SE mailbox command to complete.
If false, busy-wait, by polling the SE mailbox response register.