CAN_Init_TypeDef Struct Reference
CAN initialization structure.
#include <em_can.h>
Data Fields |
|
| bool | enable |
|
True to set the CAN Device in normal mode after initialization.
|
|
| bool | resetMessages |
|
True to reset messages during initialization.
|
|
| uint32_t | bitrate |
|
Default bitrate.
|
|
| uint8_t | propagationTimeSegment |
|
Default Propagation Time Segment.
|
|
| uint8_t | phaseBufferSegment1 |
|
Default Phase Buffer Segment 1.
|
|
| uint8_t | phaseBufferSegment2 |
|
Default Phase Buffer Segment 2.
|
|
| uint8_t | synchronisationJumpWidth |
|
Default Synchronisation Jump Width.
|
|
CAN initialization structure.
Field Documentation
◆ enable
| bool CAN_Init_TypeDef::enable |
True to set the CAN Device in normal mode after initialization.
◆ resetMessages
| bool CAN_Init_TypeDef::resetMessages |
True to reset messages during initialization.
◆ bitrate
| uint32_t CAN_Init_TypeDef::bitrate |
Default bitrate.
◆ propagationTimeSegment
| uint8_t CAN_Init_TypeDef::propagationTimeSegment |
Default Propagation Time Segment.
◆ phaseBufferSegment1
| uint8_t CAN_Init_TypeDef::phaseBufferSegment1 |
Default Phase Buffer Segment 1.
◆ phaseBufferSegment2
| uint8_t CAN_Init_TypeDef::phaseBufferSegment2 |
Default Phase Buffer Segment 2.
◆ synchronisationJumpWidth
| uint8_t CAN_Init_TypeDef::synchronisationJumpWidth |
Default Synchronisation Jump Width.