SMU - Security Management Unit

Description

Security Management Unit (SMU) Peripheral API.

SMU forms the control and status/reporting component of bus-level security in EFM32/EFR32 devices.

Peripheral-level protection is provided via the peripheral protection unit (PPU). PPU provides hardware access barrier to any peripheral that is configured to be protected. When an attempt is made to access a peripheral without the required privilege/security level, PPU detects the fault and intercepts the access. No write or read of the peripheral register space occurs, and an all-zero value is returned if the access is a read.

Usage example

// SMU is always clocked, so no call to CMU_ClockEnable() is necessary
// Initialize SMU to prevent access to CMU, EMU, SMU and GPIO
SMU_Init (&init);

Data Structures

struct SMU_PrivilegedAccess_TypeDef
SMU peripheral privileged access enablers.
struct SMU_Init_TypeDef
SMU initialization structure.

Functions

void SMU_EnablePPU (bool enable)
Enable or disable PPU of SMU.
void SMU_Init (const SMU_Init_TypeDef *init)
Initialize PPU of SMU.
void SMU_SetPrivilegedAccess ( SMU_Peripheral_TypeDef peripheral, bool privileged)
Change access settings for a peripheral.
SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral (void)
Get ID of the peripheral that caused an access fault.
void SMU_IntClear (uint32_t flags)
Clear one or more pending SMU interrupts.
void SMU_IntDisable (uint32_t flags)
Disable one or more SMU interrupts.
void SMU_IntEnable (uint32_t flags)
Enable one or more SMU interrupts.
uint32_t SMU_IntGet (void)
Get pending SMU interrupts.
uint32_t SMU_IntGetEnabled (void)
Get enabled and pending SMU interrupt flags.
void SMU_IntSet (uint32_t flags)
Set one or more pending SMU interrupts from SW.

Macros

#define SMU_INIT_DEFAULT
Default SMU initialization structure settings.

Enumerations

enum SMU_Peripheral_TypeDef {
smuPeripheralACMP0 = _SMU_PPUPATD0_ACMP0_SHIFT,
smuPeripheralACMP1 = _SMU_PPUPATD0_ACMP1_SHIFT,
smuPeripheralADC0 = _SMU_PPUPATD0_ADC0_SHIFT,
smuPeripheralCMU = _SMU_PPUPATD0_CMU_SHIFT,
smuPeripheralCRYOTIMER = _SMU_PPUPATD0_CRYOTIMER_SHIFT,
smuPeripheralCRYPTO0 = _SMU_PPUPATD0_CRYPTO0_SHIFT,
smuPeripheralCRYPTO1 = _SMU_PPUPATD0_CRYPTO1_SHIFT,
smuPeripheralCSEN = _SMU_PPUPATD0_CSEN_SHIFT,
smuPeripheralVDAC0 = _SMU_PPUPATD0_VDAC0_SHIFT,
smuPeripheralPRS = _SMU_PPUPATD0_PRS_SHIFT,
smuPeripheralEMU = _SMU_PPUPATD0_EMU_SHIFT,
smuPeripheralFPUEH = _SMU_PPUPATD0_FPUEH_SHIFT,
smuPeripheralGPCRC = _SMU_PPUPATD0_GPCRC_SHIFT,
smuPeripheralGPIO = _SMU_PPUPATD0_GPIO_SHIFT,
smuPeripheralI2C0 = _SMU_PPUPATD0_I2C0_SHIFT,
smuPeripheralI2C1 = _SMU_PPUPATD0_I2C1_SHIFT,
smuPeripheralIDAC0 = _SMU_PPUPATD0_IDAC0_SHIFT,
smuPeripheralMSC = _SMU_PPUPATD0_MSC_SHIFT,
smuPeripheralLDMA = _SMU_PPUPATD0_LDMA_SHIFT,
smuPeripheralLESENSE = _SMU_PPUPATD0_LESENSE_SHIFT,
smuPeripheralLETIMER0 = _SMU_PPUPATD0_LETIMER0_SHIFT,
smuPeripheralLEUART0 = _SMU_PPUPATD0_LEUART0_SHIFT,
smuPeripheralPCNT0 = _SMU_PPUPATD0_PCNT0_SHIFT,
smuPeripheralRMU = 32 + _SMU_PPUPATD1_RMU_SHIFT,
smuPeripheralRTCC = 32 + _SMU_PPUPATD1_RTCC_SHIFT,
smuPeripheralSMU = 32 + _SMU_PPUPATD1_SMU_SHIFT,
smuPeripheralTIMER0 = 32 + _SMU_PPUPATD1_TIMER0_SHIFT,
smuPeripheralTIMER1 = 32 + _SMU_PPUPATD1_TIMER1_SHIFT,
smuPeripheralTRNG0 = 32 + _SMU_PPUPATD1_TRNG0_SHIFT,
smuPeripheralUSART0 = 32 + _SMU_PPUPATD1_USART0_SHIFT,
smuPeripheralUSART1 = 32 + _SMU_PPUPATD1_USART1_SHIFT,
smuPeripheralUSART2 = 32 + _SMU_PPUPATD1_USART2_SHIFT,
smuPeripheralWDOG0 = 32 + _SMU_PPUPATD1_WDOG0_SHIFT,
smuPeripheralWDOG1 = 32 + _SMU_PPUPATD1_WDOG1_SHIFT,
smuPeripheralWTIMER0 = 32 + _SMU_PPUPATD1_WTIMER0_SHIFT,
smuPeripheralEnd
}
SMU peripheral identifiers.

Function Documentation

◆ SMU_EnablePPU()

void SMU_EnablePPU ( bool enable )
inline

Enable or disable PPU of SMU.

Parameters
[in] enable Set to true to enable PPU; set to false otherwise.

◆ SMU_Init()

void SMU_Init ( const SMU_Init_TypeDef * init )
inline

Initialize PPU of SMU.

Parameters
[in] init Pointer to initialization structure that defines which peripherals should only be accessed from privileged mode, and if PPU should be enabled.

◆ SMU_SetPrivilegedAccess()

void SMU_SetPrivilegedAccess ( SMU_Peripheral_TypeDef peripheral,
bool privileged
)
inline

Change access settings for a peripheral.

Set to limit access of a peripheral from privileged mode.

Parameters
[in] peripheral ID of the peripheral to change access settings for.
[in] privileged Set to true if the peripheral should only be accessed from privileged mode; set to false otherwise.

◆ SMU_GetFaultingPeripheral()

SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral ( void )
inline

Get ID of the peripheral that caused an access fault.

Note
The return value is only valid if SMU_IF_PPUPRIV interrupt flag is set.
Returns
ID of the peripheral that caused an access fault.

◆ SMU_IntClear()

void SMU_IntClear ( uint32_t flags )
inline

Clear one or more pending SMU interrupts.

Parameters
[in] flags Bitwise logic OR of SMU interrupt sources to clear.

◆ SMU_IntDisable()

void SMU_IntDisable ( uint32_t flags )
inline

Disable one or more SMU interrupts.

Parameters
[in] flags SMU interrupt sources to disable.

◆ SMU_IntEnable()

void SMU_IntEnable ( uint32_t flags )
inline

Enable one or more SMU interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using SMU_IntClear() prior to enabling the interrupt.
Parameters
[in] flags SMU interrupt sources to enable.

◆ SMU_IntGet()

uint32_t SMU_IntGet ( void )
inline

Get pending SMU interrupts.

Returns
SMU interrupt sources pending.

◆ SMU_IntGetEnabled()

uint32_t SMU_IntGetEnabled ( void )
inline

Get enabled and pending SMU interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
Interrupt flags are not cleared by this function.
Returns
Pending and enabled SMU interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in SMU_IEN register and
  • the OR combination of valid interrupt flags in SMU_IF register.

◆ SMU_IntSet()

void SMU_IntSet ( uint32_t flags )
inline

Set one or more pending SMU interrupts from SW.

Parameters
[in] flags SMU interrupt sources to set to pending.

Macro Definition Documentation

◆ SMU_INIT_DEFAULT

#define SMU_INIT_DEFAULT
Value:
{ \
{ { 0 } }, /* No peripherals access protected. */ \
true /* Enable SMU.*/ \
}

Default SMU initialization structure settings.

Enumeration Type Documentation

◆ SMU_Peripheral_TypeDef

SMU peripheral identifiers.

Enumerator
smuPeripheralACMP0

SMU peripheral identifier for ACMP0.


smuPeripheralACMP1

SMU peripheral identifier for ACMP1.


smuPeripheralADC0

SMU peripheral identifier for ADC0.


smuPeripheralCMU

SMU peripheral identifier for CMU.


smuPeripheralCRYOTIMER

SMU peripheral identifier for CRYOTIMER.

smuPeripheralCRYPTO0

SMU peripheral identifier for CRYPTO0.


smuPeripheralCRYPTO1

SMU peripheral identifier for CRYPTO1.


smuPeripheralCSEN

SMU peripheral identifier for CSEN.


smuPeripheralVDAC0

SMU peripheral identifier for VDAC0.


smuPeripheralPRS

SMU peripheral identifier for PRS.


smuPeripheralEMU

SMU peripheral identifier for EMU.


smuPeripheralFPUEH

SMU peripheral identifier for FPUEH.


smuPeripheralGPCRC

SMU peripheral identifier for GPCRC.


smuPeripheralGPIO

SMU peripheral identifier for GPIO.


smuPeripheralI2C0

SMU peripheral identifier for I2C0.


smuPeripheralI2C1

SMU peripheral identifier for I2C1.


smuPeripheralIDAC0

SMU peripheral identifier for IDAC0.


smuPeripheralMSC

SMU peripheral identifier for MSC.


smuPeripheralLDMA

SMU peripheral identifier for LDMA.


smuPeripheralLESENSE

SMU peripheral identifier for LESENSE.


smuPeripheralLETIMER0

SMU peripheral identifier for LETIMER0.


smuPeripheralLEUART0

SMU peripheral identifier for LEUART0.


smuPeripheralPCNT0

SMU peripheral identifier for PCNT0.


smuPeripheralRMU

SMU peripheral identifier for RMU.


smuPeripheralRTCC

SMU peripheral identifier for RTCC.


smuPeripheralSMU

SMU peripheral identifier for SMU.


smuPeripheralTIMER0

SMU peripheral identifier for TIMER0.


smuPeripheralTIMER1

SMU peripheral identifier for TIMER1.


smuPeripheralTRNG0

SMU peripheral identifier for TRNG0.


smuPeripheralUSART0

SMU peripheral identifier for USART0.


smuPeripheralUSART1

SMU peripheral identifier for USART1.


smuPeripheralUSART2

SMU peripheral identifier for USART2.


smuPeripheralWDOG0

SMU peripheral identifier for WDOG0.


smuPeripheralWDOG1

SMU peripheral identifier for WDOG1.


smuPeripheralWTIMER0

SMU peripheral identifier for WTIMER0.