BURTC - Backup RTC

Description

Backup Real Time Counter (BURTC) Peripheral API.

This module contains functions to control the BURTC peripheral of Silicon Labs 32-bit MCUs. The Backup Real Time Counter allows timekeeping in all energy modes. The Backup RTC is also available when the system is in backup mode.

Data Structures

struct  BURTC_Init_TypeDef
 BURTC initialization structure for Series 2 devices.
 

Functions

void BURTC_IntClear (uint32_t flags)
 Clear one or more pending BURTC interrupts.
 
void BURTC_IntDisable (uint32_t flags)
 Disable one or more BURTC interrupts.
 
void BURTC_IntEnable (uint32_t flags)
 Enable one or more BURTC interrupts.
 
uint32_t BURTC_IntGet (void)
 Get pending BURTC interrupt flags.
 
uint32_t BURTC_IntGetEnabled (void)
 Get enabled and pending BURTC interrupt flags.
 
void BURTC_IntSet (uint32_t flags)
 Set one or more pending BURTC interrupts from SW.
 
uint32_t BURTC_Status (void)
 Status of BURTC RAM, timestamp and LP Mode.
 
void BURTC_SyncWait (void)
 Wait for the BURTC to complete all synchronization of register changes and commands.
 
void BURTC_Start (void)
 Start BURTC counter.
 
void BURTC_Stop (void)
 Stop the BURTC counter.
 
uint32_t BURTC_CounterGet (void)
 Get BURTC counter.
 
void BURTC_Lock (void)
 Lock BURTC registers, will protect from writing new config settings.
 
void BURTC_Unlock (void)
 Unlock BURTC registers, enable write access to change configuration.
 
void BURTC_Reset (void)
 Restore BURTC to reset state.
 
void BURTC_Init (const BURTC_Init_TypeDef *burtcInit)
 Initialize BURTC.
 
void BURTC_Enable (bool enable)
 Enable or Disable BURTC peripheral.
 
void BURTC_CounterReset (void)
 Reset counter.
 
void BURTC_CompareSet (unsigned int comp, uint32_t value)
 Set BURTC compare channel.
 
uint32_t BURTC_CompareGet (unsigned int comp)
 Get the BURTC compare value.
 

Macros

#define burtcClkDiv_1   1
 BURTC clock divisors.
 
#define burtcClkDiv_2   2
 Divide clock by 2.
 
#define burtcClkDiv_4   4
 Divide clock by 4.
 
#define burtcClkDiv_8   8
 Divide clock by 8.
 
#define burtcClkDiv_16   16
 Divide clock by 16.
 
#define burtcClkDiv_32   32
 Divide clock by 32.
 
#define burtcClkDiv_64   64
 Divide clock by 64.
 
#define burtcClkDiv_128   128
 Divide clock by 128.
 
#define BURTC_INIT_DEFAULT
 Default configuration for BURTC init structure.
 

Function Documentation

◆ BURTC_IntClear()

void BURTC_IntClear ( uint32_t  flags)
inline

Clear one or more pending BURTC interrupts.

Parameters
[in]flagsBURTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).

◆ BURTC_IntDisable()

void BURTC_IntDisable ( uint32_t  flags)
inline

Disable one or more BURTC interrupts.

Parameters
[in]flagsBURTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).

◆ BURTC_IntEnable()

void BURTC_IntEnable ( uint32_t  flags)
inline

Enable one or more BURTC interrupts.

Note
Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using BURTC_IntClear() prior to enabling if a pending interrupt should be ignored.
Parameters
[in]flagsBURTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).

◆ BURTC_IntGet()

uint32_t BURTC_IntGet ( void  )
inline

Get pending BURTC interrupt flags.

Note
This function does not clear the event bits.
Returns
Pending BURTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).

◆ BURTC_IntGetEnabled()

uint32_t BURTC_IntGetEnabled ( void  )
inline

Get enabled and pending BURTC interrupt flags.

Note
The event bits are not cleared by the use of this function.
Returns
Pending BURTC interrupt sources that is also enabled. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).

◆ BURTC_IntSet()

void BURTC_IntSet ( uint32_t  flags)
inline

Set one or more pending BURTC interrupts from SW.

Parameters
[in]flagsBURTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn).

◆ BURTC_Status()

uint32_t BURTC_Status ( void  )
inline

Status of BURTC RAM, timestamp and LP Mode.

Returns
A mask logially OR-ed status bits

◆ BURTC_SyncWait()

void BURTC_SyncWait ( void  )
inline

Wait for the BURTC to complete all synchronization of register changes and commands.

◆ BURTC_Start()

void BURTC_Start ( void  )
inline

Start BURTC counter.

This function will send a start command to the BURTC peripheral. The BURTC peripheral will use some LF clock ticks before the command is executed. The BURTC_SyncWait() function can be used to wait for the start command to be executed.

Note
This function requires the BURTC to be enabled.

◆ BURTC_Stop()

void BURTC_Stop ( void  )
inline

Stop the BURTC counter.

This function will send a stop command to the BURTC peripheral. The BURTC peripheral will use some LF clock ticks before the command is executed. The BURTC_SyncWait() function can be used to wait for the stop command to be executed.

Note
This function requires the BURTC to be enabled.

◆ BURTC_CounterGet()

uint32_t BURTC_CounterGet ( void  )
inline

Get BURTC counter.

Returns
BURTC counter value

◆ BURTC_Lock()

void BURTC_Lock ( void  )
inline

Lock BURTC registers, will protect from writing new config settings.

◆ BURTC_Unlock()

void BURTC_Unlock ( void  )
inline

Unlock BURTC registers, enable write access to change configuration.

◆ BURTC_Reset()

void BURTC_Reset ( void  )

Restore BURTC to reset state.

Note
Before accessing the BURTC, BURSTEN in RMU->CTRL must be cleared. LOCK will not be reset to default value, as this will disable access to core BURTC registers.

◆ BURTC_Init()

void BURTC_Init ( const BURTC_Init_TypeDef burtcInit)

Initialize BURTC.

Configures the BURTC peripheral.

Note
Before initialization, BURTC module must first be enabled by clearing the reset bit in the RMU, i.e.,
*   RMU_ResetControl(rmuResetBU, rmuResetModeClear);
* 
Compare channel 0 must be configured outside this function, before initialization if enable is set to true. The counter will always be reset.
Parameters
[in]burtcInitA pointer to the BURTC initialization structure.

◆ BURTC_Enable()

void BURTC_Enable ( bool  enable)

Enable or Disable BURTC peripheral.

Parameters
[in]enabletrue to enable, false to disable.

◆ BURTC_CounterReset()

void BURTC_CounterReset ( void  )

Reset counter.

◆ BURTC_CompareSet()

void BURTC_CompareSet ( unsigned int  comp,
uint32_t  value 
)

Set BURTC compare channel.

Parameters
[in]compCompare the channel index, must be 0 for current devices.
[in]valueNew compare value.

◆ BURTC_CompareGet()

uint32_t BURTC_CompareGet ( unsigned int  comp)

Get the BURTC compare value.

Parameters
[in]compCompare the channel index value, must be 0 for Giant/Leopard Gecko.
Returns
The currently configured value for this compare channel.

Macro Definition Documentation

◆ burtcClkDiv_1

#define burtcClkDiv_1   1

BURTC clock divisors.

These values are valid for the BURTC prescaler. Divide clock by 1.

◆ burtcClkDiv_2

#define burtcClkDiv_2   2

Divide clock by 2.

◆ burtcClkDiv_4

#define burtcClkDiv_4   4

Divide clock by 4.

◆ burtcClkDiv_8

#define burtcClkDiv_8   8

Divide clock by 8.

◆ burtcClkDiv_16

#define burtcClkDiv_16   16

Divide clock by 16.

◆ burtcClkDiv_32

#define burtcClkDiv_32   32

Divide clock by 32.

◆ burtcClkDiv_64

#define burtcClkDiv_64   64

Divide clock by 64.

◆ burtcClkDiv_128

#define burtcClkDiv_128   128

Divide clock by 128.

◆ BURTC_INIT_DEFAULT

#define BURTC_INIT_DEFAULT
Value:
{ \
true, \
false, \
1, \
0, \
false, \
false, \
}

Default configuration for BURTC init structure.