EMU_DCDCInit_TypeDef Struct Reference
DCDC regulator initialization structure.
#include <em_emu.h>
Data Fields | |
EMU_DcdcMode_TypeDef | mode |
DCDC mode. | |
EMU_VreginCmpThreshold_TypeDef | cmpThreshold |
VREGIN comparator threshold. | |
EMU_DcdcTonMaxTimeout_TypeDef | tonMax |
Ton max timeout control. | |
bool | dcmOnlyEn |
DCM only mode enable. | |
EMU_DcdcDriveSpeed_TypeDef | driveSpeedEM01 |
DCDC drive speed in EM0/1. | |
EMU_DcdcDriveSpeed_TypeDef | driveSpeedEM23 |
DCDC drive speed in EM2/3. | |
EMU_DcdcPeakCurrent_TypeDef | peakCurrentEM01 |
EM0/1 peak current setting. | |
EMU_DcdcPeakCurrent_TypeDef | peakCurrentEM23 |
EM2/3 peak current setting. | |
DCDC regulator initialization structure.
Field Documentation
◆ mode
EMU_DcdcMode_TypeDef EMU_DCDCInit_TypeDef::mode |
DCDC mode.
◆ cmpThreshold
EMU_VreginCmpThreshold_TypeDef EMU_DCDCInit_TypeDef::cmpThreshold |
VREGIN comparator threshold.
◆ tonMax
EMU_DcdcTonMaxTimeout_TypeDef EMU_DCDCInit_TypeDef::tonMax |
Ton max timeout control.
◆ dcmOnlyEn
bool EMU_DCDCInit_TypeDef::dcmOnlyEn |
DCM only mode enable.
◆ driveSpeedEM01
EMU_DcdcDriveSpeed_TypeDef EMU_DCDCInit_TypeDef::driveSpeedEM01 |
DCDC drive speed in EM0/1.
◆ driveSpeedEM23
EMU_DcdcDriveSpeed_TypeDef EMU_DCDCInit_TypeDef::driveSpeedEM23 |
DCDC drive speed in EM2/3.
◆ peakCurrentEM01
EMU_DcdcPeakCurrent_TypeDef EMU_DCDCInit_TypeDef::peakCurrentEM01 |
EM0/1 peak current setting.
◆ peakCurrentEM23
EMU_DcdcPeakCurrent_TypeDef EMU_DCDCInit_TypeDef::peakCurrentEM23 |
EM2/3 peak current setting.