sl_led_rgbw_pwm_t Struct Reference
A Simple RGBW LED PWM instance.
#include <sl_simple_rgbw_pwm_led.h>
Data Fields | |
sl_led_t | led_common |
Inherit from the Common LED Driver. | |
void(* | set_rgbw_color )(void *context, uint16_t red, uint16_t green, uint16_t blue, uint16_t white) |
member function to set RGBW | |
void(* | get_rgbw_color )(void *context, uint16_t *red, uint16_t *green, uint16_t *blue, uint16_t *white) |
member function to get RGBW | |
A Simple RGBW LED PWM instance.
Field Documentation
◆ led_common
sl_led_t sl_led_rgbw_pwm_t::led_common |
Inherit from the Common LED Driver.
◆ set_rgbw_color
void(* sl_led_rgbw_pwm_t::set_rgbw_color) (void *context, uint16_t red, uint16_t green, uint16_t blue, uint16_t white) |
member function to set RGBW
◆ get_rgbw_color
void(* sl_led_rgbw_pwm_t::get_rgbw_color) (void *context, uint16_t *red, uint16_t *green, uint16_t *blue, uint16_t *white) |
member function to get RGBW