sl_cli_command_arg_t Struct Reference
Command arguments data type.
#include <sl_cli_types.h>
Data Fields | |
struct sl_cli * | handle |
The current cli handle. | |
int | argc |
The total number of input strings (command group names, if any + command + corresponding arguments). | |
void ** | argv |
A pointer to the input string array. | |
int | arg_ofs |
The offset in the input string array where the arguments start (after the command group names, if any and command). | |
const sl_cli_argument_type_t * | arg_type_list |
List of argument types. | |
Command arguments data type.
Field Documentation
◆ handle
struct sl_cli* sl_cli_command_arg_t::handle |
The current cli handle.
◆ argc
int sl_cli_command_arg_t::argc |
The total number of input strings (command group names, if any + command + corresponding arguments).
◆ argv
void** sl_cli_command_arg_t::argv |
A pointer to the input string array.
◆ arg_ofs
int sl_cli_command_arg_t::arg_ofs |
The offset in the input string array where the arguments start (after the command group names, if any and command).
◆ arg_type_list
const sl_cli_argument_type_t* sl_cli_command_arg_t::arg_type_list |
List of argument types.