|
void
|
IADC_init
(IADC_TypeDef *iadc, const
IADC_Init_t
*init, const
IADC_AllConfigs_t
*allConfigs)
|
|
Initialize IADC.
|
|
void
|
IADC_initScan
(IADC_TypeDef *iadc, const
IADC_InitScan_t
*init, const
IADC_ScanTable_t
*scanTable)
|
|
Initialize IADC scan sequence.
|
|
void
|
IADC_initSingle
(IADC_TypeDef *iadc, const
IADC_InitSingle_t
*init, const
IADC_SingleInput_t
*input)
|
|
Initialize single IADC conversion.
|
|
void
|
IADC_updateSingleInput
(IADC_TypeDef *iadc, const
IADC_SingleInput_t
*input)
|
|
Update IADC single input selection.
|
|
void
|
IADC_setScanMask
(IADC_TypeDef *iadc, uint32_t mask)
|
|
Set mask of IADC scan table entries to include in scan.
|
|
void
|
IADC_updateScanEntry
(IADC_TypeDef *iadc, uint8_t id,
IADC_ScanTableEntry_t
*entry)
|
|
Add/update entry in scan table.
|
|
void
|
IADC_reset
(IADC_TypeDef *iadc)
|
|
Reset IADC to same state as after a HW reset.
|
|
uint8_t
|
IADC_calcTimebase
(IADC_TypeDef *iadc, uint32_t cmuClkFreq)
|
|
Calculate timebase value in order to get a timebase providing at least 1us.
|
|
uint8_t
|
IADC_calcSrcClkPrescale
(IADC_TypeDef *iadc, uint32_t srcClkFreq, uint32_t cmuClkFreq)
|
|
Calculate prescaler for CLK_SRC_ADC high speed clock.
|
|
uint32_t
|
IADC_calcAdcClkPrescale
(IADC_TypeDef *iadc, uint32_t adcClkFreq, uint32_t cmuClkFreq,
IADC_CfgAdcMode_t
adcMode, uint8_t srcClkPrescaler)
|
|
Calculate prescaler for ADC_CLK clock.
|
|
IADC_Result_t
|
IADC_pullSingleFifoResult
(IADC_TypeDef *iadc)
|
|
Pull result from single data FIFO.
|
|
IADC_Result_t
|
IADC_readSingleResult
(IADC_TypeDef *iadc)
|
|
Read most recent single conversion result.
|
|
IADC_Result_t
|
IADC_pullScanFifoResult
(IADC_TypeDef *iadc)
|
|
Pull result from scan data FIFO.
|
|
IADC_Result_t
|
IADC_readScanResult
(IADC_TypeDef *iadc)
|
|
Read most recent scan conversion result.
|
|
uint32_t
|
IADC_pullSingleFifoData
(IADC_TypeDef *iadc)
|
|
Pull data from single data FIFO.
|
|
uint32_t
|
IADC_readSingleData
(IADC_TypeDef *iadc)
|
|
Read most recent single conversion data.
|
|
uint32_t
|
IADC_pullScanFifoData
(IADC_TypeDef *iadc)
|
|
Pull data from scan data FIFO.
|
|
uint32_t
|
IADC_readScanData
(IADC_TypeDef *iadc)
|
|
Read most recent scan conversion data.
|
|
void
|
IADC_clearInt
(IADC_TypeDef *iadc, uint32_t flags)
|
|
Clear one or more pending IADC interrupts.
|
|
void
|
IADC_disableInt
(IADC_TypeDef *iadc, uint32_t flags)
|
|
Disable one or more IADC interrupts.
|
|
void
|
IADC_enableInt
(IADC_TypeDef *iadc, uint32_t flags)
|
|
Enable one or more IADC interrupts.
|
|
uint32_t
|
IADC_getInt
(IADC_TypeDef *iadc)
|
|
Get pending IADC interrupt flags.
|
|
uint32_t
|
IADC_getEnabledInt
(IADC_TypeDef *iadc)
|
|
Get enabled and pending IADC interrupt flags.
|
|
void
|
IADC_setInt
(IADC_TypeDef *iadc, uint32_t flags)
|
|
Set one or more pending IADC interrupts from SW.
|
|
void
|
IADC_command
(IADC_TypeDef *iadc,
IADC_Cmd_t
cmd)
|
|
Start/stop scan sequence, single conversion and/or timer.
|
|
uint32_t
|
IADC_getScanMask
(IADC_TypeDef *iadc)
|
|
Get the scan mask currently used in the IADC.
|
|
uint32_t
|
IADC_getStatus
(IADC_TypeDef *iadc)
|
|
Get status bits of IADC.
|
|
uint8_t
|
IADC_getSingleFifoCnt
(IADC_TypeDef *iadc)
|
|
Get number of elements in the IADC single FIFO.
|
|
uint8_t
|
IADC_getScanFifoCnt
(IADC_TypeDef *iadc)
|
|
Get number of elements in the IADC scan FIFO.
|
|
IADC_NegInput_t
|
IADC_portPinToNegInput
(
GPIO_Port_TypeDef
port, uint8_t pin)
|
|
Convert GPIO port/pin to IADC negative input selection.
|
|
IADC_PosInput_t
|
IADC_portPinToPosInput
(
GPIO_Port_TypeDef
port, uint8_t pin)
|
|
Convert GPIO port/pin to IADC positive input selection.
|
|