TIMER_InitCC_TypeDef Struct Reference

TIMER compare/capture initialization structure.

#include <em_timer.h>

Data Fields

TIMER_Event_TypeDef eventCtrl
 Input capture event control.
 
TIMER_Edge_TypeDef edge
 Input capture edge select.
 
TIMER_PRSSEL_TypeDef prsSel
 Peripheral reflex system trigger selection.
 
TIMER_OutputAction_TypeDef cufoa
 Counter underflow output action.
 
TIMER_OutputAction_TypeDef cofoa
 Counter overflow output action.
 
TIMER_OutputAction_TypeDef cmoa
 Counter match output action.
 
TIMER_CCMode_TypeDef mode
 Compare/capture channel mode.
 
bool filter
 Enable digital filter.
 
bool prsInput
 Select TIMERnCCx (false) or PRS input (true).
 
bool coist
 Compare output initial state.
 
bool outInvert
 Invert output from compare/capture channel.
 
TIMER_PrsOutput_t prsOutput
 PRS output configuration.
 
TIMER_PrsInput_TypeDef prsInputType
 When PRS input is used this field is used to configure the type of PRS input.
 

TIMER compare/capture initialization structure.

Field Documentation

◆ eventCtrl

TIMER_Event_TypeDef TIMER_InitCC_TypeDef::eventCtrl

Input capture event control.

◆ edge

TIMER_Edge_TypeDef TIMER_InitCC_TypeDef::edge

Input capture edge select.

◆ prsSel

TIMER_PRSSEL_TypeDef TIMER_InitCC_TypeDef::prsSel

Peripheral reflex system trigger selection.

Only applicable if prsInput is enabled.

◆ cufoa

TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cufoa

Counter underflow output action.

◆ cofoa

TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cofoa

Counter overflow output action.

◆ cmoa

TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cmoa

Counter match output action.

◆ mode

TIMER_CCMode_TypeDef TIMER_InitCC_TypeDef::mode

Compare/capture channel mode.

◆ filter

bool TIMER_InitCC_TypeDef::filter

Enable digital filter.

◆ prsInput

bool TIMER_InitCC_TypeDef::prsInput

Select TIMERnCCx (false) or PRS input (true).

◆ coist

bool TIMER_InitCC_TypeDef::coist

Compare output initial state.

Only used in Output Compare and PWM mode. When true, the compare/PWM output is set high when the counter is disabled. When counting resumes, this value will represent the initial value for the compare/PWM output. If the bit is cleared, the output will be cleared when the counter is disabled.

◆ outInvert

bool TIMER_InitCC_TypeDef::outInvert

Invert output from compare/capture channel.

◆ prsOutput

TIMER_PrsOutput_t TIMER_InitCC_TypeDef::prsOutput

PRS output configuration.

PRS output from a timer can either be a pulse output or a level output that follows the CC out value.

◆ prsInputType

TIMER_PrsInput_TypeDef TIMER_InitCC_TypeDef::prsInputType

When PRS input is used this field is used to configure the type of PRS input.