SMU - Security Management Unit

Description

Security Management Unit (SMU) Peripheral API.

SMU forms the control and status/reporting component of bus-level security in EFM32/EFR32 devices.

Peripheral-level protection is provided via the peripheral protection unit (PPU). PPU provides hardware access barrier to any peripheral that is configured to be protected. When an attempt is made to access a peripheral without the required privilege/security level, PPU detects the fault and intercepts the access. No write or read of the peripheral register space occurs, and an all-zero value is returned if the access is a read.

Usage example

// SMU is always clocked, so no call to CMU_ClockEnable() is necessary
// Initialize SMU to prevent access to CMU, EMU, SMU and GPIO
SMU_Init (&init);

Data Structures

struct SMU_PrivilegedAccess_TypeDef
SMU peripheral privileged access enablers.
struct SMU_Init_TypeDef
SMU initialization structure.

Functions

void SMU_EnablePPU (bool enable)
Enable or disable PPU of SMU.
void SMU_Init (const SMU_Init_TypeDef *init)
Initialize PPU of SMU.
void SMU_SetPrivilegedAccess ( SMU_Peripheral_TypeDef peripheral, bool privileged)
Change access settings for a peripheral.
SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral (void)
Get ID of the peripheral that caused an access fault.
void SMU_IntClear (uint32_t flags)
Clear one or more pending SMU interrupts.
void SMU_IntDisable (uint32_t flags)
Disable one or more SMU interrupts.
void SMU_IntEnable (uint32_t flags)
Enable one or more SMU interrupts.
uint32_t SMU_IntGet (void)
Get pending SMU interrupts.
uint32_t SMU_IntGetEnabled (void)
Get enabled and pending SMU interrupt flags.
void SMU_IntSet (uint32_t flags)
Set one or more pending SMU interrupts from SW.

Macros

#define SMU_INIT_DEFAULT
Default SMU initialization structure settings.

Enumerations

enum SMU_Peripheral_TypeDef {
smuPeripheralEMU = _SMU_PPUPATD0_EMU_SHIFT,
smuPeripheralCMU = _SMU_PPUPATD0_CMU_SHIFT,
smuPeripheralHFRCO0 = _SMU_PPUPATD0_HFRCO0_SHIFT,
smuPeripheralFSRCO = _SMU_PPUPATD0_FSRCO_SHIFT,
smuPeripheralDPLL0 = _SMU_PPUPATD0_DPLL0_SHIFT,
smuPeripheralLFXO = _SMU_PPUPATD0_LFXO_SHIFT,
smuPeripheralLFRCO = _SMU_PPUPATD0_LFRCO_SHIFT,
smuPeripheralULFRCO = _SMU_PPUPATD0_ULFRCO_SHIFT,
smuPeripheralMSC = _SMU_PPUPATD0_MSC_SHIFT,
smuPeripheralICACHE0 = _SMU_PPUPATD0_ICACHE0_SHIFT,
smuPeripheralPRS = _SMU_PPUPATD0_PRS_SHIFT,
smuPeripheralGPIO = _SMU_PPUPATD0_GPIO_SHIFT,
smuPeripheralLDMA = _SMU_PPUPATD0_LDMA_SHIFT,
smuPeripheralLDMAXBAR = _SMU_PPUPATD0_LDMAXBAR_SHIFT,
smuPeripheralTIMER0 = _SMU_PPUPATD0_TIMER0_SHIFT,
smuPeripheralTIMER1 = _SMU_PPUPATD0_TIMER1_SHIFT,
smuPeripheralTIMER2 = _SMU_PPUPATD0_TIMER2_SHIFT,
smuPeripheralTIMER3 = _SMU_PPUPATD0_TIMER3_SHIFT,
smuPeripheralTIMER4 = _SMU_PPUPATD0_TIMER4_SHIFT,
smuPeripheralUSART0 = _SMU_PPUPATD0_USART0_SHIFT,
smuPeripheralBURTC = _SMU_PPUPATD0_BURTC_SHIFT,
smuPeripheralI2C1 = _SMU_PPUPATD0_I2C1_SHIFT,
smuPeripheralCHIPTESTCTRL = _SMU_PPUPATD0_CHIPTESTCTRL_SHIFT,
smuPeripheralSYSCFGCFGNS = _SMU_PPUPATD0_SYSCFGCFGNS_SHIFT,
smuPeripheralSYSCFG = _SMU_PPUPATD0_SYSCFG_SHIFT,
smuPeripheralBURAM = _SMU_PPUPATD0_BURAM_SHIFT,
smuPeripheralGPCRC = _SMU_PPUPATD0_GPCRC_SHIFT,
smuPeripheralHOSTMAILBOX = _SMU_PPUPATD0_HOSTMAILBOX_SHIFT,
smuPeripheralEUSART1 = _SMU_PPUPATD0_EUSART1_SHIFT,
smuPeripheralEUSART2 = _SMU_PPUPATD0_EUSART2_SHIFT,
smuPeripheralSYSRTC = 32 + _SMU_PPUPATD1_SYSRTC_SHIFT,
smuPeripheralLCD = 32 + _SMU_PPUPATD1_LCD_SHIFT,
smuPeripheralKEYSCAN = 32 + _SMU_PPUPATD1_KEYSCAN_SHIFT,
smuPeripheralDMEM = 32 + _SMU_PPUPATD1_DMEM_SHIFT,
smuPeripheralLCDRF = 32 + _SMU_PPUPATD1_LCDRF_SHIFT,
smuPeripheralPFMXPPRF = 32 + _SMU_PPUPATD1_PFMXPPRF_SHIFT,
smuPeripheralVDAC0 = 32 + _SMU_PPUPATD1_VDAC0_SHIFT,
smuPeripheralPCNT = 32 + _SMU_PPUPATD1_PCNT_SHIFT,
smuPeripheralLESENSE = 32 + _SMU_PPUPATD1_LESENSE_SHIFT,
smuPeripheralHFRCO1 = 32 + _SMU_PPUPATD1_HFRCO1_SHIFT,
smuPeripheralHFXO0 = 32 + _SMU_PPUPATD1_HFXO0_SHIFT,
smuPeripheralLETIMER0 = 32 + _SMU_PPUPATD1_LETIMER0_SHIFT,
smuPeripheralIADC0 = 32 + _SMU_PPUPATD1_IADC0_SHIFT,
smuPeripheralACMP0 = 32 + _SMU_PPUPATD1_ACMP0_SHIFT,
smuPeripheralACMP1 = 32 + _SMU_PPUPATD1_ACMP1_SHIFT,
smuPeripheralI2C0 = 32 + _SMU_PPUPATD1_I2C0_SHIFT,
smuPeripheralWDOG0 = 32 + _SMU_PPUPATD1_WDOG0_SHIFT,
smuPeripheralWDOG1 = 32 + _SMU_PPUPATD1_WDOG1_SHIFT,
smuPeripheralAMUXCP0 = 32 + _SMU_PPUPATD1_AMUXCP0_SHIFT,
smuPeripheralRADIOAES = 32 + _SMU_PPUPATD1_RADIOAES_SHIFT,
smuPeripheralSMU = 32 + _SMU_PPUPATD1_SMU_SHIFT,
smuPeripheralSMUCFGNS = 32 + _SMU_PPUPATD1_SMUCFGNS_SHIFT,
smuPeripheralAHBRADIO = 32 + _SMU_PPUPATD1_AHBRADIO_SHIFT,
smuPeripheralSEMAILBOX = 32 + _SMU_PPUPATD1_SEMAILBOX_SHIFT,
smuPeripheralEnd
}
SMU peripheral identifiers.

Function Documentation

◆ SMU_EnablePPU()

void SMU_EnablePPU ( bool enable )
inline

Enable or disable PPU of SMU.

Parameters
[in] enable Set to true to enable PPU; set to false otherwise.

◆ SMU_Init()

void SMU_Init ( const SMU_Init_TypeDef * init )
inline

Initialize PPU of SMU.

Parameters
[in] init Pointer to initialization structure that defines which peripherals should only be accessed from privileged mode, and if PPU should be enabled.

◆ SMU_SetPrivilegedAccess()

void SMU_SetPrivilegedAccess ( SMU_Peripheral_TypeDef peripheral,
bool privileged
)
inline

Change access settings for a peripheral.

Set to limit access of a peripheral from privileged mode.

Parameters
[in] peripheral ID of the peripheral to change access settings for.
[in] privileged Set to true if the peripheral should only be accessed from privileged mode; set to false otherwise.

◆ SMU_GetFaultingPeripheral()

SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral ( void )
inline

Get ID of the peripheral that caused an access fault.

Note
The return value is only valid if SMU_IF_PPUPRIV interrupt flag is set.
Returns
ID of the peripheral that caused an access fault.

◆ SMU_IntClear()

void SMU_IntClear ( uint32_t flags )
inline

Clear one or more pending SMU interrupts.

Parameters
[in] flags Bitwise logic OR of SMU interrupt sources to clear.

◆ SMU_IntDisable()

void SMU_IntDisable ( uint32_t flags )
inline

Disable one or more SMU interrupts.

Parameters
[in] flags SMU interrupt sources to disable.

◆ SMU_IntEnable()

void SMU_IntEnable ( uint32_t flags )
inline

Enable one or more SMU interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using SMU_IntClear() prior to enabling the interrupt.
Parameters
[in] flags SMU interrupt sources to enable.

◆ SMU_IntGet()

uint32_t SMU_IntGet ( void )
inline

Get pending SMU interrupts.

Returns
SMU interrupt sources pending.

◆ SMU_IntGetEnabled()

uint32_t SMU_IntGetEnabled ( void )
inline

Get enabled and pending SMU interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
Interrupt flags are not cleared by this function.
Returns
Pending and enabled SMU interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in SMU_IEN register and
  • the OR combination of valid interrupt flags in SMU_IF register.

◆ SMU_IntSet()

void SMU_IntSet ( uint32_t flags )
inline

Set one or more pending SMU interrupts from SW.

Parameters
[in] flags SMU interrupt sources to set to pending.

Macro Definition Documentation

◆ SMU_INIT_DEFAULT

#define SMU_INIT_DEFAULT
Value:
{ \
{ { 0 } }, /* No peripherals access protected. */ \
true /* Enable SMU.*/ \
}

Default SMU initialization structure settings.

Enumeration Type Documentation

◆ SMU_Peripheral_TypeDef

SMU peripheral identifiers.

Enumerator
smuPeripheralEMU

SMU peripheral identifier for EMU

smuPeripheralCMU

SMU peripheral identifier for CMU

smuPeripheralHFRCO0

SMU peripheral identifier for HFRCO0

smuPeripheralFSRCO

SMU peripheral identifier for FSRCO

smuPeripheralDPLL0

SMU peripheral identifier for DPLL0

smuPeripheralLFXO

SMU peripheral identifier for LFXO

smuPeripheralLFRCO

SMU peripheral identifier for LFRCO

smuPeripheralULFRCO

SMU peripheral identifier for ULFRCO

smuPeripheralMSC

SMU peripheral identifier for MSC

smuPeripheralICACHE0

SMU peripheral identifier for ICACHE0

smuPeripheralPRS

SMU peripheral identifier for PRS

smuPeripheralGPIO

SMU peripheral identifier for GPIO

smuPeripheralLDMA

SMU peripheral identifier for LDMA

smuPeripheralLDMAXBAR

SMU peripheral identifier for LDMAXBAR

smuPeripheralTIMER0

SMU peripheral identifier for TIMER0

smuPeripheralTIMER1

SMU peripheral identifier for TIMER1

smuPeripheralTIMER2

SMU peripheral identifier for TIMER2

smuPeripheralTIMER3

SMU peripheral identifier for TIMER3

smuPeripheralTIMER4

SMU peripheral identifier for TIMER4

smuPeripheralUSART0

SMU peripheral identifier for USART0

smuPeripheralBURTC

SMU peripheral identifier for BURTC

smuPeripheralI2C1

SMU peripheral identifier for I2C1

smuPeripheralCHIPTESTCTRL

SMU peripheral identifier for CHIPTESTCTRL.

smuPeripheralSYSCFGCFGNS

SMU peripheral identifier for SYSCFGCFGNS.

smuPeripheralSYSCFG

SMU peripheral identifier for SYSCFG

smuPeripheralBURAM

SMU peripheral identifier for BURAM

smuPeripheralGPCRC

SMU peripheral identifier for GPCRC

smuPeripheralHOSTMAILBOX

SMU peripheral identifier for HOSTMAILBOX.

smuPeripheralEUSART1

SMU peripheral identifier for EUSART1

smuPeripheralEUSART2

SMU peripheral identifier for EUSART2

smuPeripheralSYSRTC

SMU peripheral identifier for SYSRTC

smuPeripheralLCD

SMU peripheral identifier for LCD

smuPeripheralKEYSCAN

SMU peripheral identifier for KEYSCAN

smuPeripheralDMEM

SMU peripheral identifier for DMEM

smuPeripheralLCDRF

SMU peripheral identifier for LCDRF

smuPeripheralPFMXPPRF

SMU peripheral identifier for PFMXPPRF

smuPeripheralVDAC0

SMU peripheral identifier for VDAC0

smuPeripheralPCNT

SMU peripheral identifier for PCNT

smuPeripheralLESENSE

SMU peripheral identifier for LESENSE

smuPeripheralHFRCO1

SMU peripheral identifier for HFRCO1

smuPeripheralHFXO0

SMU peripheral identifier for HFXO0

smuPeripheralLETIMER0

SMU peripheral identifier for LETIMER

smuPeripheralIADC0

SMU peripheral identifier for IADC0

smuPeripheralACMP0

SMU peripheral identifier for ACMP0

smuPeripheralACMP1

SMU peripheral identifier for ACMP1

smuPeripheralI2C0

SMU peripheral identifier for I2C0

smuPeripheralWDOG0

SMU peripheral identifier for WDOG0

smuPeripheralWDOG1

SMU peripheral identifier for WDOG1

smuPeripheralAMUXCP0

SMU peripheral identifier for AMUXCP0

smuPeripheralRADIOAES

SMU peripheral identifier for RADIOAES

smuPeripheralSMU

SMU peripheral identifier for SMU

smuPeripheralSMUCFGNS

SMU peripheral identifier for SMUCFGNS

smuPeripheralAHBRADIO

SMU peripheral identifier for AHBRADIO

smuPeripheralSEMAILBOX

SMU peripheral identifier for SEMAILBOX.

smuPeripheralEnd

SMU peripheral end.