CMU_LFXOInit_TypeDef Struct Reference
LFXO initialization structure.
#include <em_cmu.h>
Data Fields | |
uint8_t | ctune |
CTUNE (load capacitance) value. | |
uint8_t | gain |
Gain/max startup margin. | |
uint8_t | timeout |
Startup delay. | |
CMU_OscMode_TypeDef | mode |
Oscillator mode. | |
LFXO initialization structure.
Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
Field Documentation
◆ ctune
uint8_t CMU_LFXOInit_TypeDef::ctune |
CTUNE (load capacitance) value.
◆ gain
uint8_t CMU_LFXOInit_TypeDef::gain |
Gain/max startup margin.
◆ timeout
uint8_t CMU_LFXOInit_TypeDef::timeout |
Startup delay.
◆ mode
CMU_OscMode_TypeDef CMU_LFXOInit_TypeDef::mode |
Oscillator mode.