AES - AES Accelerator
Description
Advanced Encryption Standard Accelerator (AES) Peripheral API.
The AES peripheral supports AES block cipher encryption and decryption with 128 bit and 256 bit keys. The following block cipher modes are supported:
- CBC - Cipher Block Chaining mode
- CFB - Cipher Feedback mode
- CTR - Counter mode
- ECB - Electronic Code Book mode
- OFB - Output Feedback mode
The following input/output notations should be noted:
- Input/output data (plaintext, ciphertext, key, and so on) are treated as byte arrays, starting with the most significant byte, i.e., 32 bytes of plaintext (B0...B31) is located in memory in the same order, with B0 at the lower address and B31 at the higher address.
- Byte arrays must always be a multiple of AES block size, i.e., a multiple of 16. Padding, if required, is done at the end of the byte array.
- Byte arrays should be word (32 bit) aligned for performance considerations, since the array is accessed with a 32 bit access type. Cortex-M supports unaligned accesses with a performance penalty.
- It is possible to specify the same output buffer as an input buffer as long as they point to the same address. In that case, the provided input buffer is replaced with the encrypted/decrypted output. Notice that buffers must be exactly overlapping. If partly overlapping, the behavior is undefined.
Use a cipher mode according to its requirements to avoid breaking security. See a specific cipher mode theory for details.
References:
- Wikipedia - Cipher modes, http://en.wikipedia.org/wiki/Cipher_modes
- Recommendation for Block Cipher Modes of Operation, NIST Special Publication 800-38A, 2001 Edition, http://csrc.nist.gov/publications/nistpubs/800-38a/sp800-38a.pdf
The following example shows how to perform an AES-128 CBC encryption:
Enable clocks:
Execute AES-128 CBC encryption:
This module contains functions to control the AES peripheral of Silicon Labs 32-bit MCUs and SoCs.
Functions |
|
| void | AES_CBC128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt) |
|
Cipher-block chaining (CBC) cipher mode encryption/decryption, 128 bit key.
|
|
| void | AES_CFB128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv, bool encrypt) |
|
Cipher feedback (CFB) cipher mode encryption/decryption, 128 bit key.
|
|
| void | AES_CTR128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, uint8_t *ctr, AES_CtrFuncPtr_TypeDef ctrFunc) |
|
Counter (CTR) cipher mode encryption/decryption, 128 bit key.
|
|
| void | AES_CTRUpdate32Bit (uint8_t *ctr) |
|
Update last 32 bits of 128 bit counter by incrementing with 1.
|
|
| void | AES_DecryptKey128 (uint8_t *out, const uint8_t *in) |
|
Generate a 128 bit decryption key from the 128 bit encryption key.
|
|
| void | AES_ECB128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, bool encrypt) |
|
Electronic Codebook (ECB) cipher mode encryption/decryption, 128 bit key.
|
|
| void | AES_IntClear (uint32_t flags) |
|
Clear one or more pending AES interrupts.
|
|
| void | AES_IntDisable (uint32_t flags) |
|
Disable one or more AES interrupts.
|
|
| void | AES_IntEnable (uint32_t flags) |
|
Enable one or more AES interrupts.
|
|
| uint32_t | AES_IntGet (void) |
|
Get pending AES interrupt flags.
|
|
| uint32_t | AES_IntGetEnabled (void) |
|
Get enabled and pending AES interrupt flags.
|
|
| void | AES_IntSet (uint32_t flags) |
|
Set one or more pending AES interrupts from software.
|
|
| void | AES_OFB128 (uint8_t *out, const uint8_t *in, unsigned int len, const uint8_t *key, const uint8_t *iv) |
|
Output feedback (OFB) cipher mode encryption/decryption, 128 bit key.
|
|
Typedefs |
|
| typedef void(* | AES_CtrFuncPtr_TypeDef ) (uint8_t *ctr) |
|
An AES counter modification function pointer.
|
|
Function Documentation
◆ AES_CBC128()
| void AES_CBC128 | ( | uint8_t * |
out,
|
| const uint8_t * |
in,
|
||
| unsigned int |
len,
|
||
| const uint8_t * |
key,
|
||
| const uint8_t * |
iv,
|
||
| bool |
encrypt
|
||
| ) |
Cipher-block chaining (CBC) cipher mode encryption/decryption, 128 bit key.
Encryption:
* Plaintext Plaintext * | | * V V * InitVector ->XOR +-------------->XOR * | | | * V | V * +--------------+ | +--------------+ * Key ->| Block cipher | | Key ->| Block cipher | * | encryption | | | encryption | * +--------------+ | +--------------+ * |---------+ | * V V * Ciphertext Ciphertext *
Decryption:
* Ciphertext Ciphertext * |----------+ | * V | V * +--------------+ | +--------------+ * Key ->| Block cipher | | Key ->| Block cipher | * | decryption | | | decryption | * +--------------+ | +--------------+ * | | | * V | V * InitVector ->XOR +-------------->XOR * | | * V V * Plaintext Plaintext *
See general comments on layout and byte ordering of parameters.
- Parameters
-
[out] outA buffer to place encrypted/decrypted data. Must be at least lenlong. It may be set equal toin, in which case the input buffer is overwritten.[in] inA buffer holding data to encrypt/decrypt. Must be at least lenlong.[in] lenA number of bytes to encrypt/decrypt. Must be a multiple of 16. [in] keyWhen encrypting, this is the 128 bit encryption key. When decrypting, this is the 128 bit decryption key. The decryption key may be generated from the encryption key with AES_DecryptKey128() . On devices supporting key buffering, this argument can be null. If so, the key will not be loaded as it is assumed the key has been loaded into KEYHA previously. [in] iv128 bit initialization vector. [in] encryptSet to true to encrypt, false to decrypt.
◆ AES_CFB128()
| void AES_CFB128 | ( | uint8_t * |
out,
|
| const uint8_t * |
in,
|
||
| unsigned int |
len,
|
||
| const uint8_t * |
key,
|
||
| const uint8_t * |
iv,
|
||
| bool |
encrypt
|
||
| ) |
Cipher feedback (CFB) cipher mode encryption/decryption, 128 bit key.
Encryption:
* InitVector +----------------+ * | | | * V | V * +--------------+ | +--------------+ * Key ->| Block cipher | | Key ->| Block cipher | * | encryption | | | encryption | * +--------------+ | +--------------+ * | | | * V | V * Plaintext ->XOR | Plaintext ->XOR * |---------+ | * V V * Ciphertext Ciphertext *
Decryption:
* InitVector +----------------+ * | | | * V | V * +--------------+ | +--------------+ * Key ->| Block cipher | | Key ->| Block cipher | * | encryption | | | encryption | * +--------------+ | +--------------+ * | | | * V | V * XOR<- Ciphertext XOR<- Ciphertext * | | * V V * Plaintext Plaintext *
See general comments on layout and byte ordering of parameters.
- Parameters
-
[out] outA buffer to place encrypted/decrypted data. Must be at least lenlong. It may be set equal toin, in which case the input buffer is overwritten.[in] inA buffer holding data to encrypt/decrypt. Must be at least lenlong.[in] lenA number of bytes to encrypt/decrypt. Must be a multiple of 16. [in] key128 bit encryption key is used for both encryption and decryption modes. [in] iv128 bit initialization vector to use. [in] encryptSet to true to encrypt, false to decrypt.
◆ AES_CTR128()
| void AES_CTR128 | ( | uint8_t * |
out,
|
| const uint8_t * |
in,
|
||
| unsigned int |
len,
|
||
| const uint8_t * |
key,
|
||
| uint8_t * |
ctr,
|
||
| AES_CtrFuncPtr_TypeDef |
ctrFunc
|
||
| ) |
Counter (CTR) cipher mode encryption/decryption, 128 bit key.
Encryption:
* Counter Counter * | | * V V * +--------------+ +--------------+ * Key ->| Block cipher | Key ->| Block cipher | * | encryption | | encryption | * +--------------+ +--------------+ * | | * Plaintext ->XOR Plaintext ->XOR * | | * V V * Ciphertext Ciphertext *
Decryption:
* Counter Counter * | | * V V * +--------------+ +--------------+ * Key ->| Block cipher | Key ->| Block cipher | * | encryption | | encryption | * +--------------+ +--------------+ * | | * Ciphertext ->XOR Ciphertext ->XOR * | | * V V * Plaintext Plaintext *
See general comments on layout and byte ordering of parameters.
- Parameters
-
[out] outA buffer to place encrypted/decrypted data. Must be at least lenlong. It may be set equal toin, in which case the input buffer is overwritten.[in] inA buffer holding data to encrypt/decrypt. Must be at least lenlong.[in] lenA number of bytes to encrypt/decrypt. Must be a multiple of 16. [in] key128 bit encryption key. On devices supporting key buffering this argument can be null. If so, the key will not be loaded, as it is assumed the key has been loaded into KEYHA previously. [in,out] ctr128 bit initial counter value. The counter is updated after each AES block encoding through use of ctrFunc.[in] ctrFuncA function used to update the counter value.
◆ AES_CTRUpdate32Bit()
| void AES_CTRUpdate32Bit | ( | uint8_t * |
ctr
|
) |
Update last 32 bits of 128 bit counter by incrementing with 1.
Notice that no special consideration is given to possible wrap around. If 32 least significant bits are 0xFFFFFFFF, they will be updated to 0x00000000, ignoring overflow.
See general comments on layout and byte ordering of parameters.
- Parameters
-
[in,out] ctrA buffer holding 128 bit counter to be updated.
◆ AES_DecryptKey128()
| void AES_DecryptKey128 | ( | uint8_t * |
out,
|
| const uint8_t * |
in
|
||
| ) |
Generate a 128 bit decryption key from the 128 bit encryption key.
The decryption key is used for some cipher modes when decrypting.
See general comments on layout and byte ordering of parameters.
- Parameters
-
[out] outA buffer to place 128 bit decryption key. Must be at least 16 bytes long. It may be set equal to in, in which case the input buffer is overwritten.[in] inA buffer holding 128 bit encryption key. Must be at least 16 bytes long.
◆ AES_ECB128()
| void AES_ECB128 | ( | uint8_t * |
out,
|
| const uint8_t * |
in,
|
||
| unsigned int |
len,
|
||
| const uint8_t * |
key,
|
||
| bool |
encrypt
|
||
| ) |
Electronic Codebook (ECB) cipher mode encryption/decryption, 128 bit key.
Encryption:
* Plaintext Plaintext * | | * V V * +--------------+ +--------------+ * Key ->| Block cipher | Key ->| Block cipher | * | encryption | | encryption | * +--------------+ +--------------+ * | | * V V * Ciphertext Ciphertext *
Decryption:
* Ciphertext Ciphertext * | | * V V * +--------------+ +--------------+ * Key ->| Block cipher | Key ->| Block cipher | * | decryption | | decryption | * +--------------+ +--------------+ * | | * V V * Plaintext Plaintext *
See general comments on layout and byte ordering of parameters.
- Parameters
-
[out] outA buffer to place encrypted/decrypted data. Must be at least lenlong. It may be set equal toin, in which case the input buffer is overwritten.[in] inA buffer holding data to encrypt/decrypt. Must be at least lenlong.[in] lenA number of bytes to encrypt/decrypt. Must be a multiple of 16. [in] keyWhen encrypting, this is the 128 bit encryption key. When decrypting, this is the 128 bit decryption key. The decryption key may be generated from the encryption key with AES_DecryptKey128() . [in] encryptSet to true to encrypt, false to decrypt.
◆ AES_IntClear()
|
inline |
Clear one or more pending AES interrupts.
- Parameters
-
[in] flagsA pending AES interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the AES module (AES_IF_nnn).
◆ AES_IntDisable()
|
inline |
Disable one or more AES interrupts.
- Parameters
-
[in] flagsAn AES interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the AES module (AES_IF_nnn).
◆ AES_IntEnable()
|
inline |
Enable one or more AES interrupts.
- Note
- Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using AES_IntClear() prior to enabling if a pending interrupt should be ignored.
- Parameters
-
[in] flagsAES interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the AES module (AES_IF_nnn).
◆ AES_IntGet()
|
inline |
Get pending AES interrupt flags.
- Note
- This function does not clear event bits.
- Returns
- AES interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the AES module (AES_IF_nnn).
◆ AES_IntGetEnabled()
|
inline |
Get enabled and pending AES interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- This function does not clear interrupt flags.
- Returns
-
Pending and enabled AES interrupt sources. The return value is the bitwise AND of
- the enabled interrupt sources in AES_IEN and
- the pending interrupt flags AES_IF
◆ AES_IntSet()
|
inline |
Set one or more pending AES interrupts from software.
- Parameters
-
[in] flagsAES interrupt sources to set as pending. Use a bitwise logic OR combination of valid interrupt flags for the AES module (AES_IF_nnn).
◆ AES_OFB128()
| void AES_OFB128 | ( | uint8_t * |
out,
|
| const uint8_t * |
in,
|
||
| unsigned int |
len,
|
||
| const uint8_t * |
key,
|
||
| const uint8_t * |
iv
|
||
| ) |
Output feedback (OFB) cipher mode encryption/decryption, 128 bit key.
Encryption:
* InitVector +----------------+ * | | | * V | V * +--------------+ | +--------------+ * Key ->| Block cipher | | Key ->| Block cipher | * | encryption | | | encryption | * +--------------+ | +--------------+ * | | | * |---------+ | * V V * Plaintext ->XOR Plaintext ->XOR * | | * V V * Ciphertext Ciphertext *
Decryption:
* InitVector +----------------+ * | | | * V | V * +--------------+ | +--------------+ * Key ->| Block cipher | | Key ->| Block cipher | * | encryption | | | encryption | * +--------------+ | +--------------+ * | | | * |---------+ | * V V * Ciphertext ->XOR Ciphertext ->XOR * | | * V V * Plaintext Plaintext *
See general comments on layout and byte ordering of parameters.
- Parameters
-
[out] outA buffer to place encrypted/decrypted data. Must be at least lenlong. It may be set equal toin, in which case the input buffer is overwritten.[in] inA buffer holding data to encrypt/decrypt. Must be at least lenlong.[in] lenA number of bytes to encrypt/decrypt. Must be a multiple of 16. [in] key128 bit encryption key. [in] iv128 bit initialization vector to use.
Typedef Documentation
◆ AES_CtrFuncPtr_TypeDef
| typedef void(* AES_CtrFuncPtr_TypeDef) (uint8_t *ctr) |
An AES counter modification function pointer.
Parameters:
- ctr - Ptr to byte array (16 bytes) holding a counter to be modified.