CMU - Clock Management Unit
Description
Clock management unit (CMU) Peripheral API.
This module contains functions for the CMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The CMU module controls oscillators, clocks gates, clock multiplexers, pre-scalers, calibration modules and wait-states.
Data Structures |
|
| struct | CMU_LFXOInit_TypeDef |
|
LFXO initialization structure.
|
|
| struct | CMU_HFXOInit_TypeDef |
|
HFXO initialization structure.
|
|
Functions |
|
| void | CMU_UpdateWaitStates (uint32_t freq, int vscale) |
|
Configure various wait states to switch to a certain frequency and a certain voltage scale.
|
|
| void | syncReg (uint32_t mask) |
|
Wait for an ongoing sync of register(s) to low-frequency domain to complete.
|
|
| CMU_AUXHFRCOBand_TypeDef | CMU_AUXHFRCOBandGet (void) |
|
Get the AUXHFRCO band in use.
|
|
| void | CMU_AUXHFRCOBandSet ( CMU_AUXHFRCOBand_TypeDef band) |
|
Set the AUXHFRCO band and the tuning value based on the value in the calibration table made during production.
|
|
| uint32_t | CMU_Calibrate (uint32_t HFCycles, CMU_Osc_TypeDef reference) |
|
Calibrate the clock.
|
|
| void | CMU_CalibrateConfig (uint32_t downCycles, CMU_Osc_TypeDef downSel, CMU_Osc_TypeDef upSel) |
|
Configure the clock calibration.
|
|
| uint32_t | CMU_CalibrateCountGet (void) |
|
Get the calibration count register.
|
|
| CMU_ClkDiv_TypeDef | CMU_ClockDivGet ( CMU_Clock_TypeDef clock) |
|
Get the clock divisor/prescaler.
|
|
| void | CMU_ClockDivSet ( CMU_Clock_TypeDef clock, CMU_ClkDiv_TypeDef div) |
|
Set the clock divisor/prescaler.
|
|
| void | CMU_ClockEnable ( CMU_Clock_TypeDef clock, bool enable) |
|
Enable/disable a clock.
|
|
| uint32_t | CMU_ClockFreqGet ( CMU_Clock_TypeDef clock) |
|
Get the clock frequency for a clock point.
|
|
| CMU_Select_TypeDef | CMU_ClockSelectGet ( CMU_Clock_TypeDef clock) |
|
Get the currently selected reference clock used for a clock branch.
|
|
| void | CMU_ClockSelectSet ( CMU_Clock_TypeDef clock, CMU_Select_TypeDef ref) |
|
Select the reference clock/oscillator used for a clock branch.
|
|
| uint16_t | CMU_LF_ClockPrecisionGet ( CMU_Clock_TypeDef clock) |
|
Gets the precision (in PPM) of the specified low frequency clock branch.
|
|
| void | CMU_FreezeEnable (bool enable) |
|
CMU low frequency register synchronization freeze control.
|
|
| CMU_HFRCOBand_TypeDef | CMU_HFRCOBandGet (void) |
|
Get HFRCO band in use.
|
|
| void | CMU_HFRCOBandSet ( CMU_HFRCOBand_TypeDef band) |
|
Set HFRCO band and the tuning value based on the value in the calibration table made during production.
|
|
| uint32_t | CMU_HFRCOStartupDelayGet (void) |
|
Get the HFRCO startup delay.
|
|
| void | CMU_HFRCOStartupDelaySet (uint32_t delay) |
|
Set the HFRCO startup delay.
|
|
| void | CMU_HFXOInit (const CMU_HFXOInit_TypeDef *hfxoInit) |
|
Set HFXO control registers.
|
|
| uint32_t | CMU_LCDClkFDIVGet (void) |
|
Get the LCD framerate divisor (FDIV) setting.
|
|
| void | CMU_LCDClkFDIVSet (uint32_t div) |
|
Set the LCD framerate divisor (FDIV) setting.
|
|
| void | CMU_LFXOInit (const CMU_LFXOInit_TypeDef *lfxoInit) |
|
Set LFXO control registers.
|
|
| void | CMU_LFXOPrecisionSet (uint16_t precision) |
|
Sets LFXO's crystal precision, in PPM.
|
|
| void | CMU_OscillatorEnable ( CMU_Osc_TypeDef osc, bool enable, bool wait) |
|
Enable/disable oscillator.
|
|
| uint32_t | CMU_OscillatorTuningGet ( CMU_Osc_TypeDef osc) |
|
Get the oscillator frequency tuning setting.
|
|
| void | CMU_OscillatorTuningSet ( CMU_Osc_TypeDef osc, uint32_t val) |
|
Set the oscillator frequency tuning control.
|
|
| bool | CMU_PCNTClockExternalGet (unsigned int instance) |
|
Determine if the currently selected PCNTn clock used is external or LFBCLK.
|
|
| void | CMU_PCNTClockExternalSet (unsigned int instance, bool external) |
|
Select the PCNTn clock.
|
|
| void | CMU_CalibrateCont (bool enable) |
|
Configure continuous calibration mode.
|
|
| void | CMU_CalibrateStart (void) |
|
Start calibration.
|
|
| void | CMU_CalibrateStop (void) |
|
Stop the calibration counters.
|
|
| uint32_t | CMU_DivToLog2 ( CMU_ClkDiv_TypeDef div) |
|
Convert dividend to logarithmic value.
|
|
| void | CMU_IntClear (uint32_t flags) |
|
Clear one or more pending CMU interrupts.
|
|
| void | CMU_IntDisable (uint32_t flags) |
|
Disable one or more CMU interrupts.
|
|
| void | CMU_IntEnable (uint32_t flags) |
|
Enable one or more CMU interrupts.
|
|
| uint32_t | CMU_IntGet (void) |
|
Get pending CMU interrupts.
|
|
| uint32_t | CMU_IntGetEnabled (void) |
|
Get enabled and pending CMU interrupt flags.
|
|
| void | CMU_IntSet (uint32_t flags) |
|
Set one or more pending CMU interrupts.
|
|
| void | CMU_Lock (void) |
|
Lock the CMU to protect some of its registers against unintended modification.
|
|
| SL_DEPRECATED_API_SDK_4_1 uint32_t | CMU_Log2ToDiv (uint32_t log2) |
|
Convert logarithm of 2 prescaler to division factor.
|
|
| void | CMU_Unlock (void) |
|
Unlock the CMU so that writing to locked registers again is possible.
|
|
Macros |
|
| #define | cmuClkDiv_1 1 |
|
Clock divisors.
|
|
| #define | cmuClkDiv_2 2 |
|
Divide clock by 2.
|
|
| #define | cmuClkDiv_4 4 |
|
Divide clock by 4.
|
|
| #define | cmuClkDiv_8 8 |
|
Divide clock by 8.
|
|
| #define | cmuClkDiv_16 16 |
|
Divide clock by 16.
|
|
| #define | cmuClkDiv_32 32 |
|
Divide clock by 32.
|
|
| #define | cmuClkDiv_64 64 |
|
Divide clock by 64.
|
|
| #define | cmuClkDiv_128 128 |
|
Divide clock by 128.
|
|
| #define | cmuClkDiv_256 256 |
|
Divide clock by 256.
|
|
| #define | cmuClkDiv_512 512 |
|
Divide clock by 512.
|
|
| #define | cmuClkDiv_1024 1024 |
|
Divide clock by 1024.
|
|
| #define | cmuClkDiv_2048 2048 |
|
Divide clock by 2048.
|
|
| #define | cmuClkDiv_4096 4096 |
|
Divide clock by 4096.
|
|
| #define | cmuClkDiv_8192 8192 |
|
Divide clock by 8192.
|
|
| #define | cmuClkDiv_16384 16384 |
|
Divide clock by 16384.
|
|
| #define | cmuClkDiv_32768 32768 |
|
Divide clock by 32768.
|
|
| #define | CMU_LFXOINIT_DEFAULT |
|
Default LFXO initialization values.
|
|
| #define | CMU_LFXOINIT_EXTERNAL_CLOCK |
|
Default LFXO initialization for external clock.
|
|
| #define | CMU_HFXOINIT_DEFAULT |
|
Default HFXO initialization values for Platform 1 devices.
|
|
| #define | CMU_HFXOINIT_EXTERNAL_CLOCK |
|
Default HFXO initialization for external clock.
|
|
Typedefs |
|
| typedef uint32_t | CMU_ClkDiv_TypeDef |
|
Clock divider configuration.
|
|
Function Documentation
◆ CMU_UpdateWaitStates()
| void CMU_UpdateWaitStates | ( | uint32_t |
freq,
|
| int |
vscale
|
||
| ) |
Configure various wait states to switch to a certain frequency and a certain voltage scale.
This function will set up the necessary flash, bus, and RAM wait states. Updating the wait state configuration must be done before increasing the clock frequency and it must be done after decreasing the clock frequency. Updating the wait state configuration must be done before core voltage is decreased and it must be done after a core voltage is increased.
- Parameters
-
[in] freqThe core clock frequency to configure wait-states. [in] vscaleThe voltage scale to configure wait-states. Expected values are 0 or 2, higher number is lower voltage.
- 0 = 1.2 V (VSCALE2)
- 2 = 1.0 V (VSCALE0)
◆ syncReg()
|
inline |
Wait for an ongoing sync of register(s) to low-frequency domain to complete.
- Parameters
-
[in] maskA bitmask corresponding to SYNCBUSY register defined bits, indicating registers that must complete any ongoing synchronization.
◆ CMU_AUXHFRCOBandGet()
| CMU_AUXHFRCOBand_TypeDef CMU_AUXHFRCOBandGet | ( | void |
|
) |
Get the AUXHFRCO band in use.
- Returns
- AUXHFRCO band in use.
◆ CMU_AUXHFRCOBandSet()
| void CMU_AUXHFRCOBandSet | ( | CMU_AUXHFRCOBand_TypeDef |
band
|
) |
Set the AUXHFRCO band and the tuning value based on the value in the calibration table made during production.
- Parameters
-
[in] bandAUXHFRCO band to activate.
◆ CMU_Calibrate()
| uint32_t CMU_Calibrate | ( | uint32_t |
HFCycles,
|
| CMU_Osc_TypeDef |
reference
|
||
| ) |
Calibrate the clock.
Run a calibration for HFCLK against a selectable reference clock. See the reference manual, CMU chapter, for more details.
- Note
- This function will not return until the calibration measurement is completed.
- Parameters
-
[in] HFCyclesThe number of HFCLK cycles to run the calibration. Increasing this number increases precision but the calibration will take more time. [in] referenceThe reference clock used to compare HFCLK.
- Returns
- The number of ticks the reference clock after HFCycles ticks on the HF clock.
◆ CMU_CalibrateConfig()
| void CMU_CalibrateConfig | ( | uint32_t |
downCycles,
|
| CMU_Osc_TypeDef |
downSel,
|
||
| CMU_Osc_TypeDef |
upSel
|
||
| ) |
Configure the clock calibration.
Configure a calibration for a selectable clock source against another selectable reference clock. See the reference manual, CMU chapter, for more details.
- Note
- After configuration, a call to CMU_CalibrateStart() is required and the resulting calibration value can be read out with the CMU_CalibrateCountGet() function call.
- Parameters
-
[in] downCyclesThe number of downSel clock cycles to run the calibration. Increasing this number increases precision but the calibration will take more time. [in] downSelThe clock, which will be counted down downCycles. [in] upSelThe reference clock; the number of cycles generated by this clock will be counted and added up and the result can be given with the CMU_CalibrateCountGet() function call.
◆ CMU_CalibrateCountGet()
| uint32_t CMU_CalibrateCountGet | ( | void |
|
) |
Get the calibration count register.
- Note
- If continuous calibration mode is active, calibration busy will almost always be off and only the value needs to be read. In a normal case, this function call is triggered by the CALRDY interrupt flag.
- Returns
- The calibration count, the number of UPSEL clocks in the period of DOWNSEL oscillator clock cycles configured by a previous write operation to CMU->CALCNT.
◆ CMU_ClockDivGet()
| CMU_ClkDiv_TypeDef CMU_ClockDivGet | ( | CMU_Clock_TypeDef |
clock
|
) |
Get the clock divisor/prescaler.
- Parameters
-
[in] clockA clock point to get the divisor/prescaler for. Notice that not all clock points have a divisor/prescaler. See the CMU overview in the reference manual.
- Returns
-
The current clock point divisor/prescaler. 1 is returned if
clockspecifies a clock point without a divisor/prescaler.
◆ CMU_ClockDivSet()
| void CMU_ClockDivSet | ( | CMU_Clock_TypeDef |
clock,
|
| CMU_ClkDiv_TypeDef |
div
|
||
| ) |
Set the clock divisor/prescaler.
- Note
- If setting an LF clock prescaler, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.
HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
- Parameters
-
[in] clockClock point to set divisor/prescaler for. Notice that not all clock points have a divisor/prescaler. See the CMU overview in the reference manual. [in] divThe clock divisor to use (<= cmuClkDiv_512).
◆ CMU_ClockEnable()
| void CMU_ClockEnable | ( | CMU_Clock_TypeDef |
clock,
|
| bool |
enable
|
||
| ) |
Enable/disable a clock.
In general, module clocking is disabled after a reset. If a module clock is disabled, the registers of that module are not accessible and reading from such registers may return undefined values. Writing to registers of clock-disabled modules has no effect. Avoid accessing module registers of a module with a disabled clock.
- Note
- If enabling/disabling an LF clock, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.
HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
- Parameters
-
[in] clockThe clock to enable/disable. Notice that not all defined clock points have separate enable/disable control. See the CMU overview in the reference manual. [in] enable- true - enable specified clock.
- false - disable specified clock.
◆ CMU_ClockFreqGet()
| uint32_t CMU_ClockFreqGet | ( | CMU_Clock_TypeDef |
clock
|
) |
Get the clock frequency for a clock point.
- Parameters
-
[in] clockA clock point to fetch the frequency for.
- Returns
- The current frequency in Hz.
◆ CMU_ClockSelectGet()
| CMU_Select_TypeDef CMU_ClockSelectGet | ( | CMU_Clock_TypeDef |
clock
|
) |
Get the currently selected reference clock used for a clock branch.
- Parameters
-
[in] clockClock branch to fetch selected ref. clock for. One of:
- Returns
-
The reference clock used for clocking the selected branch,
cmuSelect_Error
if invalid
clockprovided.
◆ CMU_ClockSelectSet()
| void CMU_ClockSelectSet | ( | CMU_Clock_TypeDef |
clock,
|
| CMU_Select_TypeDef |
ref
|
||
| ) |
Select the reference clock/oscillator used for a clock branch.
Notice that if a selected reference is not enabled prior to selecting its use, it will be enabled and this function will wait for the selected oscillator to be stable. It will however NOT be disabled if another reference clock is selected later.
This feature is particularly important if selecting a new reference clock for the clock branch clocking the core. Otherwise, the system may halt.
- Note
- HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
- Parameters
-
[in] clockA clock branch to select reference clock for. One of: [in] refA reference selected for clocking. See the reference manual for details about references available for a specific clock branch.
◆ CMU_LF_ClockPrecisionGet()
| uint16_t CMU_LF_ClockPrecisionGet | ( | CMU_Clock_TypeDef |
clock
|
) |
Gets the precision (in PPM) of the specified low frequency clock branch.
- Parameters
-
[in] clockClock branch.
- Returns
- Precision, in PPM, of the specified clock branch.
- Note
- This function is only for internal usage.
- The current implementation of this function is used to determine if the clock has a precision <= 500 ppm or not (which is the minimum required for BLE). Future version of this function should provide more accurate precision numbers to allow for further optimizations from the stacks.
◆ CMU_FreezeEnable()
| void CMU_FreezeEnable | ( | bool |
enable
|
) |
CMU low frequency register synchronization freeze control.
Some CMU registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several such registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).
Another use case for this feature is using an API (such as the CMU API) for modifying several bit fields consecutively in the same register. If freeze mode is enabled during this sequence, stalling can be avoided.
- Note
- When enabling freeze mode, this function will wait for all current ongoing CMU synchronization to LF domain to complete (normally synchronization will not be in progress.) However, for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling.
- Parameters
-
[in] enable- true - enable freeze, modified registers are not propagated to the LF domain
- false - disable freeze, modified registers are propagated to the LF domain
◆ CMU_HFRCOBandGet()
| CMU_HFRCOBand_TypeDef CMU_HFRCOBandGet | ( | void |
|
) |
Get HFRCO band in use.
- Returns
- HFRCO band in use.
◆ CMU_HFRCOBandSet()
| void CMU_HFRCOBandSet | ( | CMU_HFRCOBand_TypeDef |
band
|
) |
Set HFRCO band and the tuning value based on the value in the calibration table made during production.
- Note
- HFCLKLE prescaler is automatically modified based on the maximum HFLE frequency allowed.
- Parameters
-
[in] bandHFRCO band to activate.
◆ CMU_HFRCOStartupDelayGet()
| uint32_t CMU_HFRCOStartupDelayGet | ( | void |
|
) |
Get the HFRCO startup delay.
See the reference manual for more details.
- Returns
- The startup delay in use.
◆ CMU_HFRCOStartupDelaySet()
| void CMU_HFRCOStartupDelaySet | ( | uint32_t |
delay
|
) |
Set the HFRCO startup delay.
See the reference manual for more details.
- Parameters
-
[in] delayThe startup delay to set (<= 31).
◆ CMU_HFXOInit()
| void CMU_HFXOInit | ( | const CMU_HFXOInit_TypeDef * |
hfxoInit
|
) |
Set HFXO control registers.
- Note
- HFXO configuration should be obtained from a configuration tool, app note, or crystal data sheet. This function disables the HFXO to ensure a valid state before update.
- Parameters
-
[in] hfxoInitHFXO setup parameters.
◆ CMU_LCDClkFDIVGet()
| uint32_t CMU_LCDClkFDIVGet | ( | void |
|
) |
Get the LCD framerate divisor (FDIV) setting.
- Returns
- The LCD framerate divisor.
◆ CMU_LCDClkFDIVSet()
| void CMU_LCDClkFDIVSet | ( | uint32_t |
div
|
) |
Set the LCD framerate divisor (FDIV) setting.
- Note
- The FDIV field (CMU LCDCTRL register) should only be modified while the LCD module is clock disabled (CMU LFACLKEN0.LCD bit is 0). This function will NOT modify FDIV if the LCD module clock is enabled. See CMU_ClockEnable() for disabling/enabling LCD clock.
- Parameters
-
[in] divThe FDIV setting to use.
◆ CMU_LFXOInit()
| void CMU_LFXOInit | ( | const CMU_LFXOInit_TypeDef * |
lfxoInit
|
) |
Set LFXO control registers.
- Note
- LFXO configuration should be obtained from a configuration tool, app note, or crystal data sheet. This function disables the LFXO when necessary to ensure a valid state before update.
- Parameters
-
[in] lfxoInitLFXO setup parameters.
◆ CMU_LFXOPrecisionSet()
| void CMU_LFXOPrecisionSet | ( | uint16_t |
precision
|
) |
Sets LFXO's crystal precision, in PPM.
- Note
- LFXO precision should be obtained from a crystal datasheet.
- Parameters
-
[in] precisionLFXO's crystal precision, in PPM.
◆ CMU_OscillatorEnable()
| void CMU_OscillatorEnable | ( | CMU_Osc_TypeDef |
osc,
|
| bool |
enable,
|
||
| bool |
wait
|
||
| ) |
Enable/disable oscillator.
- Note
- WARNING: When this function is called to disable either cmuOsc_LFXO or cmuOsc_HFXO, the LFXOMODE or HFXOMODE fields of the CMU_CTRL register are reset to the reset value. In other words, if external clock sources are selected in either LFXOMODE or HFXOMODE fields, the configuration will be cleared and needs to be reconfigured if needed later.
- Parameters
-
[in] oscThe oscillator to enable/disable. [in] enable- true - enable specified oscillator.
- false - disable specified oscillator.
[in] waitOnly used if enableis true.- true - wait for oscillator start-up time to timeout before returning.
- false - do not wait for oscillator start-up time to timeout before returning.
◆ CMU_OscillatorTuningGet()
| uint32_t CMU_OscillatorTuningGet | ( | CMU_Osc_TypeDef |
osc
|
) |
Get the oscillator frequency tuning setting.
- Parameters
-
[in] oscAn oscillator to get tuning value for, one of the following: - cmuOsc_LFRCO
- cmuOsc_HFRCO
- cmuOsc_AUXHFRCO
- cmuOsc_HFXO if CMU_HFXOCTRL_PEAKDETSHUNTOPTMODE is defined
- Returns
- The oscillator frequency tuning setting in use.
◆ CMU_OscillatorTuningSet()
| void CMU_OscillatorTuningSet | ( | CMU_Osc_TypeDef |
osc,
|
| uint32_t |
val
|
||
| ) |
Set the oscillator frequency tuning control.
- Note
- Oscillator tuning is done during production and the tuning value is automatically loaded after reset. Changing the tuning value from the calibrated value is for more advanced use. Certain oscillators also have build-in tuning optimization.
- Parameters
-
[in] oscAn oscillator to set tuning value for, one of the following: - cmuOsc_LFRCO
- cmuOsc_HFRCO
- cmuOsc_AUXHFRCO
- cmuOsc_HFXO if PEAKDETSHUNTOPTMODE is available. Note that CMD mode is set.
[in] valThe oscillator frequency tuning setting to use.
◆ CMU_PCNTClockExternalGet()
| bool CMU_PCNTClockExternalGet | ( | unsigned int |
instance
|
) |
Determine if the currently selected PCNTn clock used is external or LFBCLK.
- Parameters
-
[in] instancePCNT instance number to get currently selected clock source for.
- Returns
-
- true - selected clock is external clock.
- false - selected clock is LFBCLK.
◆ CMU_PCNTClockExternalSet()
| void CMU_PCNTClockExternalSet | ( | unsigned int |
instance,
|
| bool |
external
|
||
| ) |
Select the PCNTn clock.
- Parameters
-
[in] instancePCNT instance number to set selected clock source for. [in] externalSet to true to select the external clock, false to select LFBCLK.
◆ CMU_CalibrateCont()
|
inline |
Configure continuous calibration mode.
- Parameters
-
[in] enableIf true, enables continuous calibration, if false disables continuous calibration.
◆ CMU_CalibrateStart()
|
inline |
Start calibration.
- Note
- This call is usually invoked after CMU_CalibrateConfig() and possibly CMU_CalibrateCont() .
◆ CMU_CalibrateStop()
|
inline |
Stop the calibration counters.
◆ CMU_DivToLog2()
|
inline |
Convert dividend to logarithmic value.
It only works for even numbers equal to 2^n.
- Parameters
-
[in] divAn unscaled dividend.
- Returns
- Logarithm of 2, as used by fixed prescalers.
◆ CMU_IntClear()
|
inline |
Clear one or more pending CMU interrupts.
- Parameters
-
[in] flagsCMU interrupt sources to clear.
◆ CMU_IntDisable()
|
inline |
Disable one or more CMU interrupts.
- Parameters
-
[in] flagsCMU interrupt sources to disable.
◆ CMU_IntEnable()
|
inline |
Enable one or more CMU interrupts.
- Note
- Depending on use case, a pending interrupt may already be set prior to enabling the interrupt. Consider using CMU_IntClear() prior to enabling if the pending interrupt should be ignored.
- Parameters
-
[in] flagsCMU interrupt sources to enable.
◆ CMU_IntGet()
|
inline |
Get pending CMU interrupts.
- Returns
- CMU interrupt sources pending.
◆ CMU_IntGetEnabled()
|
inline |
Get enabled and pending CMU interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- This function does not clear event bits.
- Returns
-
Pending and enabled CMU interrupt sources. The return value is the bitwise AND of
- the enabled interrupt sources in CMU_IEN and
- the pending interrupt flags CMU_IF
◆ CMU_IntSet()
|
inline |
Set one or more pending CMU interrupts.
- Parameters
-
[in] flagsCMU interrupt sources to set to pending.
◆ CMU_Lock()
|
inline |
Lock the CMU to protect some of its registers against unintended modification.
See the reference manual for CMU registers that will be locked.
- Note
- If locking the CMU registers, they must be unlocked prior to using any CMU API functions modifying CMU registers protected by the lock.
◆ CMU_Log2ToDiv()
|
inline |
Convert logarithm of 2 prescaler to division factor.
- Parameters
-
[in] log2Logarithm of 2, as used by fixed prescalers.
- Returns
- Dividend.
◆ CMU_Unlock()
|
inline |
Unlock the CMU so that writing to locked registers again is possible.
Macro Definition Documentation
◆ cmuClkDiv_1
| #define cmuClkDiv_1 1 |
Clock divisors.
These values are valid for prescalers. Divide clock by 1.
◆ cmuClkDiv_2
| #define cmuClkDiv_2 2 |
Divide clock by 2.
◆ cmuClkDiv_4
| #define cmuClkDiv_4 4 |
Divide clock by 4.
◆ cmuClkDiv_8
| #define cmuClkDiv_8 8 |
Divide clock by 8.
◆ cmuClkDiv_16
| #define cmuClkDiv_16 16 |
Divide clock by 16.
◆ cmuClkDiv_32
| #define cmuClkDiv_32 32 |
Divide clock by 32.
◆ cmuClkDiv_64
| #define cmuClkDiv_64 64 |
Divide clock by 64.
◆ cmuClkDiv_128
| #define cmuClkDiv_128 128 |
Divide clock by 128.
◆ cmuClkDiv_256
| #define cmuClkDiv_256 256 |
Divide clock by 256.
◆ cmuClkDiv_512
| #define cmuClkDiv_512 512 |
Divide clock by 512.
◆ cmuClkDiv_1024
| #define cmuClkDiv_1024 1024 |
Divide clock by 1024.
◆ cmuClkDiv_2048
| #define cmuClkDiv_2048 2048 |
Divide clock by 2048.
◆ cmuClkDiv_4096
| #define cmuClkDiv_4096 4096 |
Divide clock by 4096.
◆ cmuClkDiv_8192
| #define cmuClkDiv_8192 8192 |
Divide clock by 8192.
◆ cmuClkDiv_16384
| #define cmuClkDiv_16384 16384 |
Divide clock by 16384.
◆ cmuClkDiv_32768
| #define cmuClkDiv_32768 32768 |
Divide clock by 32768.
◆ CMU_LFXOINIT_DEFAULT
| #define CMU_LFXOINIT_DEFAULT |
Default LFXO initialization values.
◆ CMU_LFXOINIT_EXTERNAL_CLOCK
| #define CMU_LFXOINIT_EXTERNAL_CLOCK |
Default LFXO initialization for external clock.
◆ CMU_HFXOINIT_DEFAULT
| #define CMU_HFXOINIT_DEFAULT |
Default HFXO initialization values for Platform 1 devices.
◆ CMU_HFXOINIT_EXTERNAL_CLOCK
| #define CMU_HFXOINIT_EXTERNAL_CLOCK |
Default HFXO initialization for external clock.
Typedef Documentation
◆ CMU_ClkDiv_TypeDef
| typedef uint32_t CMU_ClkDiv_TypeDef |
Clock divider configuration.
Enumeration Type Documentation
◆ CMU_HFRCOBand_TypeDef
◆ CMU_AUXHFRCOBand_TypeDef
◆ CMU_Clock_TypeDef
| enum CMU_Clock_TypeDef |
Clock points in CMU.
See CMU overview in the reference manual.
◆ CMU_Osc_TypeDef
| enum CMU_Osc_TypeDef |
Oscillator types.
◆ CMU_OscMode_TypeDef
| enum CMU_OscMode_TypeDef |
◆ CMU_Select_TypeDef
| enum CMU_Select_TypeDef |
Selectable clock sources.
◆ CMU_LFXOBoost_TypeDef
LFXO Boost values.