Key attributes
Description
Functions | |
psa_status_t | psa_get_key_attributes (mbedtls_svc_key_id_t key, psa_key_attributes_t *attributes) |
Retrieve the attributes of a key. | |
void | psa_reset_key_attributes (psa_key_attributes_t *attributes) |
Reset a key attribute structure to a freshly initialized state. | |
psa_status_t | psa_set_key_domain_parameters (psa_key_attributes_t *attributes, psa_key_type_t type, const uint8_t *data, size_t data_length) |
Set domain parameters for a key. | |
psa_status_t | psa_get_key_domain_parameters (const psa_key_attributes_t *attributes, uint8_t *data, size_t data_size, size_t *data_length) |
Get domain parameters for a key. | |
Macros | |
#define | PSA_KEY_ATTRIBUTES_INIT { PSA_CORE_KEY_ATTRIBUTES_INIT, NULL, 0 } |
#define | PSA_DH_FAMILY_CUSTOM ((psa_dh_family_t) 0x7e) |
Custom Diffie-Hellman group. | |
#define | PSA_KEY_DOMAIN_PARAMETERS_SIZE(key_type, key_bits) |
Safe output buffer size for psa_get_key_domain_parameters(). | |
#define | PSA_DH_KEY_DOMAIN_PARAMETERS_SIZE(key_bits) (4 + (PSA_BITS_TO_BYTES(key_bits) + 5) * 3 /*without optional parts*/) |
#define | PSA_DSA_KEY_DOMAIN_PARAMETERS_SIZE(key_bits) (4 + (PSA_BITS_TO_BYTES(key_bits) + 5) * 2 /*p, g*/ + 34 /*q*/) |
Function Documentation
◆ psa_get_key_attributes()
psa_status_t psa_get_key_attributes | ( | mbedtls_svc_key_id_t | key, |
psa_key_attributes_t * | attributes |
||
) |
Retrieve the attributes of a key.
This function first resets the attribute structure as with psa_reset_key_attributes(). It then copies the attributes of the given key into the given attribute structure.
- Note
- This function may allocate memory or other resources. Once you have called this function on an attribute structure, you must call psa_reset_key_attributes() to free these resources.
- Parameters
-
[in] key
Identifier of the key to query. [in,out] attributes
On success, the attributes of the key. On failure, equivalent to a freshly-initialized structure.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_DATA_CORRUPT
PSA_ERROR_DATA_INVALID
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
◆ psa_reset_key_attributes()
void psa_reset_key_attributes | ( | psa_key_attributes_t * | attributes | ) |
Reset a key attribute structure to a freshly initialized state.
You must initialize the attribute structure as described in the documentation of the type #psa_key_attributes_t before calling this function. Once the structure has been initialized, you may call this function at any time.
This function frees any auxiliary resources that the structure may contain.
- Parameters
-
[in,out] attributes
The attribute structure to reset.
◆ psa_set_key_domain_parameters()
psa_status_t psa_set_key_domain_parameters | ( | psa_key_attributes_t * | attributes, |
psa_key_type_t | type, |
||
const uint8_t * | data, |
||
size_t | data_length |
||
) |
Set domain parameters for a key.
Some key types require additional domain parameters in addition to the key type identifier and the key size. Use this function instead of psa_set_key_type() when you need to specify domain parameters.
The format for the required domain parameters varies based on the key type.
- For RSA keys (PSA_KEY_TYPE_RSA_PUBLIC_KEY or PSA_KEY_TYPE_RSA_KEY_PAIR), the domain parameter data consists of the public exponent, represented as a big-endian integer with no leading zeros. This information is used when generating an RSA key pair. When importing a key, the public exponent is read from the imported key data and the exponent recorded in the attribute structure is ignored. As an exception, the public exponent 65537 is represented by an empty byte string.
- For DSA keys (PSA_KEY_TYPE_DSA_PUBLIC_KEY or PSA_KEY_TYPE_DSA_KEY_PAIR), the
Dss-Parms
format as defined by RFC 3279 §2.3.2.Dss-Parms ::= SEQUENCE {p INTEGER,q INTEGER,g INTEGER} - For Diffie-Hellman key exchange keys (PSA_KEY_TYPE_DH_PUBLIC_KEY(PSA_DH_FAMILY_CUSTOM) or PSA_KEY_TYPE_DH_KEY_PAIR(PSA_DH_FAMILY_CUSTOM)), the
DomainParameters
format as defined by RFC 3279 §2.3.3.DomainParameters ::= SEQUENCE {p INTEGER, -- odd prime, p=jq +1g INTEGER, -- generator, gq INTEGER, -- factor of p-1j INTEGER OPTIONAL, -- subgroup factorvalidationParms ValidationParms OPTIONAL}ValidationParms ::= SEQUENCE {seed BIT STRING,pgenCounter INTEGER}
- Note
- This function may allocate memory or other resources. Once you have called this function on an attribute structure, you must call psa_reset_key_attributes() to free these resources.
- This is an experimental extension to the interface. It may change in future versions of the library.
- Parameters
-
[in,out] attributes
Attribute structure where the specified domain parameters will be stored. If this function fails, the content of attributes
is not modified.type
Key type (a PSA_KEY_TYPE_XXX
value).[in] data
Buffer containing the key domain parameters. The content of this buffer is interpreted according to type
as described above.data_length
Size of the data
buffer in bytes.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INSUFFICIENT_MEMORY
◆ psa_get_key_domain_parameters()
psa_status_t psa_get_key_domain_parameters | ( | const psa_key_attributes_t * | attributes, |
uint8_t * | data, |
||
size_t | data_size, |
||
size_t * | data_length |
||
) |
Get domain parameters for a key.
Get the domain parameters for a key with this function, if any. The format of the domain parameters written to data
is specified in the documentation for psa_set_key_domain_parameters().
- Note
- This is an experimental extension to the interface. It may change in future versions of the library.
- Parameters
-
[in] attributes
The key attribute structure to query. [out] data
On success, the key domain parameters. data_size
Size of the data
buffer in bytes. The buffer is guaranteed to be large enough if its size in bytes is at least the value given by PSA_KEY_DOMAIN_PARAMETERS_SIZE().[out] data_length
On success, the number of bytes that make up the key domain parameters data.
- Return values
-
PSA_SUCCESS
PSA_ERROR_BUFFER_TOO_SMALL
Macro Definition Documentation
◆ PSA_KEY_ATTRIBUTES_INIT
#define PSA_KEY_ATTRIBUTES_INIT { PSA_CORE_KEY_ATTRIBUTES_INIT, NULL, 0 } |
This macro returns a suitable initializer for a key attribute structure of type #psa_key_attributes_t.
◆ PSA_DH_FAMILY_CUSTOM
#define PSA_DH_FAMILY_CUSTOM ((psa_dh_family_t) 0x7e) |
Custom Diffie-Hellman group.
For keys of type PSA_KEY_TYPE_DH_PUBLIC_KEY(PSA_DH_FAMILY_CUSTOM) or PSA_KEY_TYPE_DH_KEY_PAIR(PSA_DH_FAMILY_CUSTOM), the group data comes from domain parameters set by psa_set_key_domain_parameters().
◆ PSA_KEY_DOMAIN_PARAMETERS_SIZE
#define PSA_KEY_DOMAIN_PARAMETERS_SIZE | ( | key_type, |
|
key_bits |
|||
) |
Safe output buffer size for psa_get_key_domain_parameters().
This macro returns a compile-time constant if its arguments are compile-time constants.
- Warning
- This function may call its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
- Note
- This is an experimental extension to the interface. It may change in future versions of the library.
- Parameters
-
key_type
A supported key type. key_bits
The size of the key in bits.
- Returns
- If the parameters are valid and supported, return a buffer size in bytes that guarantees that psa_get_key_domain_parameters() will not fail with PSA_ERROR_BUFFER_TOO_SMALL. If the parameters are a valid combination that is not supported by the implementation, this macro shall return either a sensible size or 0. If the parameters are not valid, the return value is unspecified.