Key derivation
Description
Macros | |
#define | PSA_KEY_DERIVATION_INPUT_SECRET ((psa_key_derivation_step_t)0x0101) |
A secret input for key derivation. | |
#define | PSA_KEY_DERIVATION_INPUT_PASSWORD ((psa_key_derivation_step_t)0x0102) |
A low-entropy secret input for password hashing / key stretching. | |
#define | PSA_KEY_DERIVATION_INPUT_LABEL ((psa_key_derivation_step_t)0x0201) |
A label for key derivation. | |
#define | PSA_KEY_DERIVATION_INPUT_SALT ((psa_key_derivation_step_t)0x0202) |
A salt for key derivation. | |
#define | PSA_KEY_DERIVATION_INPUT_INFO ((psa_key_derivation_step_t)0x0203) |
An information string for key derivation. | |
#define | PSA_KEY_DERIVATION_INPUT_SEED ((psa_key_derivation_step_t)0x0204) |
A seed for key derivation. | |
#define | PSA_KEY_DERIVATION_INPUT_COST ((psa_key_derivation_step_t)0x0205) |
A cost parameter for password hashing / key stretching. | |
Typedefs | |
typedef uint16_t | psa_key_derivation_step_t |
Encoding of the step of a key derivation. | |
Macro Definition Documentation
◆ PSA_KEY_DERIVATION_INPUT_SECRET
#define PSA_KEY_DERIVATION_INPUT_SECRET ((psa_key_derivation_step_t)0x0101) |
A secret input for key derivation.
This should be a key of type PSA_KEY_TYPE_DERIVE (passed to psa_key_derivation_input_key()) or the shared secret resulting from a key agreement (obtained via psa_key_derivation_key_agreement()).
The secret can also be a direct input (passed to key_derivation_input_bytes()). In this case, the derivation operation may not be used to derive keys: the operation will only allow psa_key_derivation_output_bytes(), psa_key_derivation_verify_bytes(), or psa_key_derivation_verify_key(), but not psa_key_derivation_output_key().
◆ PSA_KEY_DERIVATION_INPUT_PASSWORD
#define PSA_KEY_DERIVATION_INPUT_PASSWORD ((psa_key_derivation_step_t)0x0102) |
A low-entropy secret input for password hashing / key stretching.
This is usually a key of type PSA_KEY_TYPE_PASSWORD (passed to psa_key_derivation_input_key()) or a direct input (passed to psa_key_derivation_input_bytes()) that is a password or passphrase. It can also be high-entropy secret such as a key of type PSA_KEY_TYPE_DERIVE or the shared secret resulting from a key agreement.
The secret can also be a direct input (passed to key_derivation_input_bytes()). In this case, the derivation operation may not be used to derive keys: the operation will only allow psa_key_derivation_output_bytes(), psa_key_derivation_verify_bytes(), or psa_key_derivation_verify_key(), but not psa_key_derivation_output_key().
◆ PSA_KEY_DERIVATION_INPUT_LABEL
#define PSA_KEY_DERIVATION_INPUT_LABEL ((psa_key_derivation_step_t)0x0201) |
A label for key derivation.
This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA.
◆ PSA_KEY_DERIVATION_INPUT_SALT
#define PSA_KEY_DERIVATION_INPUT_SALT ((psa_key_derivation_step_t)0x0202) |
A salt for key derivation.
This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA or PSA_KEY_TYPE_PEPPER.
◆ PSA_KEY_DERIVATION_INPUT_INFO
#define PSA_KEY_DERIVATION_INPUT_INFO ((psa_key_derivation_step_t)0x0203) |
An information string for key derivation.
This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA.
◆ PSA_KEY_DERIVATION_INPUT_SEED
#define PSA_KEY_DERIVATION_INPUT_SEED ((psa_key_derivation_step_t)0x0204) |
A seed for key derivation.
This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA.
◆ PSA_KEY_DERIVATION_INPUT_COST
#define PSA_KEY_DERIVATION_INPUT_COST ((psa_key_derivation_step_t)0x0205) |
A cost parameter for password hashing / key stretching.
This must be a direct input, passed to psa_key_derivation_input_integer().
Typedef Documentation
◆ psa_key_derivation_step_t
typedef uint16_t psa_key_derivation_step_t |
Encoding of the step of a key derivation.