sl_se_gcm_streaming_context_t Struct Reference
GCM streaming context. Deprecated.
#include <sl_se_manager_types.h>
Data Fields | |
sl_se_command_context_t * | cmd_ctx |
Pointer to command context object. | |
const sl_se_key_descriptor_t * | key |
Pointer to key object. | |
uint64_t | len |
Total length of the encrypted data. | |
uint64_t | add_len |
Total length of the additional data. | |
uint8_t | se_ctx_enc [32] |
SE encryption state. | |
uint8_t | se_ctx_dec [32] |
SE decryption state. | |
uint8_t | tagbuf [16] |
Tag. | |
int | mode |
GCM mode. | |
bool | last_op |
Last operation / update. | |
GCM streaming context. Deprecated.
Field Documentation
◆ cmd_ctx
sl_se_command_context_t* sl_se_gcm_streaming_context_t::cmd_ctx |
Pointer to command context object.
◆ key
const sl_se_key_descriptor_t* sl_se_gcm_streaming_context_t::key |
Pointer to key object.
◆ len
uint64_t sl_se_gcm_streaming_context_t::len |
Total length of the encrypted data.
◆ add_len
uint64_t sl_se_gcm_streaming_context_t::add_len |
Total length of the additional data.
◆ se_ctx_enc
uint8_t sl_se_gcm_streaming_context_t::se_ctx_enc[32] |
SE encryption state.
◆ se_ctx_dec
uint8_t sl_se_gcm_streaming_context_t::se_ctx_dec[32] |
SE decryption state.
◆ tagbuf
uint8_t sl_se_gcm_streaming_context_t::tagbuf[16] |
Tag.
◆ mode
int sl_se_gcm_streaming_context_t::mode |
GCM mode.
◆ last_op
bool sl_se_gcm_streaming_context_t::last_op |
Last operation / update.