sl_cpc_core_debug_counters_t Struct Reference
Struct representing CPC Core debug counters.
#include <sl_cpc.h>
Data Fields | |
uint32_t | endpoint_opened |
Number of endpoint opened. | |
uint32_t | endpoint_closed |
Number of endpoint closed. | |
uint32_t | rxd_frame |
Total number of frame received. | |
uint32_t | rxd_valid_iframe |
Total number of i-frame received. | |
uint32_t | rxd_valid_uframe |
Total number of u-frame received. | |
uint32_t | rxd_valid_sframe |
Total number of s-frame received. | |
uint32_t | rxd_data_frame_dropped |
Total number of frame dropped. | |
uint32_t | txd_reject_destination_unreachable |
Total number of unreachable destination transmisted. | |
uint32_t | txd_reject_error_fault |
Total number of fault transmisted. | |
uint32_t | txd_completed |
Total number of frame confirmed sent by the driver. | |
uint32_t | retxd_data_frame |
Total number of dataframe retransmission. | |
uint32_t | driver_error |
Total number of error reported by the driver. | |
uint32_t | driver_packet_dropped |
Total number of frame dropped by the driver. | |
uint32_t | invalid_header_checksum |
Total number of frame received with invalid header checksum. | |
uint32_t | invalid_payload_checksum |
Total number of frame received with invalid frame checksum. | |
Struct representing CPC Core debug counters.
Field Documentation
◆ endpoint_opened
uint32_t sl_cpc_core_debug_counters_t::endpoint_opened |
Number of endpoint opened.
◆ endpoint_closed
uint32_t sl_cpc_core_debug_counters_t::endpoint_closed |
Number of endpoint closed.
◆ rxd_frame
uint32_t sl_cpc_core_debug_counters_t::rxd_frame |
Total number of frame received.
◆ rxd_valid_iframe
uint32_t sl_cpc_core_debug_counters_t::rxd_valid_iframe |
Total number of i-frame received.
◆ rxd_valid_uframe
uint32_t sl_cpc_core_debug_counters_t::rxd_valid_uframe |
Total number of u-frame received.
◆ rxd_valid_sframe
uint32_t sl_cpc_core_debug_counters_t::rxd_valid_sframe |
Total number of s-frame received.
◆ rxd_data_frame_dropped
uint32_t sl_cpc_core_debug_counters_t::rxd_data_frame_dropped |
Total number of frame dropped.
◆ txd_reject_destination_unreachable
uint32_t sl_cpc_core_debug_counters_t::txd_reject_destination_unreachable |
Total number of unreachable destination transmisted.
◆ txd_reject_error_fault
uint32_t sl_cpc_core_debug_counters_t::txd_reject_error_fault |
Total number of fault transmisted.
◆ txd_completed
uint32_t sl_cpc_core_debug_counters_t::txd_completed |
Total number of frame confirmed sent by the driver.
◆ retxd_data_frame
uint32_t sl_cpc_core_debug_counters_t::retxd_data_frame |
Total number of dataframe retransmission.
◆ driver_error
uint32_t sl_cpc_core_debug_counters_t::driver_error |
Total number of error reported by the driver.
◆ driver_packet_dropped
uint32_t sl_cpc_core_debug_counters_t::driver_packet_dropped |
Total number of frame dropped by the driver.
◆ invalid_header_checksum
uint32_t sl_cpc_core_debug_counters_t::invalid_header_checksum |
Total number of frame received with invalid header checksum.
◆ invalid_payload_checksum
uint32_t sl_cpc_core_debug_counters_t::invalid_payload_checksum |
Total number of frame received with invalid frame checksum.