sl_sleeptimer_timer_handle_t Struct Reference
Timer structure for sleeptimer.
#include <sl_sleeptimer.h>
Data Fields | |
void * | callback_data |
User data to pass to callback function. | |
uint8_t | priority |
Priority of timer. | |
uint16_t | option_flags |
Option flags. | |
sl_sleeptimer_timer_handle_t * | next |
Pointer to next element in list. | |
sl_sleeptimer_timer_callback_t | callback |
Function to call when timer expires. | |
uint32_t | timeout_periodic |
Periodic timeout. | |
uint32_t | delta |
Delay relative to previous element in list. | |
uint32_t | timeout_expected_tc |
Expected tick count of the next timeout (only used for periodic timer). | |
Timer structure for sleeptimer.
Field Documentation
◆ callback_data
void* sl_sleeptimer_timer_handle_t::callback_data |
User data to pass to callback function.
◆ priority
uint8_t sl_sleeptimer_timer_handle_t::priority |
Priority of timer.
◆ option_flags
uint16_t sl_sleeptimer_timer_handle_t::option_flags |
Option flags.
◆ next
sl_sleeptimer_timer_handle_t* sl_sleeptimer_timer_handle_t::next |
Pointer to next element in list.
◆ callback
sl_sleeptimer_timer_callback_t sl_sleeptimer_timer_handle_t::callback |
Function to call when timer expires.
◆ timeout_periodic
uint32_t sl_sleeptimer_timer_handle_t::timeout_periodic |
Periodic timeout.
◆ delta
uint32_t sl_sleeptimer_timer_handle_t::delta |
Delay relative to previous element in list.
◆ timeout_expected_tc
uint32_t sl_sleeptimer_timer_handle_t::timeout_expected_tc |
Expected tick count of the next timeout (only used for periodic timer).