CRYOTIMER_Init_TypeDef Struct Reference
CRYOTIMER initialization structure.
      
       #include <em_cryotimer.h>
      
     
| Data Fields | |
| bool | enable | 
| Enable/disable counting when initialization is complete. | |
| bool | debugRun | 
| Enable/disable timer counting during debug halt. | |
| bool | em4Wakeup | 
| Enable/disable EM4 Wakeup. | |
| CRYOTIMER_Osc_TypeDef | osc | 
| Select the oscillator for the CRYOTIMER. | |
| CRYOTIMER_Presc_TypeDef | presc | 
| Prescaler. | |
| CRYOTIMER_Period_TypeDef | period | 
| A period between a wakeup event/interrupt. | |
CRYOTIMER initialization structure.
Field Documentation
◆ enable
| bool CRYOTIMER_Init_TypeDef::enable | 
Enable/disable counting when initialization is complete.
◆ debugRun
| bool CRYOTIMER_Init_TypeDef::debugRun | 
Enable/disable timer counting during debug halt.
◆ em4Wakeup
| bool CRYOTIMER_Init_TypeDef::em4Wakeup | 
Enable/disable EM4 Wakeup.
◆ osc
| CRYOTIMER_Osc_TypeDef CRYOTIMER_Init_TypeDef::osc | 
Select the oscillator for the CRYOTIMER.
◆ presc
| CRYOTIMER_Presc_TypeDef CRYOTIMER_Init_TypeDef::presc | 
Prescaler.
◆ period
| CRYOTIMER_Period_TypeDef CRYOTIMER_Init_TypeDef::period | 
A period between a wakeup event/interrupt.