DCDC Boost Initialization
Description
Initialize the DC-DC Boost converter.
Configures the DC-DC Boost converter. If the DC-DC Boost converter is not to be used, the configuration option SL_DEVICE_INIT_DCDC_BOOST_ENABLE
can be disabled, and the converter will be powered off.
See AN0948 Power Configurations and DC-DC for further details about DC-DC Boost converter configuration and operation.
- Series 2: AN0948.2
Functions | |
sl_status_t | sl_device_init_dcdc_boost (void) |
Initialize DCDC Boost. | |
Function Documentation
◆ sl_device_init_dcdc_boost()
sl_status_t sl_device_init_dcdc_boost | ( | void |
| ) |
Initialize DCDC Boost.
Configure and start the DCDC Boost
- Returns
- Status code
- Return values
-
SL_STATUS_OK
DC-DC Boost converter initialized successfully