CORE - Core Interrupt
Description
Core interrupt handling API.
- Introduction
- Compile-time Configuration
- Macro API
- API reimplementation
- Interrupt vector tables
- Examples
- Porting from em_int
      
     
Introduction
CORE interrupt API provides a simple and safe means to disable and enable interrupts to protect sections of code.
This is often referred to as "critical sections". This module provides support for three types of critical sections, each with different interrupt blocking capabilities.
- CRITICAL section: Inside a critical section, all interrupts are disabled (except for fault handlers). The PRIMASK register is always used for interrupt disable/enable.
- ATOMIC section: This type of section is configurable and the default method is to use PRIMASK. With BASEPRI configuration, interrupts with priority equal to or lower than a given configurable level are disabled. The interrupt disable priority level is defined at compile time. The BASEPRI register is not available for all architectures.
- NVIC mask section: Disable NVIC (external interrupts) on an individual manner.
em_core also has an API for manipulating RAM-based interrupt vector tables.
      
     
Compile-time Configuration
The following #defines are used to configure em_core:
If the default values do not support your needs, they can be overridden by supplying -D compiler flags on the compiler command line or by collecting all macro redefinitions in a file named emlib_config.h and then supplying -DEMLIB_USER_CONFIG on a compiler command line.
- Note
- The default emlib configuration for ATOMIC section interrupt disable method is using PRIMASK, i.e., ATOMIC sections are implemented as CRITICAL sections.
- Due to architectural limitations Cortex-M0+ devices do not support ATOMIC type critical sections using the BASEPRI register. On M0+ devices ATOMIC section helper macros are available but they are implemented as CRITICAL sections using PRIMASK register.
      
     
Macro API
The primary em_core API is the macro API. Macro API will map to correct CORE functions according to the selected CORE_ATOMIC_METHOD and similar configurations (the full CORE API is of course also available). The most useful macros are as follows:
      
       CORE_DECLARE_IRQ_STATE
      
      
      
       CORE_ENTER_ATOMIC()
      
      
      
       CORE_EXIT_ATOMIC()
      
      
      Used together to implement an ATOMIC section.
     
      
      
       CORE_ATOMIC_SECTION(yourcode)
      
      
      A concatenation of all three macros above.
     
      
      
       CORE_DECLARE_IRQ_STATE
      
      
      
       CORE_ENTER_CRITICAL()
      
      
      
       CORE_EXIT_CRITICAL()
      
      
      
       CORE_CRITICAL_SECTION(yourcode)
      
      
      These macros implement CRITICAL sections in a similar fashion as described above for ATOMIC sections.
     
      
      
       CORE_DECLARE_NVIC_STATE
      
      
      
       CORE_ENTER_NVIC()
      
      
      
       CORE_EXIT_NVIC()
      
      
      
       CORE_NVIC_SECTION(yourcode)
      
      
      These macros implement NVIC mask sections in a similar fashion as described above for ATOMIC sections. See
      
       Examples
      
      for an example.
     
Refer to Macros or Macro Definition Documentation below for a full list of macros.
      
     
API reimplementation
Most of the functions in the API are implemented as weak functions. This means that it is easy to reimplement when special needs arise. Shown below is a reimplementation of CRITICAL sections suitable if FreeRTOS OS is used:
Also note that CORE_Enter/ExitCritical() are not implemented as inline functions. As a result, reimplementations will be possible even when original implementations are inside a linked library.
Some RTOSes must be notified on interrupt handler entry and exit. Macros CORE_INTERRUPT_ENTRY() and CORE_INTERRUPT_EXIT() are suitable placeholders for inserting such code. Insert these macros in all your interrupt handlers and then override the default macro implementations. This is an example if uC/OS is used:
      
     
Interrupt vector tables
When using RAM based interrupt vector tables it is the user's responsibility to allocate the table space correctly. The tables must be aligned as specified in the CPU reference manual.
      
       CORE_InitNvicVectorTable()
      
      
      Initialize a RAM based vector table by copying table entries from a source vector table to a target table. VTOR is set to the address of the target vector table.
     
      
      
       CORE_GetNvicRamTableHandler()
      
      
      
       CORE_SetNvicRamTableHandler()
      
      
      Use these functions to get or set the interrupt handler for a specific IRQn. They both use the interrupt vector table defined by the current VTOR register value.
     
      
     
Maximum Interrupt Disabled Time
      The maximum time spent (in cycles) in critical and atomic sections can be measured for performance and interrupt latency analysis. To activate this feature, the Cycle Counter driver must be included in the project. To enable the timings, use the SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING configuration option. When enabled, the functions
      
      
       CORE_get_max_time_critical_section()
      
      
      
       CORE_get_max_time_atomic_section()
      
      
      can be used to get the max timings since startup.
     
      
     
Examples
Implement an NVIC critical section:
      
     
Porting from em_int
Existing code using INT_Enable() and INT_Disable() must be ported to the em_core API. While em_int used, a global counter to store the interrupt state, em_core uses a local variable. Any usage of INT_Disable(), therefore, needs to be replaced with a declaration of the interrupt state variable before entering the critical section.
Since the state variable is in local scope, the critical section exit needs to occur within the scope of the variable. If multiple nested critical sections are used, each needs to have its own state variable in its own scope.
In many cases, completely disabling all interrupts using CRITICAL sections might be more heavy-handed than needed. When porting, consider whether other types of sections, such as ATOMIC or NVIC mask, can be used to only disable a subset of the interrupts.
Replacing em_int calls with em_core function calls:
| Data Structures | |
| struct | CORE_nvicMask_t | 
| Storage for NVIC interrupt masks. | |
| Functions | |
| void | CORE_CriticalDisableIrq (void) | 
| Disable interrupts. | |
| void | CORE_CriticalEnableIrq (void) | 
| Enable interrupts. | |
| CORE_irqState_t | CORE_EnterCritical (void) | 
| Enter a CRITICAL section. | |
| void | CORE_ExitCritical ( CORE_irqState_t irqState) | 
| Exit a CRITICAL section. | |
| void | CORE_YieldCritical (void) | 
| Brief interrupt enable/disable sequence to allow handling of pending interrupts. | |
| void | CORE_AtomicDisableIrq (void) | 
| Disable interrupts. | |
| void | CORE_AtomicEnableIrq (void) | 
| Enable interrupts. | |
| CORE_irqState_t | CORE_EnterAtomic (void) | 
| Enter an ATOMIC section. | |
| void | CORE_ExitAtomic ( CORE_irqState_t irqState) | 
| Exit an ATOMIC section. | |
| void | CORE_YieldAtomic (void) | 
| Brief interrupt enable/disable sequence to allow handling of pending interrupts. | |
| void | CORE_EnterNvicMask ( CORE_nvicMask_t *nvicState, const CORE_nvicMask_t *disable) | 
| Enter a NVIC mask section. | |
| void | CORE_NvicDisableMask (const CORE_nvicMask_t *disable) | 
| Disable NVIC interrupts. | |
| void | CORE_NvicEnableMask (const CORE_nvicMask_t *enable) | 
| Set current NVIC interrupt enable mask. | |
| void | CORE_YieldNvicMask (const CORE_nvicMask_t *enable) | 
| Brief NVIC interrupt enable/disable sequence to allow handling of pending interrupts. | |
| void | CORE_NvicMaskSetIRQ (IRQn_Type irqN, CORE_nvicMask_t *mask) | 
| Utility function to set an IRQn bit in a NVIC enable/disable mask. | |
| void | CORE_NvicMaskClearIRQ (IRQn_Type irqN, CORE_nvicMask_t *mask) | 
| Utility function to clear an IRQn bit in a NVIC enable/disable mask. | |
| bool | CORE_InIrqContext (void) | 
| Check whether the current CPU operation mode is handler mode. | |
| bool | CORE_IrqIsBlocked (IRQn_Type irqN) | 
| Check if a specific interrupt is disabled or blocked. | |
| bool | CORE_IrqIsDisabled (void) | 
| Check if interrupts are disabled. | |
| void | CORE_GetNvicEnabledMask ( CORE_nvicMask_t *mask) | 
| Get the current NVIC enable mask state. | |
| bool | CORE_GetNvicMaskDisableState (const CORE_nvicMask_t *mask) | 
| Get NVIC disable state for a given mask. | |
| bool | CORE_NvicIRQDisabled (IRQn_Type irqN) | 
| Check if an NVIC interrupt is disabled. | |
| void * | CORE_GetNvicRamTableHandler (IRQn_Type irqN) | 
| Utility function to get the handler for a specific interrupt. | |
| void | CORE_SetNvicRamTableHandler (IRQn_Type irqN, void *handler) | 
| Utility function to set the handler for a specific interrupt. | |
| void | CORE_InitNvicVectorTable (uint32_t *sourceTable, uint32_t sourceSize, uint32_t *targetTable, uint32_t targetSize, void *defaultHandler, bool overwriteActive) | 
| Initialize an interrupt vector table by copying table entries from a source to a target table. | |
| uint32_t | CORE_get_max_time_critical_section (void) | 
| Returns the max time spent in critical section. | |
| uint32_t | CORE_get_max_time_atomic_section (void) | 
| Returns the max time spent in atomic section. | |
| Macros | |
| #define | CORE_INTERRUPT_ENTRY () | 
| Placeholder for optional interrupt handler entry code. | |
| #define | CORE_INTERRUPT_EXIT () | 
| Placeholder for optional interrupt handler exit code. | |
| #define | CORE_DECLARE_IRQ_STATE | 
| Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros. | |
| #define | CORE_CRITICAL_IRQ_DISABLE () | 
| CRITICAL style interrupt disable. | |
| #define | CORE_CRITICAL_IRQ_ENABLE () | 
| CRITICAL style interrupt enable. | |
| #define | CORE_CRITICAL_SECTION (yourcode) | 
| Convenience macro for implementing a CRITICAL section. | |
| #define | CORE_ENTER_CRITICAL () | 
| Enter CRITICAL section. | |
| #define | CORE_EXIT_CRITICAL () | 
| Exit CRITICAL section. | |
| #define | CORE_YIELD_CRITICAL () | 
| CRITICAL style yield. | |
| #define | CORE_ATOMIC_IRQ_DISABLE () | 
| ATOMIC style interrupt disable. | |
| #define | CORE_ATOMIC_IRQ_ENABLE () | 
| ATOMIC style interrupt enable. | |
| #define | CORE_ATOMIC_SECTION (yourcode) | 
| Convenience macro for implementing an ATOMIC section. | |
| #define | CORE_ENTER_ATOMIC () | 
| Enter ATOMIC section. | |
| #define | CORE_EXIT_ATOMIC () | 
| Exit ATOMIC section. | |
| #define | CORE_YIELD_ATOMIC () | 
| ATOMIC style yield. | |
| #define | CORE_ATOMIC_METHOD_PRIMASK 0 | 
| Use PRIMASK register to disable interrupts in ATOMIC sections. | |
| #define | CORE_ATOMIC_METHOD_BASEPRI 1 | 
| Use BASEPRI register to disable interrupts in ATOMIC sections. | |
| #define | CORE_NVIC_REG_WORDS ((EXT_IRQ_COUNT + 31) / 32) | 
| Number of words in a NVIC mask set. | |
| #define | CORE_DEFAULT_VECTOR_TABLE_ENTRIES (EXT_IRQ_COUNT + 16) | 
| Number of entries in a default interrupt vector table. | |
| #define | CORE_INTERRUPT_HIGHEST_PRIORITY 0 | 
| Highest priority for core interrupt. | |
| #define | CORE_INTERRUPT_DEFAULT_PRIORITY 1 | 
| Default priority for core interrupt. | |
| #define | CORE_INTERRUPT_LOWEST_PRIORITY 3 | 
| Lowest priority for core interrupt. | |
| #define | CORE_ATOMIC_METHOD_DEFAULT CORE_ATOMIC_METHOD_PRIMASK | 
| Default method to disable interrupts in ATOMIC sections. | |
| #define | CORE_ATOMIC_BASE_PRIORITY_LEVEL 3 | 
| The interrupt priority level disabled within ATOMIC regions. | |
| #define | CORE_ATOMIC_METHOD CORE_ATOMIC_METHOD_PRIMASK | 
| Specify which method to use when implementing ATOMIC sections. | |
| #define | CORE_DECLARE_IRQ_STATE CORE_irqState_t irqState | 
| Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros. | |
| #define | CORE_CRITICAL_IRQ_DISABLE () CORE_CriticalDisableIrq () | 
| CRITICAL style interrupt disable. | |
| #define | CORE_CRITICAL_IRQ_ENABLE () CORE_CriticalEnableIrq () | 
| CRITICAL style interrupt enable. | |
| #define | CORE_CRITICAL_SECTION (yourcode) | 
| Convenience macro for implementing a CRITICAL section. | |
| #define | CORE_ENTER_CRITICAL () irqState = CORE_EnterCritical () | 
| Enter CRITICAL section. | |
| #define | CORE_EXIT_CRITICAL () CORE_ExitCritical (irqState) | 
| Exit CRITICAL section. | |
| #define | CORE_YIELD_CRITICAL () CORE_YieldCritical () | 
| CRITICAL style yield. | |
| #define | CORE_ATOMIC_IRQ_DISABLE () CORE_AtomicDisableIrq () | 
| ATOMIC style interrupt disable. | |
| #define | CORE_ATOMIC_IRQ_ENABLE () CORE_AtomicEnableIrq () | 
| ATOMIC style interrupt enable. | |
| #define | CORE_ATOMIC_SECTION (yourcode) | 
| Convenience macro for implementing an ATOMIC section. | |
| #define | CORE_ENTER_ATOMIC () irqState = CORE_EnterAtomic () | 
| Enter ATOMIC section. | |
| #define | CORE_EXIT_ATOMIC () CORE_ExitAtomic (irqState) | 
| Exit ATOMIC section. | |
| #define | CORE_YIELD_ATOMIC () CORE_YieldAtomic () | 
| ATOMIC style yield. | |
| #define | CORE_DECLARE_NVIC_STATE CORE_nvicMask_t nvicState | 
| Allocate storage for NVIC interrupt masks for use by CORE_ENTER/EXIT_NVIC() macros. | |
| #define | CORE_DECLARE_NVIC_MASK (x) CORE_nvicMask_t x | 
| Allocate storage for NVIC interrupt masks. | |
| #define | CORE_DECLARE_NVIC_ZEROMASK (x) CORE_nvicMask_t x = { { 0 } } | 
| Allocate storage for and zero initialize NVIC interrupt mask. | |
| #define | CORE_NVIC_DISABLE (mask) CORE_NvicDisableMask (mask) | 
| NVIC mask style interrupt disable. | |
| #define | CORE_NVIC_ENABLE (mask) CORE_NvicEnableMask (mask) | 
| NVIC mask style interrupt enable. | |
| #define | CORE_NVIC_SECTION (mask, yourcode) | 
| Convenience macro for implementing a NVIC mask section. | |
| #define | CORE_ENTER_NVIC (disable) CORE_EnterNvicMask (&nvicState, disable) | 
| Enter NVIC mask section. | |
| #define | CORE_EXIT_NVIC () CORE_NvicEnableMask (&nvicState) | 
| Exit NVIC mask section. | |
| #define | CORE_YIELD_NVIC (enable) CORE_YieldNvicMask (enable) | 
| NVIC maks style yield. | |
| #define | CORE_IRQ_DISABLED () CORE_IrqIsDisabled () | 
| Check if IRQ is disabled. | |
| #define | CORE_IN_IRQ_CONTEXT () CORE_InIrqContext () | 
| Check if inside an IRQ handler. | |
| #define | START_COUNTER (handle) | 
| Start counter. | |
| #define | STOP_COUNTER (handle) | 
| Stop counter. | |
| Typedefs | |
| typedef uint32_t | CORE_irqState_t | 
| Storage for PRIMASK or BASEPRI value. | |
Function Documentation
◆ CORE_CriticalDisableIrq()
| void CORE_CriticalDisableIrq | ( | void | 
            | ) | 
Disable interrupts.
Disable all interrupts by setting PRIMASK. (Fault exception handlers will still be enabled).
◆ CORE_CriticalEnableIrq()
| void CORE_CriticalEnableIrq | ( | void | 
            | ) | 
Enable interrupts.
Enable interrupts by clearing PRIMASK.
◆ CORE_EnterCritical()
| CORE_irqState_t CORE_EnterCritical | ( | void | 
            | ) | 
Enter a CRITICAL section.
When a CRITICAL section is entered, all interrupts (except fault handlers) are disabled.
- Returns
- The value of PRIMASK register prior to the CRITICAL section entry.
◆ CORE_ExitCritical()
| void CORE_ExitCritical | ( | CORE_irqState_t | 
            irqState
            | ) | 
Exit a CRITICAL section.
- Parameters
- 
         [in] irqStateThe interrupt priority blocking level to restore to PRIMASK when exiting the CRITICAL section. This value is usually the one returned by a prior call to CORE_EnterCritical() . 
◆ CORE_YieldCritical()
| void CORE_YieldCritical | ( | void | 
            | ) | 
Brief interrupt enable/disable sequence to allow handling of pending interrupts.
- Note
- Usually used within a CRITICAL section.
◆ CORE_AtomicDisableIrq()
| void CORE_AtomicDisableIrq | ( | void | 
            | ) | 
Disable interrupts.
Disable interrupts with a priority lower or equal to CORE_ATOMIC_BASE_PRIORITY_LEVEL . Sets core BASEPRI register to CORE_ATOMIC_BASE_PRIORITY_LEVEL.
- Note
- If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_PRIMASK , this function is identical to CORE_CriticalDisableIrq() .
◆ CORE_AtomicEnableIrq()
| void CORE_AtomicEnableIrq | ( | void | 
            | ) | 
Enable interrupts.
Enable interrupts by setting core BASEPRI register to 0.
- Note
- If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_BASEPRI and PRIMASK is set (CPU is inside a CRITICAL section), interrupts will still be disabled after calling this function.
- If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_PRIMASK , this function is identical to CORE_CriticalEnableIrq() .
◆ CORE_EnterAtomic()
| CORE_irqState_t CORE_EnterAtomic | ( | void | 
            | ) | 
Enter an ATOMIC section.
When an ATOMIC section is entered, interrupts with priority lower or equal to CORE_ATOMIC_BASE_PRIORITY_LEVEL are disabled.
- Note
- If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_PRIMASK , this function is identical to CORE_EnterCritical() .
- Returns
- The value of BASEPRI register prior to ATOMIC section entry.
◆ CORE_ExitAtomic()
| void CORE_ExitAtomic | ( | CORE_irqState_t | 
            irqState
            | ) | 
Exit an ATOMIC section.
- Parameters
- 
         [in] irqStateThe interrupt priority blocking level to restore to BASEPRI when exiting the ATOMIC section. This value is usually the one returned by a prior call to CORE_EnterAtomic() . 
- Note
- If CORE_ATOMIC_METHOD is set to CORE_ATOMIC_METHOD_PRIMASK , this function is identical to CORE_ExitCritical() .
◆ CORE_YieldAtomic()
| void CORE_YieldAtomic | ( | void | 
            | ) | 
Brief interrupt enable/disable sequence to allow handling of pending interrupts.
- Note
- Usully used within an ATOMIC section.
- If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_PRIMASK , this function is identical to CORE_YieldCritical() .
◆ CORE_EnterNvicMask()
| void CORE_EnterNvicMask | ( | CORE_nvicMask_t * | 
            nvicState,
            | 
| const CORE_nvicMask_t * | 
            disable
            | ||
| ) | 
Enter a NVIC mask section.
When a NVIC mask section is entered, specified NVIC interrupts are disabled.
- Parameters
- 
         [out] nvicStateReturn NVIC interrupts enable mask prior to section entry. [in] disableA mask specifying which NVIC interrupts to disable within the section. 
◆ CORE_NvicDisableMask()
| void CORE_NvicDisableMask | ( | const CORE_nvicMask_t * | 
            disable
            | ) | 
Disable NVIC interrupts.
- Parameters
- 
         [in] disableA mask specifying which NVIC interrupts to disable. 
◆ CORE_NvicEnableMask()
| void CORE_NvicEnableMask | ( | const CORE_nvicMask_t * | 
            enable
            | ) | 
Set current NVIC interrupt enable mask.
- Parameters
- 
         [out] enableA mask specifying which NVIC interrupts are currently enabled. 
◆ CORE_YieldNvicMask()
| void CORE_YieldNvicMask | ( | const CORE_nvicMask_t * | 
            enable
            | ) | 
Brief NVIC interrupt enable/disable sequence to allow handling of pending interrupts.
- Parameters
- 
         [in] enableA mask specifying which NVIC interrupts to briefly enable. 
- Note
- Usually used within an NVIC mask section.
◆ CORE_NvicMaskSetIRQ()
| void CORE_NvicMaskSetIRQ | ( | IRQn_Type | 
            irqN,
            | 
| CORE_nvicMask_t * | 
            mask
            | ||
| ) | 
Utility function to set an IRQn bit in a NVIC enable/disable mask.
- Parameters
- 
         [in] irqNThe IRQn_Type enumerator for the interrupt. [in,out] maskThe mask to set the interrupt bit in. 
◆ CORE_NvicMaskClearIRQ()
| void CORE_NvicMaskClearIRQ | ( | IRQn_Type | 
            irqN,
            | 
| CORE_nvicMask_t * | 
            mask
            | ||
| ) | 
Utility function to clear an IRQn bit in a NVIC enable/disable mask.
- Parameters
- 
         [in] irqNThe IRQn_Type enumerator for the interrupt. [in,out] maskThe mask to clear the interrupt bit in. 
◆ CORE_InIrqContext()
| bool CORE_InIrqContext | ( | void | 
            | ) | 
Check whether the current CPU operation mode is handler mode.
- Returns
- 
         True if the CPU is in handler mode (currently executing an interrupt handler).
         
 False if the CPU is in thread mode.
◆ CORE_IrqIsBlocked()
| bool CORE_IrqIsBlocked | ( | IRQn_Type | 
            irqN
            | ) | 
Check if a specific interrupt is disabled or blocked.
- Parameters
- 
         [in] irqNThe IRQn_Type enumerator for the interrupt to check. 
- Returns
- True if the interrupt is disabled or blocked.
◆ CORE_IrqIsDisabled()
| bool CORE_IrqIsDisabled | ( | void | 
            | ) | 
Check if interrupts are disabled.
- Returns
- True if interrupts are disabled.
◆ CORE_GetNvicEnabledMask()
| void CORE_GetNvicEnabledMask | ( | CORE_nvicMask_t * | 
            mask
            | ) | 
Get the current NVIC enable mask state.
- Parameters
- 
         [out] maskThe current NVIC enable mask. 
◆ CORE_GetNvicMaskDisableState()
| bool CORE_GetNvicMaskDisableState | ( | const CORE_nvicMask_t * | 
            mask
            | ) | 
Get NVIC disable state for a given mask.
- Parameters
- 
         [in] maskAn NVIC mask to check. 
- Returns
- True if all NVIC interrupt mask bits are clear.
◆ CORE_NvicIRQDisabled()
| bool CORE_NvicIRQDisabled | ( | IRQn_Type | 
            irqN
            | ) | 
Check if an NVIC interrupt is disabled.
- Parameters
- 
         [in] irqNThe IRQn_Type enumerator for the interrupt to check. 
- Returns
- True if the interrupt is disabled.
◆ CORE_GetNvicRamTableHandler()
| void * CORE_GetNvicRamTableHandler | ( | IRQn_Type | 
            irqN
            | ) | 
Utility function to get the handler for a specific interrupt.
- Parameters
- 
         [in] irqNThe IRQn_Type enumerator for the interrupt. 
- Returns
- The handler address.
- Note
- Uses the interrupt vector table defined by the current VTOR register value.
◆ CORE_SetNvicRamTableHandler()
| void CORE_SetNvicRamTableHandler | ( | IRQn_Type | 
            irqN,
            | 
| void * | 
            handler
            | ||
| ) | 
Utility function to set the handler for a specific interrupt.
- Parameters
- 
         [in] irqNThe IRQn_Type enumerator for the interrupt. [in] handlerThe handler address. 
- Note
- Uses the interrupt vector table defined by the current VTOR register value.
◆ CORE_InitNvicVectorTable()
| void CORE_InitNvicVectorTable | ( | uint32_t * | 
            sourceTable,
            | 
| uint32_t | 
            sourceSize,
            | ||
| uint32_t * | 
            targetTable,
            | ||
| uint32_t | 
            targetSize,
            | ||
| void * | 
            defaultHandler,
            | ||
| bool | 
            overwriteActive
            | ||
| ) | 
Initialize an interrupt vector table by copying table entries from a source to a target table.
- Note
- This function will set a new VTOR register value.
- Parameters
- 
         [in] sourceTableThe address of the source vector table. [in] sourceSizeA number of entries in the source vector table. [in] targetTableThe address of the target (new) vector table. [in] targetSizeA number of entries in the target vector table. [in] defaultHandlerAn address of the interrupt handler used for target entries for which where there is no corresponding source entry (i.e., the target table is larger than the source table). [in] overwriteActiveWhen true, a target table entry is always overwritten with the corresponding source entry. If false, a target table entry is only overwritten if it is zero. This makes it possible for an application to partly initialize a target table before passing it to this function. 
◆ CORE_get_max_time_critical_section()
| uint32_t CORE_get_max_time_critical_section | ( | void | 
            | ) | 
Returns the max time spent in critical section.
- Returns
- The max time spent in critical section.
- Note
- SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.
◆ CORE_get_max_time_atomic_section()
| uint32_t CORE_get_max_time_atomic_section | ( | void | 
            | ) | 
Returns the max time spent in atomic section.
- Returns
- The max time spent in atomic section.
- Note
- SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.
Macro Definition Documentation
◆ CORE_INTERRUPT_ENTRY
| #define CORE_INTERRUPT_ENTRY | ( | 
            | ) | 
Placeholder for optional interrupt handler entry code.
This might be needed when working with an RTOS.
◆ CORE_INTERRUPT_EXIT
| #define CORE_INTERRUPT_EXIT | ( | 
            | ) | 
Placeholder for optional interrupt handler exit code.
This might be needed when working with an RTOS.
◆ CORE_DECLARE_IRQ_STATE [1/2]
| #define CORE_DECLARE_IRQ_STATE | 
Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.
◆ CORE_CRITICAL_IRQ_DISABLE [1/2]
| #define CORE_CRITICAL_IRQ_DISABLE | ( | 
            | ) | 
CRITICAL style interrupt disable.
◆ CORE_CRITICAL_IRQ_ENABLE [1/2]
| #define CORE_CRITICAL_IRQ_ENABLE | ( | 
            | ) | 
CRITICAL style interrupt enable.
◆ CORE_CRITICAL_SECTION [1/2]
| #define CORE_CRITICAL_SECTION | ( | 
            yourcode
            | ) | 
Convenience macro for implementing a CRITICAL section.
◆ CORE_ENTER_CRITICAL [1/2]
| #define CORE_ENTER_CRITICAL | ( | 
            | ) | 
Enter CRITICAL section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
◆ CORE_EXIT_CRITICAL [1/2]
| #define CORE_EXIT_CRITICAL | ( | 
            | ) | 
Exit CRITICAL section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
◆ CORE_YIELD_CRITICAL [1/2]
| #define CORE_YIELD_CRITICAL | ( | 
            | ) | 
CRITICAL style yield.
◆ CORE_ATOMIC_IRQ_DISABLE [1/2]
| #define CORE_ATOMIC_IRQ_DISABLE | ( | 
            | ) | 
ATOMIC style interrupt disable.
◆ CORE_ATOMIC_IRQ_ENABLE [1/2]
| #define CORE_ATOMIC_IRQ_ENABLE | ( | 
            | ) | 
ATOMIC style interrupt enable.
◆ CORE_ATOMIC_SECTION [1/2]
| #define CORE_ATOMIC_SECTION | ( | 
            yourcode
            | ) | 
Convenience macro for implementing an ATOMIC section.
◆ CORE_ENTER_ATOMIC [1/2]
| #define CORE_ENTER_ATOMIC | ( | 
            | ) | 
Enter ATOMIC section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
◆ CORE_EXIT_ATOMIC [1/2]
| #define CORE_EXIT_ATOMIC | ( | 
            | ) | 
Exit ATOMIC section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
◆ CORE_YIELD_ATOMIC [1/2]
| #define CORE_YIELD_ATOMIC | ( | 
            | ) | 
ATOMIC style yield.
◆ CORE_ATOMIC_METHOD_PRIMASK
| #define CORE_ATOMIC_METHOD_PRIMASK 0 | 
Use PRIMASK register to disable interrupts in ATOMIC sections.
◆ CORE_ATOMIC_METHOD_BASEPRI
| #define CORE_ATOMIC_METHOD_BASEPRI 1 | 
Use BASEPRI register to disable interrupts in ATOMIC sections.
◆ CORE_NVIC_REG_WORDS
| #define CORE_NVIC_REG_WORDS ((EXT_IRQ_COUNT + 31) / 32) | 
Number of words in a NVIC mask set.
◆ CORE_DEFAULT_VECTOR_TABLE_ENTRIES
| #define CORE_DEFAULT_VECTOR_TABLE_ENTRIES (EXT_IRQ_COUNT + 16) | 
Number of entries in a default interrupt vector table.
◆ CORE_INTERRUPT_HIGHEST_PRIORITY
| #define CORE_INTERRUPT_HIGHEST_PRIORITY 0 | 
Highest priority for core interrupt.
◆ CORE_INTERRUPT_DEFAULT_PRIORITY
| #define CORE_INTERRUPT_DEFAULT_PRIORITY 1 | 
Default priority for core interrupt.
◆ CORE_INTERRUPT_LOWEST_PRIORITY
| #define CORE_INTERRUPT_LOWEST_PRIORITY 3 | 
Lowest priority for core interrupt.
◆ CORE_ATOMIC_METHOD_DEFAULT
| #define CORE_ATOMIC_METHOD_DEFAULT CORE_ATOMIC_METHOD_PRIMASK | 
Default method to disable interrupts in ATOMIC sections.
◆ CORE_ATOMIC_BASE_PRIORITY_LEVEL
| #define CORE_ATOMIC_BASE_PRIORITY_LEVEL 3 | 
The interrupt priority level disabled within ATOMIC regions.
Interrupts with priority level equal to or lower than this definition will be disabled within ATOMIC regions.
◆ CORE_ATOMIC_METHOD
| #define CORE_ATOMIC_METHOD CORE_ATOMIC_METHOD_PRIMASK | 
Specify which method to use when implementing ATOMIC sections.
You can select between BASEPRI or PRIMASK method.
- Note
- On Cortex-M0+ devices only PRIMASK can be used.
◆ CORE_DECLARE_IRQ_STATE [2/2]
| #define CORE_DECLARE_IRQ_STATE CORE_irqState_t irqState | 
Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.
◆ CORE_CRITICAL_IRQ_DISABLE [2/2]
| #define CORE_CRITICAL_IRQ_DISABLE | ( | 
            | ) | CORE_CriticalDisableIrq () | 
CRITICAL style interrupt disable.
◆ CORE_CRITICAL_IRQ_ENABLE [2/2]
| #define CORE_CRITICAL_IRQ_ENABLE | ( | 
            | ) | CORE_CriticalEnableIrq () | 
CRITICAL style interrupt enable.
◆ CORE_CRITICAL_SECTION [2/2]
| #define CORE_CRITICAL_SECTION | ( | 
            yourcode
            | ) | 
Convenience macro for implementing a CRITICAL section.
◆ CORE_ENTER_CRITICAL [2/2]
| #define CORE_ENTER_CRITICAL | ( | 
            | ) | irqState = CORE_EnterCritical () | 
Enter CRITICAL section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
◆ CORE_EXIT_CRITICAL [2/2]
| #define CORE_EXIT_CRITICAL | ( | 
            | ) | CORE_ExitCritical (irqState) | 
Exit CRITICAL section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
◆ CORE_YIELD_CRITICAL [2/2]
| #define CORE_YIELD_CRITICAL | ( | 
            | ) | CORE_YieldCritical () | 
CRITICAL style yield.
◆ CORE_ATOMIC_IRQ_DISABLE [2/2]
| #define CORE_ATOMIC_IRQ_DISABLE | ( | 
            | ) | CORE_AtomicDisableIrq () | 
ATOMIC style interrupt disable.
◆ CORE_ATOMIC_IRQ_ENABLE [2/2]
| #define CORE_ATOMIC_IRQ_ENABLE | ( | 
            | ) | CORE_AtomicEnableIrq () | 
ATOMIC style interrupt enable.
◆ CORE_ATOMIC_SECTION [2/2]
| #define CORE_ATOMIC_SECTION | ( | 
            yourcode
            | ) | 
Convenience macro for implementing an ATOMIC section.
◆ CORE_ENTER_ATOMIC [2/2]
| #define CORE_ENTER_ATOMIC | ( | 
            | ) | irqState = CORE_EnterAtomic () | 
Enter ATOMIC section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
◆ CORE_EXIT_ATOMIC [2/2]
| #define CORE_EXIT_ATOMIC | ( | 
            | ) | CORE_ExitAtomic (irqState) | 
Exit ATOMIC section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
◆ CORE_YIELD_ATOMIC [2/2]
| #define CORE_YIELD_ATOMIC | ( | 
            | ) | CORE_YieldAtomic () | 
ATOMIC style yield.
◆ CORE_DECLARE_NVIC_STATE
| #define CORE_DECLARE_NVIC_STATE CORE_nvicMask_t nvicState | 
Allocate storage for NVIC interrupt masks for use by CORE_ENTER/EXIT_NVIC() macros.
◆ CORE_DECLARE_NVIC_MASK
| #define CORE_DECLARE_NVIC_MASK | ( | 
            x
            | ) | CORE_nvicMask_t x | 
Allocate storage for NVIC interrupt masks.
- Parameters
- 
         [in] xThe storage variable name to use. 
◆ CORE_DECLARE_NVIC_ZEROMASK
| #define CORE_DECLARE_NVIC_ZEROMASK | ( | 
            x
            | ) | CORE_nvicMask_t x = { { 0 } } | 
Allocate storage for and zero initialize NVIC interrupt mask.
- Parameters
- 
         [in] xThe storage variable name to use. 
◆ CORE_NVIC_DISABLE
| #define CORE_NVIC_DISABLE | ( | 
            mask
            | ) | CORE_NvicDisableMask (mask) | 
NVIC mask style interrupt disable.
- Parameters
- 
         [in] maskMask specifying which NVIC interrupts to disable. 
◆ CORE_NVIC_ENABLE
| #define CORE_NVIC_ENABLE | ( | 
            mask
            | ) | CORE_NvicEnableMask (mask) | 
NVIC mask style interrupt enable.
- Parameters
- 
         [in] maskMask specifying which NVIC interrupts to enable. 
◆ CORE_NVIC_SECTION
| #define CORE_NVIC_SECTION | ( | 
            mask,
            | |
| 
            yourcode
            | |||
| ) | 
Convenience macro for implementing a NVIC mask section.
- Parameters
- 
         [in] maskMask specifying which NVIC interrupts to disable within the section. [in] yourcodeThe code for the section. 
◆ CORE_ENTER_NVIC
| #define CORE_ENTER_NVIC | ( | 
            disable
            | ) | CORE_EnterNvicMask (&nvicState, disable) | 
Enter NVIC mask section.
Assumes that a CORE_DECLARE_NVIC_STATE exist in scope.
- Parameters
- 
         [in] disableMask specifying which NVIC interrupts to disable within the section. 
◆ CORE_EXIT_NVIC
| #define CORE_EXIT_NVIC | ( | 
            | ) | CORE_NvicEnableMask (&nvicState) | 
Exit NVIC mask section.
Assumes that a CORE_DECLARE_NVIC_STATE exist in scope.
◆ CORE_YIELD_NVIC
| #define CORE_YIELD_NVIC | ( | 
            enable
            | ) | CORE_YieldNvicMask (enable) | 
NVIC maks style yield.
- Parameters
- 
         [in] enableMask specifying which NVIC interrupts to briefly enable. 
◆ CORE_IRQ_DISABLED
| #define CORE_IRQ_DISABLED | ( | 
            | ) | CORE_IrqIsDisabled () | 
Check if IRQ is disabled.
◆ CORE_IN_IRQ_CONTEXT
| #define CORE_IN_IRQ_CONTEXT | ( | 
            | ) | CORE_InIrqContext () | 
Check if inside an IRQ handler.
◆ START_COUNTER
| #define START_COUNTER | ( | 
            handle
            | ) | 
Start counter.
◆ STOP_COUNTER
| #define STOP_COUNTER | ( | 
            handle
            | ) | 
Stop counter.
Typedef Documentation
◆ CORE_irqState_t
| typedef uint32_t CORE_irqState_t | 
Storage for PRIMASK or BASEPRI value.