ACMP_Init_TypeDef Struct Reference
ACMP initialization structure.
      
       #include <em_acmp.h>
      
     
| Data Fields | |
| bool | fullBias | 
| Full-bias current. | |
| bool | halfBias | 
| Half-bias current. | |
| uint32_t | biasProg | 
| Bias current. | |
| bool | interruptOnFallingEdge | 
| Enable setting the interrupt flag on the falling edge. | |
| bool | interruptOnRisingEdge | 
| Enable setting the interrupt flag on the rising edge. | |
| ACMP_WarmTime_TypeDef | warmTime | 
| Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time. | |
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel | 
| Hysteresis level. | |
| bool | inactiveValue | 
| Inactive value emitted by ACMP during warmup. | |
| bool | lowPowerReferenceEnabled | 
| Low power reference enabled. | |
| uint32_t | vddLevel | 
| VDD reference value. | |
| bool | enable | 
| If true, ACMP is enabled after configuration. | |
ACMP initialization structure.
Field Documentation
◆ fullBias
| bool ACMP_Init_TypeDef::fullBias | 
Full-bias current.
See the ACMP chapter about bias and response time in the reference manual for details.
◆ halfBias
| bool ACMP_Init_TypeDef::halfBias | 
Half-bias current.
See the ACMP chapter about bias and response time in the reference manual for details.
◆ biasProg
| uint32_t ACMP_Init_TypeDef::biasProg | 
Bias current.
See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
◆ interruptOnFallingEdge
| bool ACMP_Init_TypeDef::interruptOnFallingEdge | 
Enable setting the interrupt flag on the falling edge.
◆ interruptOnRisingEdge
| bool ACMP_Init_TypeDef::interruptOnRisingEdge | 
Enable setting the interrupt flag on the rising edge.
◆ warmTime
| ACMP_WarmTime_TypeDef ACMP_Init_TypeDef::warmTime | 
Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time.
◆ hysteresisLevel
| ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel | 
Hysteresis level.
◆ inactiveValue
| bool ACMP_Init_TypeDef::inactiveValue | 
Inactive value emitted by ACMP during warmup.
◆ lowPowerReferenceEnabled
| bool ACMP_Init_TypeDef::lowPowerReferenceEnabled | 
Low power reference enabled.
This setting, if enabled, reduces the power used by the VDD and bandgap references.
◆ vddLevel
| uint32_t ACMP_Init_TypeDef::vddLevel | 
VDD reference value.
VDD_SCALED = VDD * VDDLEVEL * 50 mV/3.8 V. Valid values are in the 0-63 range.
◆ enable
| bool ACMP_Init_TypeDef::enable | 
If true, ACMP is enabled after configuration.