ACMP - Analog Comparator
Description
Analog comparator (ACMP) Peripheral API.
The Analog Comparator is used to compare voltage of two analog inputs with a digital output indicating which input voltage is higher. Inputs can either be one of the selectable internal references or from external pins. Response time and current consumption can be configured by altering the current supply to the comparator.
ACMP is available down to EM3 and is able to wake up the system when input signals pass a certain threshold. Use ACMP_IntEnable() to enable an edge interrupt to use this functionality.
This example shows how to use the em_acmp.h API for comparing an input pin to an internal 2.5 V reference voltage.
- Note
- ACMP can also be used to compare two separate input pins.
ACMP also contains specialized hardware for capacitive sensing. This module contains the ACMP_CapsenseInit() function to initialize ACMP for capacitive sensing and the ACMP_CapsenseChannelSet() function to select the current capsense channel.
For applications that require capacitive sensing it is recommended to use a library, such as cslib, which is provided by Silicon Labs.
| Data Structures | |
| struct | ACMP_CapsenseInit_TypeDef | 
| Capsense initialization structure. | |
| struct | ACMP_Init_TypeDef | 
| ACMP initialization structure. | |
| struct | ACMP_VAConfig_TypeDef | 
| VA Configuration structure. | |
| struct | ACMP_VBConfig_TypeDef | 
| VB Configuration structure. | |
| Functions | |
| void | ACMP_CapsenseInit (ACMP_TypeDef *acmp, const ACMP_CapsenseInit_TypeDef *init) | 
| Set up ACMP for use in capacitive sense applications. | |
| void | ACMP_CapsenseChannelSet (ACMP_TypeDef *acmp, ACMP_Channel_TypeDef channel) | 
| Set the ACMP channel used for capacitive sensing. | |
| void | ACMP_ChannelSet (ACMP_TypeDef *acmp, ACMP_Channel_TypeDef negSel, ACMP_Channel_TypeDef posSel) | 
| Set which channels should be used in ACMP comparisons. | |
| void | ACMP_Disable (ACMP_TypeDef *acmp) | 
| Disable ACMP. | |
| void | ACMP_Enable (ACMP_TypeDef *acmp) | 
| Enable ACMP. | |
| void | ACMP_ExternalInputSelect (ACMP_TypeDef *acmp, ACMP_ExternalInput_Typedef aport) | 
| Select and enable external input. | |
| void | ACMP_GPIOSetup (ACMP_TypeDef *acmp, uint32_t location, bool enable, bool invert) | 
| Set up GPIO output from ACMP. | |
| void | ACMP_Init (ACMP_TypeDef *acmp, const ACMP_Init_TypeDef *init) | 
| Initialize ACMP. | |
| void | ACMP_Reset (ACMP_TypeDef *acmp) | 
| Reset ACMP to the same state that it was in after a hardware reset. | |
| void | ACMP_VASetup (ACMP_TypeDef *acmp, const ACMP_VAConfig_TypeDef *vaconfig) | 
| Set up the VA source. | |
| void | ACMP_VBSetup (ACMP_TypeDef *acmp, const ACMP_VBConfig_TypeDef *vbconfig) | 
| Set up the VB Source. | |
| void | ACMP_IntClear (ACMP_TypeDef *acmp, uint32_t flags) | 
| Clear one or more pending ACMP interrupts. | |
| void | ACMP_IntDisable (ACMP_TypeDef *acmp, uint32_t flags) | 
| Disable one or more ACMP interrupts. | |
| void | ACMP_IntEnable (ACMP_TypeDef *acmp, uint32_t flags) | 
| Enable one or more ACMP interrupts. | |
| uint32_t | ACMP_IntGet (ACMP_TypeDef *acmp) | 
| Get pending ACMP interrupt flags. | |
| uint32_t | ACMP_IntGetEnabled (ACMP_TypeDef *acmp) | 
| Get enabled and pending ACMP interrupt flags. | |
| void | ACMP_IntSet (ACMP_TypeDef *acmp, uint32_t flags) | 
| Set one or more pending ACMP interrupts from software. | |
| Macros | |
| #define | ACMP_CAPSENSE_INIT_DEFAULT | 
| A default configuration for capacitive sense mode initialization. | |
| #define | ACMP_INIT_DEFAULT | 
| Default configuration for ACMP regular initialization. | |
| #define | ACMP_VACONFIG_DEFAULT | 
| VA default configuration. | |
| #define | ACMP_VBCONFIG_DEFAULT | 
| VB default configuration. | |
| Enumerations | |
| enum | ACMP_CapsenseResistor_TypeDef
         
         { acmpResistor0 = _ACMP_INPUTSEL_CSRESSEL_RES0, acmpResistor1 = _ACMP_INPUTSEL_CSRESSEL_RES1, acmpResistor2 = _ACMP_INPUTSEL_CSRESSEL_RES2, acmpResistor3 = _ACMP_INPUTSEL_CSRESSEL_RES3, acmpResistor4 = _ACMP_INPUTSEL_CSRESSEL_RES4, acmpResistor5 = _ACMP_INPUTSEL_CSRESSEL_RES5, acmpResistor6 = _ACMP_INPUTSEL_CSRESSEL_RES6, acmpResistor7 = _ACMP_INPUTSEL_CSRESSEL_RES7 } | 
| Resistor values used for the internal capacitive sense resistor. | |
| enum | ACMP_HysteresisLevel_TypeDef
         
         { acmpHysteresisLevel0 = _ACMP_HYSTERESIS0_HYST_HYST0, acmpHysteresisLevel1 = _ACMP_HYSTERESIS0_HYST_HYST1, acmpHysteresisLevel2 = _ACMP_HYSTERESIS0_HYST_HYST2, acmpHysteresisLevel3 = _ACMP_HYSTERESIS0_HYST_HYST3, acmpHysteresisLevel4 = _ACMP_HYSTERESIS0_HYST_HYST4, acmpHysteresisLevel5 = _ACMP_HYSTERESIS0_HYST_HYST5, acmpHysteresisLevel6 = _ACMP_HYSTERESIS0_HYST_HYST6, acmpHysteresisLevel7 = _ACMP_HYSTERESIS0_HYST_HYST7, acmpHysteresisLevel8 = _ACMP_HYSTERESIS0_HYST_HYST8, acmpHysteresisLevel9 = _ACMP_HYSTERESIS0_HYST_HYST9, acmpHysteresisLevel10 = _ACMP_HYSTERESIS0_HYST_HYST10, acmpHysteresisLevel11 = _ACMP_HYSTERESIS0_HYST_HYST11, acmpHysteresisLevel12 = _ACMP_HYSTERESIS0_HYST_HYST12, acmpHysteresisLevel13 = _ACMP_HYSTERESIS0_HYST_HYST13, acmpHysteresisLevel14 = _ACMP_HYSTERESIS0_HYST_HYST14, acmpHysteresisLevel15 = _ACMP_HYSTERESIS0_HYST_HYST15 } | 
| Hysteresis level. | |
| enum | ACMP_InputRange_TypeDef
         
         { acmpInputRangeFull = _ACMP_CTRL_INPUTRANGE_FULL, acmpInputRangeHigh = _ACMP_CTRL_INPUTRANGE_GTVDDDIV2, acmpInputRangeLow = _ACMP_CTRL_INPUTRANGE_LTVDDDIV2 } | 
| Adjust ACMP performance for a given input voltage range. | |
| enum | ACMP_PowerSource_TypeDef
         
         { acmpPowerSourceAvdd = _ACMP_CTRL_PWRSEL_AVDD, acmpPowerSourceDvdd = _ACMP_CTRL_PWRSEL_DVDD, acmpPowerSourceIOVdd0 = _ACMP_CTRL_PWRSEL_IOVDD0, acmpPowerSourceIOVdd1 = _ACMP_CTRL_PWRSEL_IOVDD1 } | 
| ACMP Power source. | |
| enum | ACMP_Accuracy_TypeDef
         
         { acmpAccuracyLow = _ACMP_CTRL_ACCURACY_LOW, acmpAccuracyHigh = _ACMP_CTRL_ACCURACY_HIGH } | 
| ACMP accuracy mode. | |
| enum | ACMP_VAInput_TypeDef
         
         { acmpVAInputVDD = _ACMP_INPUTSEL_VASEL_VDD, acmpVAInputAPORT2YCH0 = _ACMP_INPUTSEL_VASEL_APORT2YCH0, acmpVAInputAPORT2YCH2 = _ACMP_INPUTSEL_VASEL_APORT2YCH2, acmpVAInputAPORT2YCH4 = _ACMP_INPUTSEL_VASEL_APORT2YCH4, acmpVAInputAPORT2YCH6 = _ACMP_INPUTSEL_VASEL_APORT2YCH6, acmpVAInputAPORT2YCH8 = _ACMP_INPUTSEL_VASEL_APORT2YCH8, acmpVAInputAPORT2YCH10 = _ACMP_INPUTSEL_VASEL_APORT2YCH10, acmpVAInputAPORT2YCH12 = _ACMP_INPUTSEL_VASEL_APORT2YCH12, acmpVAInputAPORT2YCH14 = _ACMP_INPUTSEL_VASEL_APORT2YCH14, acmpVAInputAPORT2YCH16 = _ACMP_INPUTSEL_VASEL_APORT2YCH16, acmpVAInputAPORT2YCH18 = _ACMP_INPUTSEL_VASEL_APORT2YCH18, acmpVAInputAPORT2YCH20 = _ACMP_INPUTSEL_VASEL_APORT2YCH20, acmpVAInputAPORT2YCH22 = _ACMP_INPUTSEL_VASEL_APORT2YCH22, acmpVAInputAPORT2YCH24 = _ACMP_INPUTSEL_VASEL_APORT2YCH24, acmpVAInputAPORT2YCH26 = _ACMP_INPUTSEL_VASEL_APORT2YCH26, acmpVAInputAPORT2YCH28 = _ACMP_INPUTSEL_VASEL_APORT2YCH28, acmpVAInputAPORT2YCH30 = _ACMP_INPUTSEL_VASEL_APORT2YCH30, acmpVAInputAPORT1XCH0 = _ACMP_INPUTSEL_VASEL_APORT1XCH0, acmpVAInputAPORT1YCH1 = _ACMP_INPUTSEL_VASEL_APORT1YCH1, acmpVAInputAPORT1XCH2 = _ACMP_INPUTSEL_VASEL_APORT1XCH2, acmpVAInputAPORT1YCH3 = _ACMP_INPUTSEL_VASEL_APORT1YCH3, acmpVAInputAPORT1XCH4 = _ACMP_INPUTSEL_VASEL_APORT1XCH4, acmpVAInputAPORT1YCH5 = _ACMP_INPUTSEL_VASEL_APORT1YCH5, acmpVAInputAPORT1XCH6 = _ACMP_INPUTSEL_VASEL_APORT1XCH6, acmpVAInputAPORT1YCH7 = _ACMP_INPUTSEL_VASEL_APORT1YCH7, acmpVAInputAPORT1XCH8 = _ACMP_INPUTSEL_VASEL_APORT1XCH8, acmpVAInputAPORT1YCH9 = _ACMP_INPUTSEL_VASEL_APORT1YCH9, acmpVAInputAPORT1XCH10 = _ACMP_INPUTSEL_VASEL_APORT1XCH10, acmpVAInputAPORT1YCH11 = _ACMP_INPUTSEL_VASEL_APORT1YCH11, acmpVAInputAPORT1XCH12 = _ACMP_INPUTSEL_VASEL_APORT1XCH12, acmpVAInputAPORT1YCH13 = _ACMP_INPUTSEL_VASEL_APORT1YCH13, acmpVAInputAPORT1XCH14 = _ACMP_INPUTSEL_VASEL_APORT1XCH14, acmpVAInputAPORT1YCH15 = _ACMP_INPUTSEL_VASEL_APORT1YCH15, acmpVAInputAPORT1XCH16 = _ACMP_INPUTSEL_VASEL_APORT1XCH16, acmpVAInputAPORT1YCH17 = _ACMP_INPUTSEL_VASEL_APORT1YCH17, acmpVAInputAPORT1XCH18 = _ACMP_INPUTSEL_VASEL_APORT1XCH18, acmpVAInputAPORT1YCH19 = _ACMP_INPUTSEL_VASEL_APORT1YCH19, acmpVAInputAPORT1XCH20 = _ACMP_INPUTSEL_VASEL_APORT1XCH20, acmpVAInputAPORT1YCH21 = _ACMP_INPUTSEL_VASEL_APORT1YCH21, acmpVAInputAPORT1XCH22 = _ACMP_INPUTSEL_VASEL_APORT1XCH22, acmpVAInputAPORT1YCH23 = _ACMP_INPUTSEL_VASEL_APORT1YCH23, acmpVAInputAPORT1XCH24 = _ACMP_INPUTSEL_VASEL_APORT1XCH24, acmpVAInputAPORT1YCH25 = _ACMP_INPUTSEL_VASEL_APORT1YCH25, acmpVAInputAPORT1XCH26 = _ACMP_INPUTSEL_VASEL_APORT1XCH26, acmpVAInputAPORT1YCH27 = _ACMP_INPUTSEL_VASEL_APORT1YCH27, acmpVAInputAPORT1XCH28 = _ACMP_INPUTSEL_VASEL_APORT1XCH28, acmpVAInputAPORT1YCH29 = _ACMP_INPUTSEL_VASEL_APORT1YCH29, acmpVAInputAPORT1XCH30 = _ACMP_INPUTSEL_VASEL_APORT1XCH30, acmpVAInputAPORT1YCH31 = _ACMP_INPUTSEL_VASEL_APORT1YCH31 } | 
| ACMP input to the VA divider. | |
| enum | ACMP_VBInput_TypeDef
         
         { acmpVBInput1V25 = _ACMP_INPUTSEL_VBSEL_1V25, acmpVBInput2V5 = _ACMP_INPUTSEL_VBSEL_2V5 } | 
| ACMP input to the VB divider. | |
| enum | ACMP_VLPInput_Typedef
         
         { acmpVLPInputVADIV = _ACMP_INPUTSEL_VLPSEL_VADIV, acmpVLPInputVBDIV = _ACMP_INPUTSEL_VLPSEL_VBDIV } | 
| ACMP Low-Power Input Selection. | |
| enum | ACMP_Channel_TypeDef
         
         { acmpInputAPORT0XCH0 = _ACMP_INPUTSEL_POSSEL_APORT0XCH0, acmpInputAPORT0XCH1 = _ACMP_INPUTSEL_POSSEL_APORT0XCH1, acmpInputAPORT0XCH2 = _ACMP_INPUTSEL_POSSEL_APORT0XCH2, acmpInputAPORT0XCH3 = _ACMP_INPUTSEL_POSSEL_APORT0XCH3, acmpInputAPORT0XCH4 = _ACMP_INPUTSEL_POSSEL_APORT0XCH4, acmpInputAPORT0XCH5 = _ACMP_INPUTSEL_POSSEL_APORT0XCH5, acmpInputAPORT0XCH6 = _ACMP_INPUTSEL_POSSEL_APORT0XCH6, acmpInputAPORT0XCH7 = _ACMP_INPUTSEL_POSSEL_APORT0XCH7, acmpInputAPORT0XCH8 = _ACMP_INPUTSEL_POSSEL_APORT0XCH8, acmpInputAPORT0XCH9 = _ACMP_INPUTSEL_POSSEL_APORT0XCH9, acmpInputAPORT0XCH10 = _ACMP_INPUTSEL_POSSEL_APORT0XCH10, acmpInputAPORT0XCH11 = _ACMP_INPUTSEL_POSSEL_APORT0XCH11, acmpInputAPORT0XCH12 = _ACMP_INPUTSEL_POSSEL_APORT0XCH12, acmpInputAPORT0XCH13 = _ACMP_INPUTSEL_POSSEL_APORT0XCH13, acmpInputAPORT0XCH14 = _ACMP_INPUTSEL_POSSEL_APORT0XCH14, acmpInputAPORT0XCH15 = _ACMP_INPUTSEL_POSSEL_APORT0XCH15, acmpInputAPORT0YCH0 = _ACMP_INPUTSEL_POSSEL_APORT0YCH0, acmpInputAPORT0YCH1 = _ACMP_INPUTSEL_POSSEL_APORT0YCH1, acmpInputAPORT0YCH2 = _ACMP_INPUTSEL_POSSEL_APORT0YCH2, acmpInputAPORT0YCH3 = _ACMP_INPUTSEL_POSSEL_APORT0YCH3, acmpInputAPORT0YCH4 = _ACMP_INPUTSEL_POSSEL_APORT0YCH4, acmpInputAPORT0YCH5 = _ACMP_INPUTSEL_POSSEL_APORT0YCH5, acmpInputAPORT0YCH6 = _ACMP_INPUTSEL_POSSEL_APORT0YCH6, acmpInputAPORT0YCH7 = _ACMP_INPUTSEL_POSSEL_APORT0YCH7, acmpInputAPORT0YCH8 = _ACMP_INPUTSEL_POSSEL_APORT0YCH8, acmpInputAPORT0YCH9 = _ACMP_INPUTSEL_POSSEL_APORT0YCH9, acmpInputAPORT0YCH10 = _ACMP_INPUTSEL_POSSEL_APORT0YCH10, acmpInputAPORT0YCH11 = _ACMP_INPUTSEL_POSSEL_APORT0YCH11, acmpInputAPORT0YCH12 = _ACMP_INPUTSEL_POSSEL_APORT0YCH12, acmpInputAPORT0YCH13 = _ACMP_INPUTSEL_POSSEL_APORT0YCH13, acmpInputAPORT0YCH14 = _ACMP_INPUTSEL_POSSEL_APORT0YCH14, acmpInputAPORT0YCH15 = _ACMP_INPUTSEL_POSSEL_APORT0YCH15, acmpInputAPORT1XCH0 = _ACMP_INPUTSEL_POSSEL_APORT1XCH0, acmpInputAPORT1YCH1 = _ACMP_INPUTSEL_POSSEL_APORT1YCH1, acmpInputAPORT1XCH2 = _ACMP_INPUTSEL_POSSEL_APORT1XCH2, acmpInputAPORT1YCH3 = _ACMP_INPUTSEL_POSSEL_APORT1YCH3, acmpInputAPORT1XCH4 = _ACMP_INPUTSEL_POSSEL_APORT1XCH4, acmpInputAPORT1YCH5 = _ACMP_INPUTSEL_POSSEL_APORT1YCH5, acmpInputAPORT1XCH6 = _ACMP_INPUTSEL_POSSEL_APORT1XCH6, acmpInputAPORT1YCH7 = _ACMP_INPUTSEL_POSSEL_APORT1YCH7, acmpInputAPORT1XCH8 = _ACMP_INPUTSEL_POSSEL_APORT1XCH8, acmpInputAPORT1YCH9 = _ACMP_INPUTSEL_POSSEL_APORT1YCH9, acmpInputAPORT1XCH10 = _ACMP_INPUTSEL_POSSEL_APORT1XCH10, acmpInputAPORT1YCH11 = _ACMP_INPUTSEL_POSSEL_APORT1YCH11, acmpInputAPORT1XCH12 = _ACMP_INPUTSEL_POSSEL_APORT1XCH12, acmpInputAPORT1YCH13 = _ACMP_INPUTSEL_POSSEL_APORT1YCH13, acmpInputAPORT1XCH14 = _ACMP_INPUTSEL_POSSEL_APORT1XCH14, acmpInputAPORT1YCH15 = _ACMP_INPUTSEL_POSSEL_APORT1YCH15, acmpInputAPORT1XCH16 = _ACMP_INPUTSEL_POSSEL_APORT1XCH16, acmpInputAPORT1YCH17 = _ACMP_INPUTSEL_POSSEL_APORT1YCH17, acmpInputAPORT1XCH18 = _ACMP_INPUTSEL_POSSEL_APORT1XCH18, acmpInputAPORT1YCH19 = _ACMP_INPUTSEL_POSSEL_APORT1YCH19, acmpInputAPORT1XCH20 = _ACMP_INPUTSEL_POSSEL_APORT1XCH20, acmpInputAPORT1YCH21 = _ACMP_INPUTSEL_POSSEL_APORT1YCH21, acmpInputAPORT1XCH22 = _ACMP_INPUTSEL_POSSEL_APORT1XCH22, acmpInputAPORT1YCH23 = _ACMP_INPUTSEL_POSSEL_APORT1YCH23, acmpInputAPORT1XCH24 = _ACMP_INPUTSEL_POSSEL_APORT1XCH24, acmpInputAPORT1YCH25 = _ACMP_INPUTSEL_POSSEL_APORT1YCH25, acmpInputAPORT1XCH26 = _ACMP_INPUTSEL_POSSEL_APORT1XCH26, acmpInputAPORT1YCH27 = _ACMP_INPUTSEL_POSSEL_APORT1YCH27, acmpInputAPORT1XCH28 = _ACMP_INPUTSEL_POSSEL_APORT1XCH28, acmpInputAPORT1YCH29 = _ACMP_INPUTSEL_POSSEL_APORT1YCH29, acmpInputAPORT1XCH30 = _ACMP_INPUTSEL_POSSEL_APORT1XCH30, acmpInputAPORT1YCH31 = _ACMP_INPUTSEL_POSSEL_APORT1YCH31, acmpInputAPORT2YCH0 = _ACMP_INPUTSEL_POSSEL_APORT2YCH0, acmpInputAPORT2XCH1 = _ACMP_INPUTSEL_POSSEL_APORT2XCH1, acmpInputAPORT2YCH2 = _ACMP_INPUTSEL_POSSEL_APORT2YCH2, acmpInputAPORT2XCH3 = _ACMP_INPUTSEL_POSSEL_APORT2XCH3, acmpInputAPORT2YCH4 = _ACMP_INPUTSEL_POSSEL_APORT2YCH4, acmpInputAPORT2XCH5 = _ACMP_INPUTSEL_POSSEL_APORT2XCH5, acmpInputAPORT2YCH6 = _ACMP_INPUTSEL_POSSEL_APORT2YCH6, acmpInputAPORT2XCH7 = _ACMP_INPUTSEL_POSSEL_APORT2XCH7, acmpInputAPORT2YCH8 = _ACMP_INPUTSEL_POSSEL_APORT2YCH8, acmpInputAPORT2XCH9 = _ACMP_INPUTSEL_POSSEL_APORT2XCH9, acmpInputAPORT2YCH10 = _ACMP_INPUTSEL_POSSEL_APORT2YCH10, acmpInputAPORT2XCH11 = _ACMP_INPUTSEL_POSSEL_APORT2XCH11, acmpInputAPORT2YCH12 = _ACMP_INPUTSEL_POSSEL_APORT2YCH12, acmpInputAPORT2XCH13 = _ACMP_INPUTSEL_POSSEL_APORT2XCH13, acmpInputAPORT2YCH14 = _ACMP_INPUTSEL_POSSEL_APORT2YCH14, acmpInputAPORT2XCH15 = _ACMP_INPUTSEL_POSSEL_APORT2XCH15, acmpInputAPORT2YCH16 = _ACMP_INPUTSEL_POSSEL_APORT2YCH16, acmpInputAPORT2XCH17 = _ACMP_INPUTSEL_POSSEL_APORT2XCH17, acmpInputAPORT2YCH18 = _ACMP_INPUTSEL_POSSEL_APORT2YCH18, acmpInputAPORT2XCH19 = _ACMP_INPUTSEL_POSSEL_APORT2XCH19, acmpInputAPORT2YCH20 = _ACMP_INPUTSEL_POSSEL_APORT2YCH20, acmpInputAPORT2XCH21 = _ACMP_INPUTSEL_POSSEL_APORT2XCH21, acmpInputAPORT2YCH22 = _ACMP_INPUTSEL_POSSEL_APORT2YCH22, acmpInputAPORT2XCH23 = _ACMP_INPUTSEL_POSSEL_APORT2XCH23, acmpInputAPORT2YCH24 = _ACMP_INPUTSEL_POSSEL_APORT2YCH24, acmpInputAPORT2XCH25 = _ACMP_INPUTSEL_POSSEL_APORT2XCH25, acmpInputAPORT2YCH26 = _ACMP_INPUTSEL_POSSEL_APORT2YCH26, acmpInputAPORT2XCH27 = _ACMP_INPUTSEL_POSSEL_APORT2XCH27, acmpInputAPORT2YCH28 = _ACMP_INPUTSEL_POSSEL_APORT2YCH28, acmpInputAPORT2XCH29 = _ACMP_INPUTSEL_POSSEL_APORT2XCH29, acmpInputAPORT2YCH30 = _ACMP_INPUTSEL_POSSEL_APORT2YCH30, acmpInputAPORT2XCH31 = _ACMP_INPUTSEL_POSSEL_APORT2XCH31, acmpInputAPORT3XCH0 = _ACMP_INPUTSEL_POSSEL_APORT3XCH0, acmpInputAPORT3YCH1 = _ACMP_INPUTSEL_POSSEL_APORT3YCH1, acmpInputAPORT3XCH2 = _ACMP_INPUTSEL_POSSEL_APORT3XCH2, acmpInputAPORT3YCH3 = _ACMP_INPUTSEL_POSSEL_APORT3YCH3, acmpInputAPORT3XCH4 = _ACMP_INPUTSEL_POSSEL_APORT3XCH4, acmpInputAPORT3YCH5 = _ACMP_INPUTSEL_POSSEL_APORT3YCH5, acmpInputAPORT3XCH6 = _ACMP_INPUTSEL_POSSEL_APORT3XCH6, acmpInputAPORT3YCH7 = _ACMP_INPUTSEL_POSSEL_APORT3YCH7, acmpInputAPORT3XCH8 = _ACMP_INPUTSEL_POSSEL_APORT3XCH8, acmpInputAPORT3YCH9 = _ACMP_INPUTSEL_POSSEL_APORT3YCH9, acmpInputAPORT3XCH10 = _ACMP_INPUTSEL_POSSEL_APORT3XCH10, acmpInputAPORT3YCH11 = _ACMP_INPUTSEL_POSSEL_APORT3YCH11, acmpInputAPORT3XCH12 = _ACMP_INPUTSEL_POSSEL_APORT3XCH12, acmpInputAPORT3YCH13 = _ACMP_INPUTSEL_POSSEL_APORT3YCH13, acmpInputAPORT3XCH14 = _ACMP_INPUTSEL_POSSEL_APORT3XCH14, acmpInputAPORT3YCH15 = _ACMP_INPUTSEL_POSSEL_APORT3YCH15, acmpInputAPORT3XCH16 = _ACMP_INPUTSEL_POSSEL_APORT3XCH16, acmpInputAPORT3YCH17 = _ACMP_INPUTSEL_POSSEL_APORT3YCH17, acmpInputAPORT3XCH18 = _ACMP_INPUTSEL_POSSEL_APORT3XCH18, acmpInputAPORT3YCH19 = _ACMP_INPUTSEL_POSSEL_APORT3YCH19, acmpInputAPORT3XCH20 = _ACMP_INPUTSEL_POSSEL_APORT3XCH20, acmpInputAPORT3YCH21 = _ACMP_INPUTSEL_POSSEL_APORT3YCH21, acmpInputAPORT3XCH22 = _ACMP_INPUTSEL_POSSEL_APORT3XCH22, acmpInputAPORT3YCH23 = _ACMP_INPUTSEL_POSSEL_APORT3YCH23, acmpInputAPORT3XCH24 = _ACMP_INPUTSEL_POSSEL_APORT3XCH24, acmpInputAPORT3YCH25 = _ACMP_INPUTSEL_POSSEL_APORT3YCH25, acmpInputAPORT3XCH26 = _ACMP_INPUTSEL_POSSEL_APORT3XCH26, acmpInputAPORT3YCH27 = _ACMP_INPUTSEL_POSSEL_APORT3YCH27, acmpInputAPORT3XCH28 = _ACMP_INPUTSEL_POSSEL_APORT3XCH28, acmpInputAPORT3YCH29 = _ACMP_INPUTSEL_POSSEL_APORT3YCH29, acmpInputAPORT3XCH30 = _ACMP_INPUTSEL_POSSEL_APORT3XCH30, acmpInputAPORT3YCH31 = _ACMP_INPUTSEL_POSSEL_APORT3YCH31, acmpInputAPORT4YCH0 = _ACMP_INPUTSEL_POSSEL_APORT4YCH0, acmpInputAPORT4XCH1 = _ACMP_INPUTSEL_POSSEL_APORT4XCH1, acmpInputAPORT4YCH2 = _ACMP_INPUTSEL_POSSEL_APORT4YCH2, acmpInputAPORT4XCH3 = _ACMP_INPUTSEL_POSSEL_APORT4XCH3, acmpInputAPORT4YCH4 = _ACMP_INPUTSEL_POSSEL_APORT4YCH4, acmpInputAPORT4XCH5 = _ACMP_INPUTSEL_POSSEL_APORT4XCH5, acmpInputAPORT4YCH6 = _ACMP_INPUTSEL_POSSEL_APORT4YCH6, acmpInputAPORT4XCH7 = _ACMP_INPUTSEL_POSSEL_APORT4XCH7, acmpInputAPORT4YCH8 = _ACMP_INPUTSEL_POSSEL_APORT4YCH8, acmpInputAPORT4XCH9 = _ACMP_INPUTSEL_POSSEL_APORT4XCH9, acmpInputAPORT4YCH10 = _ACMP_INPUTSEL_POSSEL_APORT4YCH10, acmpInputAPORT4XCH11 = _ACMP_INPUTSEL_POSSEL_APORT4XCH11, acmpInputAPORT4YCH12 = _ACMP_INPUTSEL_POSSEL_APORT4YCH12, acmpInputAPORT4XCH13 = _ACMP_INPUTSEL_POSSEL_APORT4XCH13, acmpInputAPORT4YCH16 = _ACMP_INPUTSEL_POSSEL_APORT4YCH16, acmpInputAPORT4XCH17 = _ACMP_INPUTSEL_POSSEL_APORT4XCH17, acmpInputAPORT4YCH18 = _ACMP_INPUTSEL_POSSEL_APORT4YCH18, acmpInputAPORT4XCH19 = _ACMP_INPUTSEL_POSSEL_APORT4XCH19, acmpInputAPORT4YCH20 = _ACMP_INPUTSEL_POSSEL_APORT4YCH20, acmpInputAPORT4XCH21 = _ACMP_INPUTSEL_POSSEL_APORT4XCH21, acmpInputAPORT4YCH22 = _ACMP_INPUTSEL_POSSEL_APORT4YCH22, acmpInputAPORT4XCH23 = _ACMP_INPUTSEL_POSSEL_APORT4XCH23, acmpInputAPORT4YCH24 = _ACMP_INPUTSEL_POSSEL_APORT4YCH24, acmpInputAPORT4XCH25 = _ACMP_INPUTSEL_POSSEL_APORT4XCH25, acmpInputAPORT4YCH26 = _ACMP_INPUTSEL_POSSEL_APORT4YCH26, acmpInputAPORT4XCH27 = _ACMP_INPUTSEL_POSSEL_APORT4XCH27, acmpInputAPORT4YCH28 = _ACMP_INPUTSEL_POSSEL_APORT4YCH28, acmpInputAPORT4XCH29 = _ACMP_INPUTSEL_POSSEL_APORT4XCH29, acmpInputAPORT4YCH30 = _ACMP_INPUTSEL_POSSEL_APORT4YCH30, acmpInputAPORT4YCH14 = _ACMP_INPUTSEL_POSSEL_APORT4YCH14, acmpInputAPORT4XCH15 = _ACMP_INPUTSEL_POSSEL_APORT4XCH15, acmpInputAPORT4XCH31 = _ACMP_INPUTSEL_POSSEL_APORT4XCH31, acmpInputDACOUT0 = _ACMP_INPUTSEL_POSSEL_DACOUT0, acmpInputDACOUT1 = _ACMP_INPUTSEL_POSSEL_DACOUT1, acmpInputVLP = _ACMP_INPUTSEL_POSSEL_VLP, acmpInputVBDIV = _ACMP_INPUTSEL_POSSEL_VBDIV, acmpInputVADIV = _ACMP_INPUTSEL_POSSEL_VADIV, acmpInputVDD = _ACMP_INPUTSEL_POSSEL_VDD, acmpInputVSS = _ACMP_INPUTSEL_POSSEL_VSS } | 
| ACMP Input Selection. | |
| enum | ACMP_ExternalInput_Typedef
         
         { acmpExternalInputAPORT0X = _ACMP_EXTIFCTRL_APORTSEL_APORT0X, acmpExternalInputAPORT0Y = _ACMP_EXTIFCTRL_APORTSEL_APORT0Y, acmpExternalInputAPORT1X = _ACMP_EXTIFCTRL_APORTSEL_APORT1X, acmpExternalInputAPORT1Y = _ACMP_EXTIFCTRL_APORTSEL_APORT1Y, acmpExternalInputAPORT1XY = _ACMP_EXTIFCTRL_APORTSEL_APORT1XY, acmpExternalInputAPORT2X = _ACMP_EXTIFCTRL_APORTSEL_APORT2X, acmpExternalInputAPORT2Y = _ACMP_EXTIFCTRL_APORTSEL_APORT2Y, acmpExternalInputAPORT2YX = _ACMP_EXTIFCTRL_APORTSEL_APORT2YX, acmpExternalInputAPORT3X = _ACMP_EXTIFCTRL_APORTSEL_APORT3X, acmpExternalInputAPORT3Y = _ACMP_EXTIFCTRL_APORTSEL_APORT3Y, acmpExternalInputAPORT3XY = _ACMP_EXTIFCTRL_APORTSEL_APORT3XY, acmpExternalInputAPORT4X = _ACMP_EXTIFCTRL_APORTSEL_APORT4X, acmpExternalInputAPORT4Y = _ACMP_EXTIFCTRL_APORTSEL_APORT4Y, acmpExternalInputAPORT4YX = _ACMP_EXTIFCTRL_APORTSEL_APORT4YX } | 
| ACMP external input select. | |
Function Documentation
◆ ACMP_CapsenseInit()
| void ACMP_CapsenseInit | ( | ACMP_TypeDef * | 
            acmp,
            | 
| const ACMP_CapsenseInit_TypeDef * | 
            init
            | ||
| ) | 
Set up ACMP for use in capacitive sense applications.
This function sets up ACMP for use in capacitive sense applications. To use the capacitive sense functionality in the ACMP, use the PRS output of the ACMP module to count the number of oscillations in the capacitive sense circuit (possibly using a TIMER).
- Note
- A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] initA pointer to the initialization structure used to configure ACMP for capacitive sensing operation. 
◆ ACMP_CapsenseChannelSet()
| void ACMP_CapsenseChannelSet | ( | ACMP_TypeDef * | 
            acmp,
            | 
| ACMP_Channel_TypeDef | 
            channel
            | ||
| ) | 
Set the ACMP channel used for capacitive sensing.
- Note
- A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] channelThe ACMP channel to use for capacitive sensing (Possel). 
◆ ACMP_ChannelSet()
| void ACMP_ChannelSet | ( | ACMP_TypeDef * | 
            acmp,
            | 
| ACMP_Channel_TypeDef | 
            negSel,
            | ||
| ACMP_Channel_TypeDef | 
            posSel
            | ||
| ) | 
Set which channels should be used in ACMP comparisons.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. negSelA channel to use on the negative input to the ACMP. posSelA channel to use on the positive input to the ACMP. 
◆ ACMP_Disable()
| void ACMP_Disable | ( | ACMP_TypeDef * | 
            acmp
            | ) | 
Disable ACMP.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. 
◆ ACMP_Enable()
| void ACMP_Enable | ( | ACMP_TypeDef * | 
            acmp
            | ) | 
Enable ACMP.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. 
◆ ACMP_ExternalInputSelect()
| void ACMP_ExternalInputSelect | ( | ACMP_TypeDef * | 
            acmp,
            | 
| ACMP_ExternalInput_Typedef | 
            aport
            | ||
| ) | 
Select and enable external input.
This is used when an external module needs to take control of the ACMP POSSEL field to configure the APORT input for the ACMP. Modules, such as LESENSE, use this to change the ACMP input during a scan sequence.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] aportThis parameter decides which APORT(s) the ACMP will use when it's controlled by an external module. 
◆ ACMP_GPIOSetup()
| void ACMP_GPIOSetup | ( | ACMP_TypeDef * | 
            acmp,
            | 
| uint32_t | 
            location,
            | ||
| bool | 
            enable,
            | ||
| bool | 
            invert
            | ||
| ) | 
Set up GPIO output from ACMP.
- Note
- 
         GPIO must be enabled in the CMU before this function call, i.e.,
         CMU_ClockEnable(cmuClock_GPIO, true); 
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. locationThe pin location to use. See the data sheet for location to pin mappings. enableEnable or disable pin output. invertInvert output. 
◆ ACMP_Init()
| void ACMP_Init | ( | ACMP_TypeDef * | 
            acmp,
            | 
| const ACMP_Init_TypeDef * | 
            init
            | ||
| ) | 
Initialize ACMP.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] initA pointer to the initialization structure used to configure ACMP. 
◆ ACMP_Reset()
| void ACMP_Reset | ( | ACMP_TypeDef * | 
            acmp
            | ) | 
Reset ACMP to the same state that it was in after a hardware reset.
- Note
- The GPIO ACMP ROUTE register is NOT reset by this function to allow for centralized setup of this feature.
- The peripheral may be enabled and disabled during reset.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. 
◆ ACMP_VASetup()
| void ACMP_VASetup | ( | ACMP_TypeDef * | 
            acmp,
            | 
| const ACMP_VAConfig_TypeDef * | 
            vaconfig
            | ||
| ) | 
Set up the VA source.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] vaconfigA pointer to the structure used to configure the VA source. This structure contains the input source and the 2 divider values. 
◆ ACMP_VBSetup()
| void ACMP_VBSetup | ( | ACMP_TypeDef * | 
            acmp,
            | 
| const ACMP_VBConfig_TypeDef * | 
            vbconfig
            | ||
| ) | 
Set up the VB Source.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] vbconfigA pointer to the structure used to configure the VB source. This structure contains the input source and the 2 divider values. 
◆ ACMP_IntClear()
| 
 | inline | 
Clear one or more pending ACMP interrupts.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] flagsPending ACMP interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFC_EDGE or ACMP_IFC_WARMUP. 
◆ ACMP_IntDisable()
| 
 | inline | 
Disable one or more ACMP interrupts.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] flagsACMP interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP. 
◆ ACMP_IntEnable()
| 
 | inline | 
Enable one or more ACMP interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using ACMP_IntClear() prior to enabling if a pending interrupt should be ignored.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] flagsACMP interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP. 
◆ ACMP_IntGet()
| 
 | inline | 
Get pending ACMP interrupt flags.
- Note
- This function does not clear event bits.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. 
- Returns
- Pending ACMP interrupt sources. A bitwise logic OR combination of valid interrupt flags for the ACMP module. The pending interrupt sources can be, for instance, ACMP_IF_EDGE or ACMP_IF_WARMUP.
◆ ACMP_IntGetEnabled()
| 
 | inline | 
Get enabled and pending ACMP interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. 
- Note
- This function does not clear interrupt flags.
- Returns
- 
         Pending and enabled ACMP interrupt sources. The return value is the bitwise AND combination of
         - the OR combination of enabled interrupt sources in ACMPx_IEN_nnn register (ACMPx_IEN_nnn) and
- the OR combination of valid interrupt flags of the ACMP module (ACMPx_IF_nnn).
 
◆ ACMP_IntSet()
| 
 | inline | 
Set one or more pending ACMP interrupts from software.
- Parameters
- 
         [in] acmpA pointer to the ACMP peripheral register block. [in] flagsACMP interrupt sources to set as pending. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFS_EDGE or ACMP_IFS_WARMUP. 
Macro Definition Documentation
◆ ACMP_CAPSENSE_INIT_DEFAULT
| #define ACMP_CAPSENSE_INIT_DEFAULT | 
A default configuration for capacitive sense mode initialization.
◆ ACMP_INIT_DEFAULT
| #define ACMP_INIT_DEFAULT | 
Default configuration for ACMP regular initialization.
◆ ACMP_VACONFIG_DEFAULT
| #define ACMP_VACONFIG_DEFAULT | 
VA default configuration.
◆ ACMP_VBCONFIG_DEFAULT
| #define ACMP_VBCONFIG_DEFAULT | 
VB default configuration.
Enumeration Type Documentation
◆ ACMP_CapsenseResistor_TypeDef
Resistor values used for the internal capacitive sense resistor.
See data sheet for your device for details on each resistor value.
◆ ACMP_HysteresisLevel_TypeDef
Hysteresis level.
See data sheet for your device for details on each level.
◆ ACMP_InputRange_TypeDef
◆ ACMP_PowerSource_TypeDef
◆ ACMP_Accuracy_TypeDef
◆ ACMP_VAInput_TypeDef
| enum ACMP_VAInput_TypeDef | 
ACMP input to the VA divider.
This enumeration is used to select the input for the VA Divider.
◆ ACMP_VBInput_TypeDef
| enum ACMP_VBInput_TypeDef | 
◆ ACMP_VLPInput_Typedef
◆ ACMP_Channel_TypeDef
| enum ACMP_Channel_TypeDef | 
ACMP Input Selection.
◆ ACMP_ExternalInput_Typedef
ACMP external input select.
This type is used to select which APORT is used by an external module, such as LESENSE, when it's taking control over the ACMP input.