EUSART_IrDAInit_TypeDef Struct Reference
IrDA Initialization structure.
      
       #include <em_eusart.h>
      
     
| Data Fields | |
| EUSART_UartInit_TypeDef | init | 
| General EUSART initialization structure. | |
| bool | irDALowFrequencyEnable | 
| Enable the IrDA low frequency mode. Only RX operation are enabled. | |
| EUSART_IrDARxFilterEnable_TypeDef | irDARxFilterEnable | 
| Set to enable filter on IrDA demodulator. | |
| EUSART_IrDAPulseWidth_Typedef | irDAPulseWidth | 
| Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period. | |
IrDA Initialization structure.
Field Documentation
◆ init
| EUSART_UartInit_TypeDef EUSART_IrDAInit_TypeDef::init | 
General EUSART initialization structure.
◆ irDALowFrequencyEnable
| bool EUSART_IrDAInit_TypeDef::irDALowFrequencyEnable | 
Enable the IrDA low frequency mode. Only RX operation are enabled.
◆ irDARxFilterEnable
| EUSART_IrDARxFilterEnable_TypeDef EUSART_IrDAInit_TypeDef::irDARxFilterEnable | 
Set to enable filter on IrDA demodulator.
◆ irDAPulseWidth
| EUSART_IrDAPulseWidth_Typedef EUSART_IrDAInit_TypeDef::irDAPulseWidth | 
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.