QSPI_Init_TypeDef Struct Reference

QSPI initialization structure.

#include <em_qspi.h>

Data Fields

bool enable
 Enable/disable Quad SPI when initialization is completed.
 
uint8_t divisor
 Master mode baud rate divisor.
 

QSPI initialization structure.

Field Documentation

◆ enable

bool QSPI_Init_TypeDef::enable

Enable/disable Quad SPI when initialization is completed.

◆ divisor

uint8_t QSPI_Init_TypeDef::divisor

Master mode baud rate divisor.

Values can be even numbers in the range [2-32] inclusive.