SWO Debug
Description
Serial Wire Output Debug Configuration.
Initializes Serial Wire Output using the DWT and ITM peripherals of Cortex-M processors. Configures output of Program Counter samples, interrupt events, and data over any ITM channel.
Functions | |
sl_status_t | sl_debug_swo_init (void) |
Initialize SWO Debug. | |
sl_status_t | sl_debug_swo_enable_itm (uint32_t channel) |
Enable an ITM channel. | |
sl_status_t | sl_debug_swo_disable_itm (uint32_t channel) |
Disable an ITM channel. | |
sl_status_t | sl_debug_swo_write_u8 (uint32_t channel, uint8_t byte) |
Write a byte to an ITM channel. | |
sl_status_t | sl_debug_swo_write_u16 (uint32_t channel, uint16_t half_word) |
Write a half-word to an ITM channel. | |
sl_status_t | sl_debug_swo_write_u32 (uint32_t channel, uint32_t word) |
Write a word to an ITM channel. | |
Macros | |
#define | sl_debug_swo_write sl_debug_swo_write_u8 |
alias for backward compatibility | |
Function Documentation
◆ sl_debug_swo_init()
sl_status_t sl_debug_swo_init | ( | void |
| ) |
Initialize SWO Debug.
Initializes SWO debug using configuration parameters for frequency, as well as whether PC sample events and interrupt events should be emitted.
- Note
- This function does not enable any software stimulus ports in the ITM. This can be done by calling sl_debug_swo_enable_itm or by using sl_debug_swo_write which enables the necessary ports automatically.
- Returns
- Status code
- Return values
-
SL_STATUS_OK
SWO initialized successfully
◆ sl_debug_swo_enable_itm()
sl_status_t sl_debug_swo_enable_itm | ( | uint32_t | channel | ) |
Enable an ITM channel.
Enables the given ITM channel in the Trace Enable Register.
- Parameters
-
[in] channel
ITM channel number
- Returns
- Status code
- Return values
-
SL_STATUS_OK
ITM channel enabled successfully
◆ sl_debug_swo_disable_itm()
sl_status_t sl_debug_swo_disable_itm | ( | uint32_t | channel | ) |
Disable an ITM channel.
Disables the given ITM channel in the Trace Enable Register.
- Parameters
-
[in] channel
ITM channel number
- Returns
- Status code
- Return values
-
SL_STATUS_OK
ITM channel disabled successfully
◆ sl_debug_swo_write_u8()
sl_status_t sl_debug_swo_write_u8 | ( | uint32_t | channel, |
uint8_t | byte |
||
) |
Write a byte to an ITM channel.
Writes the given byte to the given ITM channel
- Note
- This function ensures that the ITM channel is enabled, and enables it if it wasn't already. Note that even if the debug port is locked, the byte will still be written on the SWO.
- Parameters
-
[in] channel
ITM channel number [in] byte
Byte to send
- Returns
- Status code
- Return values
-
SL_STATUS_OK
Byte sent successfully SL_STATUS_NOT_INITIALIZED
ITM has not been enabled, call sl_debug_swo_init first.
◆ sl_debug_swo_write_u16()
sl_status_t sl_debug_swo_write_u16 | ( | uint32_t | channel, |
uint16_t | half_word |
||
) |
Write a half-word to an ITM channel.
Writes the given half-word to the given ITM channel
- Note
- This function ensures that the ITM channel is enabled, and enables it if it wasn't already.
- Parameters
-
[in] channel
ITM channel number [in] half_word
Half-word to send
- Returns
- Status code
- Return values
-
SL_STATUS_OK
half-word sent successfully SL_STATUS_NOT_INITIALIZED
ITM has not been enabled, call sl_debug_swo_init first.
◆ sl_debug_swo_write_u32()
sl_status_t sl_debug_swo_write_u32 | ( | uint32_t | channel, |
uint32_t | word |
||
) |
Write a word to an ITM channel.
Writes the given word to the given ITM channel
- Note
- This function ensures that the ITM channel is enabled, and enables it if it wasn't already.
- Parameters
-
[in] channel
ITM channel number [in] word
Word to send
- Returns
- Status code
- Return values
-
SL_STATUS_OK
half-word sent successfully SL_STATUS_NOT_INITIALIZED
ITM has not been enabled, call sl_debug_swo_init first.
Macro Definition Documentation
◆ sl_debug_swo_write
#define sl_debug_swo_write sl_debug_swo_write_u8 |
alias for backward compatibility