GLIB - Graphics Library
Description
Silicon Labs Graphics Library.
Graphics Library
Silicon Labs Graphics Library. Feature rich graphics library for memory constrained applications.
Introduction
GLIB is a graphics library that can be used to draw pixels, common shapes, text or bitmaps to a display connected to an MCU. The main goal of this library is easy of use and small code and memory footprint. In this way GLIB can be used on even the smallest Cortex-M0 devices.
GLIB treats the display as a matrix of pixels which is a model of the physical display. This matrix is exposed to GLIB via an API called DMD (Dot Matrix Display). So in order to draw something on a physical display the user application needs to provide GLIB with a single implementation of the DMD interface. Sample DMD implementations are provided for the displays that are connected to the Silion Labs Starter Kits and the Silicon Labs Development Kits.
Initialization
There are two things that must be initialized before GLIB can be used to draw pixels on the display. First the user needs to initialize the DMD implementation for the actual hardware display which is used. This initialization is display hardware specific.
After the DMD is initialized the user needs to initialize a GLIB_Context_t that can be used for all the drawing operations. A GLIB_Context_t structure is initialized using the GLIB_contextInit() function.
Every GLIB drawing function will require a GLIB_Context_t as one of the functions arguments. The GBLI context contains important configuration values that all the drawing functions use. It contains the foreground and background color, and it also contains information on what font to use when rendering text on the display.
Color
GLIB represent color in a pixel as three 8 bit color values representing red, green and blue, giving the user support for a 24 bit color depth. The GLIB_rgbColor() function can be used to convert from distinct red, green and blue values to an 32-bit integer representing the color of single pixel. Similarly the GLIB_colorTranslate24bpp() function can be used to convert from the 32-bit integer representation into the 3 separate red, green and blue components. The 32-bit integer representation of a pixel color is used when configuring the foreground and background color.
GLIB also contains some common predefined colors for use in places where a 32-bit integer is used to represent the color. These predefined colors include White, Black, Brown, Orange, and many more. See the GLIB Colors for the full list of colors.
Some displays are monochrome, meaning that they only support 2 colors. When using GLIB to draw shapes on these displays the applications should use only the 2 colors White and Black.
Draw Shapes
GLIB contains functions for drawing common shapes to a display. Here is a list containing all the drawing functions.
- GLIB_drawCircle(). Draw a circle outline with the foreground color.
- GLIB_drawCircleFilled(). Draw a circle filled with the foreground color.
- GLIB_drawPartialCircle(). Draw specific octants of a circle with the foreground color.
- GLIB_drawLine(). Draw line with the foreground color.
- GLIB_drawLineH(). Draw a horizontal line.
- GLIB_drawLineV(). Draw a vertical line.
- GLIB_drawRect(). Draw a rectangle outline with the foreground color.
- GLIB_drawRectFilled(). Draw a filled rectangle using the foreground color.
- GLIB_drawPolygon(). Draw lines between all the points in the given set using the foreground color.
- GLIB_drawPolygonFilled(). Draw filled polygon between points.
Draw Pixels
These are functions that GLIB provides for drawing one pixel.
- GLIB_drawPixel(). Draw a pixel using the foreground color.
- GLIB_drawPixelRGB(). Draw a single pixel using a specific color.
- GLIB_drawPixelColor(). Draw a single pixel using a specific color.
Font rendering
GLIB Supports fixed width font rendering. The functions GLIB_drawString() and GLIB_drawChar() are used to render text on the display.
GLIB provides these fonts for the user
- GLIB_FontNormal8x8 A normal 8x8 pixel font which is the defaul font if nothing else is configured.
- GLIB_FontNarrow6x8 A narrow 6x8 pixel font which can be used if the default font is to wide.
- GLIB_FontNumber16x20 A large font for use with only numbers. This font is 16x20 pixels.
To change the font the user calls GLIB_setFont() with a pointer to a GLIB_Font_t structure which describes the whole font. The GLIB_Font_t structure contains a pointer to the bitmap for each character and it describes attributes of the font like the width and height of each character and it also contains the bitmap of each character.
Draw Bitmap
To draw an image or custom bitmaps on the display the GLIB_drawBitmap() function can be used. The color displays typically use a bitmap format where each pixel is represented by 3 consecutive bytes representing the red, green and blue color components. While monochrome displays typically use a bitmap format where 1 byte represents 8 pixels where a 1 bit is white and a 0 bit is black. Note that bitmaps are insensitive to the foreground and background color settings, and that the format of the bitmap depends on the DMD implementation of the display.
Example
This examples shows how to initialize a GLIB context and draw something on a display.
Modules | |
DMD - Dot Matrix Display | |
Hardware abstraction layer for dot matrix displays. | |
GLIB BMP | |
Bitmap Support. | |
GLIB Colors | |
Predefined Colors. | |
Data Structures | |
struct | __GLIB_Font_t |
Font definition structure. | |
struct | __GLIB_Rectangle_t |
Rectangle structure. | |
struct | __GLIB_Context_t |
GLIB Drawing Context (Multiple instances of GLIB_Context_t can exist) | |
Functions | |
EMSTATUS | GLIB_contextInit (GLIB_Context_t *pContext) |
Initialize the GLIB_Context_t. | |
EMSTATUS | GLIB_displayWakeUp (void) |
Returns the display from sleep mode. | |
EMSTATUS | GLIB_displaySleep (void) |
Sets the display in sleep mode. | |
EMSTATUS | GLIB_clear (GLIB_Context_t *pContext) |
Clears the display with the background color of the GLIB_Context_t. | |
EMSTATUS | GLIB_clearRegion (const GLIB_Context_t *pContext) |
Clears the clipping region by filling it with the background color of the GLIB_Context_t. | |
EMSTATUS | GLIB_resetDisplayClippingArea (GLIB_Context_t *pContext) |
Reset the display driver clipping area to the whole display. | |
EMSTATUS | GLIB_resetClippingRegion (GLIB_Context_t *pContext) |
Reset the GLIB_Context_t clipping region to the whole display. | |
EMSTATUS | GLIB_applyClippingRegion (const GLIB_Context_t *pContext) |
Apply the clipping region from the GLIB_Context_t in the DMD driver. | |
void | GLIB_colorTranslate24bpp (uint32_t color, uint8_t *red, uint8_t *green, uint8_t *blue) |
Extracts the color components from the 32-bit color passed and puts them in the passed in 8-bits ints. | |
uint32_t | GLIB_rgbColor (uint8_t red, uint8_t green, uint8_t blue) |
Convert 3 uint8_t color components into a 24-bit color. | |
bool | GLIB_rectContainsPoint (const GLIB_Rectangle_t *pRect, int32_t xCenter, int32_t yCenter) |
Checks if the point passed in is in the interior of the rectangle passed in. | |
void | GLIB_normalizeRect (GLIB_Rectangle_t *pRect) |
Normalize the rectangle that is passed in. | |
EMSTATUS | GLIB_setClippingRegion (GLIB_Context_t *pContext, const GLIB_Rectangle_t *pRect) |
Sets the clippingRegion of the passed in GLIB_Context_t. | |
EMSTATUS | GLIB_drawCircle (GLIB_Context_t *pContext, int32_t x, int32_t y, uint32_t radius) |
Draws a circle with center at x, y, and a radius. | |
EMSTATUS | GLIB_drawCircleFilled (GLIB_Context_t *pContext, int32_t x, int32_t y, uint32_t radius) |
Draws a filled circle with center at x, y, and a radius. | |
EMSTATUS | GLIB_drawPartialCircle (GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, uint32_t radius, uint8_t bitMask) |
Draws a partial circle with center at x, y, and a radius. | |
EMSTATUS | GLIB_setFont (GLIB_Context_t *pContext, GLIB_Font_t *pFont) |
Set new font for the library. | |
EMSTATUS | GLIB_drawString (GLIB_Context_t *pContext, const char *pString, uint32_t sLength, int32_t x0, int32_t y0, bool opaque) |
Draws a string using the font supplied with the library. | |
EMSTATUS | GLIB_drawStringOnLine (GLIB_Context_t *pContext, const char *pString, uint8_t line, GLIB_Align_t align, int32_t xOffset, int32_t yOffset, bool opaque) |
Draws a string on the specified line on the display. | |
EMSTATUS | GLIB_drawChar (GLIB_Context_t *pContext, char myChar, int32_t x, int32_t y, bool opaque) |
Draws a char using the font supplied with the library. | |
EMSTATUS | GLIB_drawBitmap (GLIB_Context_t *pContext, int32_t x, int32_t y, uint32_t width, uint32_t height, const uint8_t *picData) |
Draws a bitmap. | |
void | GLIB_invertBitmap (GLIB_Context_t *pContext, uint32_t bitmapSize, uint8_t *picData) |
Inverts each bit of the bitmap. | |
EMSTATUS | GLIB_drawLine (GLIB_Context_t *pContext, int32_t x1, int32_t y1, int32_t x2, int32_t y2) |
Draws a line from x1,y1 to x2, y2. | |
EMSTATUS | GLIB_drawLineH (GLIB_Context_t *pContext, int32_t x1, int32_t y1, int32_t x2) |
Draws a horizontal line from x1, y1 to x2, y2. | |
EMSTATUS | GLIB_drawLineV (GLIB_Context_t *pContext, int32_t x1, int32_t y1, int32_t y2) |
Draws a vertical line from x1, y1 to x1, y2. | |
EMSTATUS | GLIB_drawRect (GLIB_Context_t *pContext, const GLIB_Rectangle_t *pRect) |
Draws a rectangle outline defined by the passed in rectangle. | |
EMSTATUS | GLIB_drawRectFilled (GLIB_Context_t *pContext, const GLIB_Rectangle_t *pRect) |
Draws a filled rectangle defined by the passed in rectangle. | |
EMSTATUS | GLIB_drawPolygon (GLIB_Context_t *pContext, uint32_t numPoints, const int32_t *polyPoints) |
Draws a polygon using Bresnham's Midpoint Line Algorithm. | |
EMSTATUS | GLIB_drawPolygonFilled (GLIB_Context_t *pContext, uint32_t numPoints, const int32_t *polyPoints) |
Draws a filled polygon using a scan line algorithm. | |
EMSTATUS | GLIB_drawPixelRGB (GLIB_Context_t *pContext, int32_t x, int32_t y, uint8_t red, uint8_t green, uint8_t blue) |
Draws a pixel at x, y with color defined by red, green and blue 1 byte per channel. | |
EMSTATUS | GLIB_drawPixel (GLIB_Context_t *pContext, int32_t x, int32_t y) |
Draws a pixel at x, y using foregroundColor defined in the GLIB_Context_t. | |
EMSTATUS | GLIB_drawPixelColor (GLIB_Context_t *pContext, int32_t x, int32_t y, uint32_t color) |
Draws a pixel at x, y using the color parameter. | |
Macros | |
#define | ECODE_GLIB_BASE 0x00000000 |
GLIB Base error code. | |
#define | GLIB_OK 0x00000000 |
Successful call. | |
#define | GLIB_ERROR_NOTHING_TO_DRAW (ECODE_GLIB_BASE | 0x0001) |
Function did not draw. | |
#define | GLIB_ERROR_INVALID_CHAR (ECODE_GLIB_BASE | 0x0002) |
Invalid char. | |
#define | GLIB_OUT_OF_BOUNDS (ECODE_GLIB_BASE | 0x0003) |
Coordinates out of bounds. | |
#define | GLIB_ERROR_INVALID_CLIPPINGREGION (ECODE_GLIB_BASE | 0x0004) |
Invalid coordinates (ex. | |
#define | GLIB_ERROR_INVALID_ARGUMENT (ECODE_GLIB_BASE | 0x0005) |
Invalid argument. | |
#define | GLIB_ERROR_OUT_OF_MEMORY (ECODE_GLIB_BASE | 0x0006) |
Out of memory. | |
#define | GLIB_ERROR_FILE_NOT_SUPPORTED (ECODE_GLIB_BASE | 0x0007) |
File not supported. | |
#define | GLIB_ERROR_IO (ECODE_GLIB_BASE | 0x0008) |
General IO Error. | |
#define | GLIB_ERROR_INVALID_FILE (ECODE_GLIB_BASE | 0x0009) |
Invalid file. | |
Enumerations | |
enum | __GLIB_Font_Class { InvalidFont = 0, FullFont, NumbersOnlyFont } |
Font classes. | |
enum | __GLIB_Align { GLIB_ALIGN_LEFT, GLIB_ALIGN_CENTER, GLIB_ALIGN_RIGHT } |
Alignment types. | |
Function Documentation
◆ GLIB_contextInit()
EMSTATUS GLIB_contextInit | ( | GLIB_Context_t * | pContext | ) |
Initialize the GLIB_Context_t.
The context is set to default values and gets information about the display from the display driver.
- Parameters
-
pContext
Pointer to a GLIB_Context_t
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_displayWakeUp()
EMSTATUS GLIB_displayWakeUp | ( |
| ) |
Returns the display from sleep mode.
- Returns
- Returns DMD_OK on success, or else error code
◆ GLIB_displaySleep()
EMSTATUS GLIB_displaySleep | ( |
| ) |
Sets the display in sleep mode.
- Returns
- Returns DMD_OK on success, or else error code
◆ GLIB_clear()
EMSTATUS GLIB_clear | ( | GLIB_Context_t * | pContext | ) |
Clears the display with the background color of the GLIB_Context_t.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the background color.
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_clearRegion()
EMSTATUS GLIB_clearRegion | ( | const GLIB_Context_t * | pContext | ) |
Clears the clipping region by filling it with the background color of the GLIB_Context_t.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the background color.
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_resetDisplayClippingArea()
EMSTATUS GLIB_resetDisplayClippingArea | ( | GLIB_Context_t * | pContext | ) |
Reset the display driver clipping area to the whole display.
- Parameters
-
pContext
Pointer to a GLIB_Context_t
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_resetClippingRegion()
EMSTATUS GLIB_resetClippingRegion | ( | GLIB_Context_t * | pContext | ) |
Reset the GLIB_Context_t clipping region to the whole display.
- Parameters
-
pContext
Pointer to a GLIB_Context_t
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_applyClippingRegion()
EMSTATUS GLIB_applyClippingRegion | ( | const GLIB_Context_t * | pContext | ) |
Apply the clipping region from the GLIB_Context_t in the DMD driver.
- Parameters
-
pContext
Pointer to a GLIB_Context_t
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_colorTranslate24bpp()
void GLIB_colorTranslate24bpp | ( | uint32_t | color, |
uint8_t * | red, |
||
uint8_t * | green, |
||
uint8_t * | blue |
||
) |
Extracts the color components from the 32-bit color passed and puts them in the passed in 8-bits ints.
The color is 24-bit RGB.
Example: color = 0x00FFFF00 -> red = 0xFF, green = 0xFF, blue = 0x00.
- Parameters
-
color
The color which is to be translated red
Pointer to a uint8_t holding the red component green
Pointer to a uint8_t holding the green component blue
Pointer to a uint8_t holding the blue component
◆ GLIB_rgbColor()
uint32_t GLIB_rgbColor | ( | uint8_t | red, |
uint8_t | green, |
||
uint8_t | blue |
||
) |
Convert 3 uint8_t color components into a 24-bit color.
Example: red = 0xFF, green = 0xFF, blue = 0x00 -> 0x00FFFF00 = Yellow
- Parameters
-
red
Red component green
Green component blue
Blue component
- Returns
- Returns a 32-bit unsigned integer representing the color. The 8 LSB is blue, the next 8 is green and the next 8 is red. 0x00RRGGBB
◆ GLIB_rectContainsPoint()
bool GLIB_rectContainsPoint | ( | const GLIB_Rectangle_t * | pRect, |
int32_t | x, |
||
int32_t | y |
||
) |
Checks if the point passed in is in the interior of the rectangle passed in.
If the point is on the edge of the rectangle the function returns 1.
- Parameters
-
pRect
Pointer to a rectangle structure x
X-coordinate of point y
Y-coordinate of point
- Returns
- Returns false if coordinate is outside the rectangle
- Returns true otherwise
◆ GLIB_normalizeRect()
void GLIB_normalizeRect | ( | GLIB_Rectangle_t * | pRect | ) |
Normalize the rectangle that is passed in.
Sets yMin to the minimum value of yMin and yMax. Sets yMax to the maximum value of yMin and yMax. And the same for xMin and xMax
- Parameters
-
pRect
Pointer to a rectangle structure
◆ GLIB_setClippingRegion()
EMSTATUS GLIB_setClippingRegion | ( | GLIB_Context_t * | pContext, |
const GLIB_Rectangle_t * | pRect |
||
) |
Sets the clippingRegion of the passed in GLIB_Context_t.
- Parameters
-
pContext
Pointer to a GLIB_Context_t pRect
Pointer to a GLIB_Rectangle_t which is the clipping region to be set.
- Returns
- Returns GLIB_OK on success
- Returns GLIB_ERROR_INVALID_CLIPPINGREGION if invalid coordinates
- Returns GLIB_OUT_OF_BOUNDS if clipping region is bigger than display clipping area
◆ GLIB_drawCircle()
EMSTATUS GLIB_drawCircle | ( | GLIB_Context_t * | pContext, |
int32_t | xCenter, |
||
int32_t | yCenter, |
||
uint32_t | radius |
||
) |
Draws a circle with center at x, y, and a radius.
Draws a circle using the Midpoint Circle Algorithm. See Wikipedia for algorithm. Algorithm is optimized to use only integer arithmetic, so no floating point arithmetic is needed.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the circle is drawn. The circle is drawn using the foreground color. xCenter
Center x-coordinate yCenter
Center y-coordinate radius
Radius of the circle
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawCircleFilled()
EMSTATUS GLIB_drawCircleFilled | ( | GLIB_Context_t * | pContext, |
int32_t | xCenter, |
||
int32_t | yCenter, |
||
uint32_t | radius |
||
) |
Draws a filled circle with center at x, y, and a radius.
Draws a circle using the Midpoint Circle Algorithm and using horizontal lines. See Wikipedia for algorithm.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the circle is drawn. The circle is drawn using the foreground color. xCenter
Center x-coordinate yCenter
Center y-coordinate radius
Radius of the circle
- Returns
- Returns GLIB_OK on succes. Returns GLIB_ERROR_NOTHING_TO_DRAW if none of the pixel coordinates were inside the clipping region. Returns error code otherwise.
◆ GLIB_drawPartialCircle()
EMSTATUS GLIB_drawPartialCircle | ( | GLIB_Context_t * | pContext, |
int32_t | xCenter, |
||
int32_t | yCenter, |
||
uint32_t | radius, |
||
uint8_t | bitMask |
||
) |
Draws a partial circle with center at x, y, and a radius.
Draws a partial circle using the Midpoint Circle Algorithm. Algorithm is optimized to use only integer arithmetic, so no floating point arithmetic is needed. The bitMask passed in decides which octant that should be drawn. The octants is numbered 1 to 8 in counterclockwise order.
Example: bitMask == 4 draws only pixels in 3. octant (00000100). bitMask == 5 draws only pixels in 3. and 1. octant (00000101).
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the circle is drawn. The circle is drawn using the foreground color. xCenter
Center x-coordinate yCenter
Center y-coordinate radius
Radius of the circle bitMask
Bitmask which decides which octants pixels should be drawn. The LSB is 1. octant, and the MSB is 8. octant.
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_setFont()
EMSTATUS GLIB_setFont | ( | GLIB_Context_t * | pContext, |
GLIB_Font_t * | pFont |
||
) |
Set new font for the library.
Note that GLIB defines a default font in glib.c. Redefine GLIB_DEFAULT_FONT to change the default font.
- Parameters
-
pContext
Pointer to the GLIB_Context_t pFont
Pointer to the new font
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawString()
EMSTATUS GLIB_drawString | ( | GLIB_Context_t * | pContext, |
const char * | pString, |
||
uint32_t | sLength, |
||
int32_t | x0, |
||
int32_t | y0, |
||
bool | opaque |
||
) |
Draws a string using the font supplied with the library.
- Parameters
-
pContext
Pointer to a GLIB_Context_t pString
Pointer to the string that is drawn sLength
number of characters in the string x0
Start x-coordinate for the string (Upper left corner) y0
Start y-coordinate for the string (Upper left corner) opaque
Determines whether to show the background or color it with the background color specified by the GLIB_Context_t. If opaque == 1, the background color is used.
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawStringOnLine()
EMSTATUS GLIB_drawStringOnLine | ( | GLIB_Context_t * | pContext, |
const char * | pString, |
||
uint8_t | line, |
||
GLIB_Align_t | align, |
||
int32_t | xOffset, |
||
int32_t | yOffset, |
||
bool | opaque |
||
) |
Draws a string on the specified line on the display.
- Parameters
-
pContext
Pointer to a GLIB_Context_t pString
Pointer to the string that is drawn line
Specifies which line on the display to draw on. align
Horizontal alignment of the string on the line. This can be left, right or center. Note that left alignment is default. xOffset
This parameter can be used to create a margin on the left or right side of the string. Note that this argument accepts a negative value which can be useful when aligning the string to the right. yOffset
This parameter can be used to move the string further down or up a certain number of pixels. A positive value would move the string down, while a negative value would move the string up. opaque
Determines whether to show the background or color it with the background color specified by the GLIB_Context_t. If opaque == 1, the background color is used.
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawChar()
EMSTATUS GLIB_drawChar | ( | GLIB_Context_t * | pContext, |
char | myChar, |
||
int32_t | x, |
||
int32_t | y, |
||
bool | opaque |
||
) |
Draws a char using the font supplied with the library.
- Parameters
-
pContext
Pointer to the GLIB_Context_t myChar
Char to be drawn x
Start x-coordinate for the char (Upper left corner) y
Start y-coordinate for the char (Upper left corner) opaque
Determines whether to show the background or color it with the background color specified by the GLIB_Context_t. If opaque == true, the background color is used.
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawBitmap()
EMSTATUS GLIB_drawBitmap | ( | GLIB_Context_t * | pContext, |
int32_t | x, |
||
int32_t | y, |
||
uint32_t | width, |
||
uint32_t | height, |
||
const uint8_t * | picData |
||
) |
Draws a bitmap.
Sets up a bitmap that starts at x0,y0 and draws bitmap.
For monochrome displays, each 8-bit element contains 8 pixel values. A bit value of 1 indicates a white pixel, while 0 indicates a black pixel. Note that this format may vary with the DMD implementation.
For 3-bit RGB displays, each bit in the array are one color component (red, green and blue) of the pixel, so that 3 bits represent one pixel (0xBGR). Pixel 0: Bits 2:0 (0bBGR) of byte 0 Pixel 1: Bits 5:3 (0bBGR) of byte 0 Pixel 2: Bits 7:6 (0bGR) of byte 0 and bit 0 (0bB) of byte 1 Pixel 3: Bits 3:1 (0bBGR) of byte 1 ...
For RGB displays with 8-bits per color, each pixel is represented by 24-bits, with one byte for each of the red, green and blue components. The data has to be organized like this: picData = { R, G, B, R, G, B, R, G, B ... }
The pixels are ordered by increasing x coordinate, after the last pixel of a row, the next pixel will be the first pixel on the next row.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the bitmap is drawn. x
Start x-coordinate for bitmap y
Start y-coordinate for bitmap width
Width of picture height
Height of picture picData
Bitmap data
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_invertBitmap()
void GLIB_invertBitmap | ( | GLIB_Context_t * | pContext, |
uint32_t | bitmapSize, |
||
uint8_t * | picData |
||
) |
Inverts each bit of the bitmap.
For monochrome displays, the result is an inversion of the image.
For RGB displays, the result is the negative of the input image.
- Note
- The function inverts entire bytes, meaning that any bits contained within the array that may not be part of the image will also be inverted.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the bitmap is drawn. bitmapSize
Size of the bitmap array in terms of bytes. picData
Bitmap data.
◆ GLIB_drawLine()
EMSTATUS GLIB_drawLine | ( | GLIB_Context_t * | pContext, |
int32_t | x1, |
||
int32_t | y1, |
||
int32_t | x2, |
||
int32_t | y2 |
||
) |
Draws a line from x1,y1 to x2, y2.
Draws a straight line using the Bresnham's Midpoint Line Algorithm. Checks for vertical and horizontal line.
- Parameters
-
pContext
Pointer to the GLIB_Context_t which holds the clipping region x1
Start x-coordinate y1
Start y-coordinate x2
End x-coordinate y2
End y-coordinate
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawLineH()
EMSTATUS GLIB_drawLineH | ( | GLIB_Context_t * | pContext, |
int32_t | x1, |
||
int32_t | y1, |
||
int32_t | x2 |
||
) |
Draws a horizontal line from x1, y1 to x2, y2.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the line is drawn. The line is drawn using the foreground color. x1
Start x-coordinate y1
Start y-coordinate x2
End x-coordinate
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawLineV()
EMSTATUS GLIB_drawLineV | ( | GLIB_Context_t * | pContext, |
int32_t | x1, |
||
int32_t | y1, |
||
int32_t | y2 |
||
) |
Draws a vertical line from x1, y1 to x1, y2.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which the line is drawn. The line is drawn using the foreground color. x1
Start x-coordinate y1
Start y-coordinate y2
End y-coordinate
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawRect()
EMSTATUS GLIB_drawRect | ( | GLIB_Context_t * | pContext, |
const GLIB_Rectangle_t * | pRect |
||
) |
Draws a rectangle outline defined by the passed in rectangle.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the rectangle is drawn. The rectangle is drawn using the foreground color. pRect
Pointer to a rectangle structure
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawRectFilled()
EMSTATUS GLIB_drawRectFilled | ( | GLIB_Context_t * | pContext, |
const GLIB_Rectangle_t * | pRect |
||
) |
Draws a filled rectangle defined by the passed in rectangle.
The filled rectangle is drawn from (xMin, yMin) to (xMax, yMax), inclusive, of the rectangle passed in.
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the rectangle is drawn. The rectangle is filled with the foreground color. pRect
Pointer to a rectangle structure
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawPolygon()
EMSTATUS GLIB_drawPolygon | ( | GLIB_Context_t * | pContext, |
uint32_t | numPoints, |
||
const int32_t * | polyPoints |
||
) |
Draws a polygon using Bresnham's Midpoint Line Algorithm.
This function draws a line between all points outlining the polygon. The first and last point doesn't have to be the same. The function automatically draws a line from the start point to the end point.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which the line is drawn. The lines are drawn using the foreground color. numPoints
Number of points in the polygon ( Has to be greater than 1 ) polyPoints
Pointer to array of polygon points. The points are laid out like this: polyPoints = {x1,y1,x2,y2 ... } Polypoints has to contain at least (numPoints * 2) entries
- Returns
- Returns GLIB_OK on if at least one element was drawn, or else error code
◆ GLIB_drawPolygonFilled()
EMSTATUS GLIB_drawPolygonFilled | ( | GLIB_Context_t * | pContext, |
uint32_t | numPoints, |
||
const int32_t * | polyPoints |
||
) |
Draws a filled polygon using a scan line algorithm.
This function draws a line between all points outlining the polygon. The first and last point doesn't have to be the same. The function automatically draws a line from the start point to the end point.
- Parameters
-
pContext
Pointer to a GLIB_Context_t where the polygon is drawn. The polygon drawn using the foreground color. numPoints
Number of points in the polygon ( Has to be greater than 1 ) polyPoints
Pointer to array of polygon points. The points are laid out like this: polyPoints = {x1,y1,x2,y2 ... } Polypoints has to contain at least (numPoints * 2) entries
- Returns
- Returns GLIB_OK on success, otherwise a GLIB error code.
◆ GLIB_drawPixelRGB()
EMSTATUS GLIB_drawPixelRGB | ( | GLIB_Context_t * | pContext, |
int32_t | x, |
||
int32_t | y, |
||
uint8_t | red, |
||
uint8_t | green, |
||
uint8_t | blue |
||
) |
Draws a pixel at x, y with color defined by red, green and blue 1 byte per channel.
Example: To draw a yellow pixel at (10, 10). x = 10, y = 10, red = 0xFF, green = 0xFF, blue = 0x00
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the clipping region x
X-coordinate y
Y-coordinate red
8-bit red code green
8-bit green code blue
8-bit blue code
- Returns
- Returns DMD_OK on success, or else error code
◆ GLIB_drawPixel()
EMSTATUS GLIB_drawPixel | ( | GLIB_Context_t * | pContext, |
int32_t | x, |
||
int32_t | y |
||
) |
Draws a pixel at x, y using foregroundColor defined in the GLIB_Context_t.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the foreground color and clipping region x
X-coordinate y
Y-coordinate
- Returns
- Returns GLIB_OK on success, or else error code
◆ GLIB_drawPixelColor()
EMSTATUS GLIB_drawPixelColor | ( | GLIB_Context_t * | pContext, |
int32_t | x, |
||
int32_t | y, |
||
uint32_t | color |
||
) |
Draws a pixel at x, y using the color parameter.
- Parameters
-
pContext
Pointer to a GLIB_Context_t which holds the clipping region x
X-coordinate y
Y-coordinate color
32-bit int defining the RGB color. The 24 LSB defines the RGB color like this: RRRRRRRRGGGGGGGGBBBBBBBB. Example: Yellow = 0x00FFFF00
- Returns
- Returns DMD_OK on success, or else error code
Macro Definition Documentation
◆ ECODE_GLIB_BASE
#define ECODE_GLIB_BASE 0x00000000 |
GLIB Base error code.
◆ GLIB_OK
#define GLIB_OK 0x00000000 |
Successful call.
◆ GLIB_ERROR_NOTHING_TO_DRAW
#define GLIB_ERROR_NOTHING_TO_DRAW (ECODE_GLIB_BASE | 0x0001) |
Function did not draw.
◆ GLIB_ERROR_INVALID_CHAR
#define GLIB_ERROR_INVALID_CHAR (ECODE_GLIB_BASE | 0x0002) |
Invalid char.
◆ GLIB_OUT_OF_BOUNDS
#define GLIB_OUT_OF_BOUNDS (ECODE_GLIB_BASE | 0x0003) |
Coordinates out of bounds.
◆ GLIB_ERROR_INVALID_CLIPPINGREGION
#define GLIB_ERROR_INVALID_CLIPPINGREGION (ECODE_GLIB_BASE | 0x0004) |
Invalid coordinates (ex.
xMin > xMax)
◆ GLIB_ERROR_INVALID_ARGUMENT
#define GLIB_ERROR_INVALID_ARGUMENT (ECODE_GLIB_BASE | 0x0005) |
Invalid argument.
◆ GLIB_ERROR_OUT_OF_MEMORY
#define GLIB_ERROR_OUT_OF_MEMORY (ECODE_GLIB_BASE | 0x0006) |
Out of memory.
◆ GLIB_ERROR_FILE_NOT_SUPPORTED
#define GLIB_ERROR_FILE_NOT_SUPPORTED (ECODE_GLIB_BASE | 0x0007) |
File not supported.
◆ GLIB_ERROR_IO
#define GLIB_ERROR_IO (ECODE_GLIB_BASE | 0x0008) |
General IO Error.
◆ GLIB_ERROR_INVALID_FILE
#define GLIB_ERROR_INVALID_FILE (ECODE_GLIB_BASE | 0x0009) |
Invalid file.
Enumeration Type Documentation
◆ __GLIB_Font_Class
enum __GLIB_Font_Class |
◆ __GLIB_Align
enum __GLIB_Align |
Alignment types.