sl_se_ccm_multipart_context_t Struct Reference
CCM streaming context.
#include <sl_se_manager_types.h>
Data Fields | |
uint32_t | processed_message_length |
Current length of the encrypted/decrypted data. | |
uint32_t | total_message_length |
Total length of data to be encrypted/decrypted. | |
uint8_t | iv [13] |
Nonce (MAX size is 13 bytes) | |
uint32_t | tag_len |
Tag length. | |
sl_se_cipher_operation_t | mode |
CCM mode (decrypt or encrypt) | |
uint8_t | se_ctx [32] |
SE encryption state. | |
union { | |
uint8_t tagbuf [16] | |
Tag. | |
uint8_t final_data [16] | |
Input data saved for finish operation. | |
} | mode_specific_buffer |
uint8_t | final_data_length |
Length of data saved. | |
CCM streaming context.
Field Documentation
◆ processed_message_length
uint32_t sl_se_ccm_multipart_context_t::processed_message_length |
Current length of the encrypted/decrypted data.
◆ total_message_length
uint32_t sl_se_ccm_multipart_context_t::total_message_length |
Total length of data to be encrypted/decrypted.
◆ iv
uint8_t sl_se_ccm_multipart_context_t::iv[13] |
Nonce (MAX size is 13 bytes)
◆ tag_len
uint32_t sl_se_ccm_multipart_context_t::tag_len |
Tag length.
◆ mode
sl_se_cipher_operation_t sl_se_ccm_multipart_context_t::mode |
CCM mode (decrypt or encrypt)
◆ se_ctx
uint8_t sl_se_ccm_multipart_context_t::se_ctx[32] |
SE encryption state.
◆ tagbuf
uint8_t sl_se_ccm_multipart_context_t::tagbuf[16] |
Tag.
◆ final_data
uint8_t sl_se_ccm_multipart_context_t::final_data[16] |
Input data saved for finish operation.
◆ final_data_length
uint8_t sl_se_ccm_multipart_context_t::final_data_length |
Length of data saved.