ADC_InitScan_TypeDef Struct Reference
Scan sequence initialization structure.
#include <em_adc.h>
Data Fields |
|
| ADC_PRSSEL_TypeDef | prsSel |
|
Peripheral reflex system trigger selection.
|
|
| ADC_AcqTime_TypeDef | acqTime |
|
Acquisition time (in ADC clock cycles).
|
|
| ADC_Ref_TypeDef | reference |
|
Sample reference selection.
|
|
| ADC_Res_TypeDef | resolution |
|
Sample resolution.
|
|
| ADC_InitScanInput_TypeDef | scanInputConfig |
|
Scan input configuration.
|
|
| bool | diff |
|
Select if single-ended or differential input.
|
|
| bool | prsEnable |
|
Peripheral reflex system trigger enable.
|
|
| bool | leftAdjust |
|
Select if left adjustment should be done.
|
|
| bool | rep |
|
Select if continuous conversion until explicit stop.
|
|
| bool | scanDmaEm2Wu |
|
When true, DMA is available in EM2 for scan conversion.
|
|
| bool | fifoOverwrite |
|
When true, FIFO overwrites old data when full.
|
|
Scan sequence initialization structure.
Field Documentation
◆ prsSel
| ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel |
Peripheral reflex system trigger selection.
Only applicable if
prsEnable
is enabled.
◆ acqTime
| ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
◆ reference
| ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference |
Sample reference selection.
Note that, for external references, the ADC calibration register must be set explicitly.
◆ resolution
| ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution |
Sample resolution.
◆ scanInputConfig
| ADC_InitScanInput_TypeDef ADC_InitScan_TypeDef::scanInputConfig |
Scan input configuration.
Use ADC_ScanInputClear() , ADC_ScanSingleEndedInputAdd() or ADC_ScanDifferentialInputAdd() to update this structure.
◆ diff
| bool ADC_InitScan_TypeDef::diff |
Select if single-ended or differential input.
◆ prsEnable
| bool ADC_InitScan_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
◆ leftAdjust
| bool ADC_InitScan_TypeDef::leftAdjust |
Select if left adjustment should be done.
◆ rep
| bool ADC_InitScan_TypeDef::rep |
Select if continuous conversion until explicit stop.
◆ scanDmaEm2Wu
| bool ADC_InitScan_TypeDef::scanDmaEm2Wu |
When true, DMA is available in EM2 for scan conversion.
◆ fifoOverwrite
| bool ADC_InitScan_TypeDef::fifoOverwrite |
When true, FIFO overwrites old data when full.
If false, FIFO discards new data. The SINGLEOF IRQ is triggered in both cases.