TIMER_Init_TypeDef Struct Reference
TIMER initialization structure.
#include <em_timer.h>
Data Fields |
|
| bool | enable |
|
Start counting when initialization completed.
|
|
| bool | debugRun |
|
Counter shall keep running during debug halt.
|
|
| TIMER_Prescale_TypeDef | prescale |
|
Prescaling factor, if HFPER / HFPERB clock used.
|
|
| TIMER_ClkSel_TypeDef | clkSel |
|
Clock selection.
|
|
| bool | count2x |
|
2x Count mode, counter increments/decrements by 2, meant for PWM mode.
|
|
| bool | ati |
|
ATI (Always Track Inputs) makes CCPOL always track the polarity of the inputs.
|
|
| TIMER_InputAction_TypeDef | fallAction |
|
Action on falling input edge.
|
|
| TIMER_InputAction_TypeDef | riseAction |
|
Action on rising input edge.
|
|
| TIMER_Mode_TypeDef | mode |
|
Counting mode.
|
|
| bool | dmaClrAct |
|
DMA request clear on active.
|
|
| bool | quadModeX4 |
|
Select X2 or X4 quadrature decode mode (if used).
|
|
| bool | oneShot |
|
Determines if only counting up or down once.
|
|
| bool | sync |
|
Timer can be start/stop/reload by other timers.
|
|
TIMER initialization structure.
Field Documentation
◆ enable
| bool TIMER_Init_TypeDef::enable |
Start counting when initialization completed.
◆ debugRun
| bool TIMER_Init_TypeDef::debugRun |
Counter shall keep running during debug halt.
◆ prescale
| TIMER_Prescale_TypeDef TIMER_Init_TypeDef::prescale |
Prescaling factor, if HFPER / HFPERB clock used.
◆ clkSel
| TIMER_ClkSel_TypeDef TIMER_Init_TypeDef::clkSel |
Clock selection.
◆ count2x
| bool TIMER_Init_TypeDef::count2x |
2x Count mode, counter increments/decrements by 2, meant for PWM mode.
◆ ati
| bool TIMER_Init_TypeDef::ati |
ATI (Always Track Inputs) makes CCPOL always track the polarity of the inputs.
◆ fallAction
| TIMER_InputAction_TypeDef TIMER_Init_TypeDef::fallAction |
Action on falling input edge.
◆ riseAction
| TIMER_InputAction_TypeDef TIMER_Init_TypeDef::riseAction |
Action on rising input edge.
◆ mode
| TIMER_Mode_TypeDef TIMER_Init_TypeDef::mode |
Counting mode.
◆ dmaClrAct
| bool TIMER_Init_TypeDef::dmaClrAct |
DMA request clear on active.
◆ quadModeX4
| bool TIMER_Init_TypeDef::quadModeX4 |
Select X2 or X4 quadrature decode mode (if used).
◆ oneShot
| bool TIMER_Init_TypeDef::oneShot |
Determines if only counting up or down once.
◆ sync
| bool TIMER_Init_TypeDef::sync |
Timer can be start/stop/reload by other timers.