Deprecated Functions
Description
Deprecated Functions.
Data Structures | |
struct | SE_OTPInit_t |
SE OTP initialization struct. | |
struct | SE_DebugStatus_t |
SE debug status. | |
struct | SE_Status_t |
SE status. | |
Functions | |
SE_Response_t | SE_initOTP (SE_OTPInit_t *otp_init) SL_DEPRECATED_API_SDK_3_0 |
SE_Response_t | SE_initPubkey (uint32_t key_type, void *pubkey, uint32_t numBytes, bool signature) SL_DEPRECATED_API_SDK_3_0 |
Function Documentation
◆ SE_initOTP()
SE_Response_t SE_initOTP | ( | SE_OTPInit_t * | otp_init | ) |
Initialize SE one-time-programmable (OTP) configuration.
Configuration is performed by setting the desired options in the SE_OTPInit_t structure.
This function can be used to enable secure boot, to configure flash page locking, and to enable anti-rollback protection when using the SE to perform an application upgrade, typically a Gecko bootloader upgrade.
Before secure boot can be enabled, the public key used for secure boot verification must be uploaded using SE_initPubkey()
.
- Warning
- This command can only be executed once per device! When the configuration has been programmed it is not possible to update any of the fields.
- Parameters
-
[in] otp_init
SE_OTPInit_t structure containing the SE configuration.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OK
when the command was executed successfully
◆ SE_initPubkey()
SE_Response_t SE_initPubkey | ( | uint32_t | key_type, |
void * | pubkey, |
||
uint32_t | numBytes, |
||
bool | signature |
||
) |
Init pubkey or pubkey signature.
Initialize public key stored in the SE, or its corresponding signature. The command can be used to write:
- SE_KEY_TYPE_BOOT – public key used to perform secure boot
- SE_KEY_TYPE_AUTH – public key used to perform secure debug
- Note
- These keys can not be overwritten, so this command can only be issued once per key per part.
- Parameters
-
[in] key_type
ID of key type to initialize. [in] pubkey
Pointer to a buffer that contains the public key or signature. Must be word aligned and have a length of 64 bytes. [in] numBytes
Length of pubkey buffer (64 bytes). [in] signature
If true, initialize signature for the specified key type instead of the public key itself.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OK
when the command was executed successfully SE_RESPONSE_TEST_FAILED
when the pubkey is not set SE_RESPONSE_INVALID_PARAMETER
when an invalid type is passed