IADC_Init_t Struct Reference
IADC init structure, common for single conversion and scan sequence.
#include <em_iadc.h>
Data Fields | |
bool | iadcClkSuspend0 |
Suspend IADC_CLK when in scan mode until PRS trigger. | |
bool | iadcClkSuspend1 |
Suspend IADC_CLK when in single mode until PRS trigger. | |
bool | debugHalt |
Halt IADC during debug mode. | |
IADC_Warmup_t | warmup |
IADC warmup mode. | |
uint8_t | timebase |
IADC clock cycles (timebase+1) corresponding to 1us. | |
uint8_t | srcClkPrescale |
User requested source clock divider (prescale+1) which will be used if the calculated prescaler value is less. | |
uint16_t | timerCycles |
Number of ADC_CLK cycles per TIMER event. | |
uint16_t | greaterThanEqualThres |
Digital window comparator greater-than or equal threshold. | |
uint16_t | lessThanEqualThres |
Digital window comparator less-than or equal threshold. | |
IADC init structure, common for single conversion and scan sequence.
Field Documentation
◆ iadcClkSuspend0
bool IADC_Init_t::iadcClkSuspend0 |
Suspend IADC_CLK when in scan mode until PRS trigger.
◆ iadcClkSuspend1
bool IADC_Init_t::iadcClkSuspend1 |
Suspend IADC_CLK when in single mode until PRS trigger.
◆ debugHalt
bool IADC_Init_t::debugHalt |
Halt IADC during debug mode.
◆ warmup
IADC_Warmup_t IADC_Init_t::warmup |
IADC warmup mode.
◆ timebase
uint8_t IADC_Init_t::timebase |
IADC clock cycles (timebase+1) corresponding to 1us.
Used as time reference for IADC delays, e.g. warmup. If the user sets timebase to 0, then IADC_Init() will calculate the timebase using the currently defined CMU clock setting for the IADC.
◆ srcClkPrescale
uint8_t IADC_Init_t::srcClkPrescale |
User requested source clock divider (prescale+1) which will be used if the calculated prescaler value is less.
◆ timerCycles
uint16_t IADC_Init_t::timerCycles |
Number of ADC_CLK cycles per TIMER event.
◆ greaterThanEqualThres
uint16_t IADC_Init_t::greaterThanEqualThres |
Digital window comparator greater-than or equal threshold.
◆ lessThanEqualThres
uint16_t IADC_Init_t::lessThanEqualThres |
Digital window comparator less-than or equal threshold.