EUSART_AdvancedInit_TypeDef Struct Reference
Advanced initialization structure.
      
       #include <em_eusart.h>
      
     
| Data Fields | |
| EUSART_HwFlowControl_TypeDef | hwFlowControl | 
| Hardware flow control mode. | |
| bool | collisionDetectEnable | 
| Enable the collision Detection feature. | |
| bool | msbFirst | 
| If true, data will be send with most significant bit first. | |
| EUSART_InvertIO_TypeDef | invertIO | 
| Enable inversion of RX and/or TX signals. | |
| bool | dmaWakeUpOnRx | 
| Enable the automatic wake up from EM2 to EM1 for DMA RX operation. | |
| bool | dmaWakeUpOnTx | 
| Enable the automatic wake up from EM2 to EM1 for DMA TX operation. | |
| bool | dmaHaltOnError | 
| Enable DMA requests blocking while framing or parity errors. | |
| uint8_t | startFrame | 
| Start frame that will enable RX operation. 0x00 Disable this feature. | |
| bool | txAutoTristate | 
| Enable automatic tristating of transmistter output when there is nothing to transmit. | |
| bool | prsRxEnable | 
| Enable EUSART capability to use a PRS channel as an input data line for the receiver. | |
| EUSART_PrsChannel_TypeDef | prsRxChannel | 
| PRS Channel used to transmit data from PRS to the EUSART. | |
| bool | multiProcessorEnable | 
| Enable Multiprocessor mode. Address and data filtering using the 9th bit. | |
| bool | multiProcessorAddressBitHigh | 
| Multiprocessor address bit value. If true, 9th bit of address frame must bit 1, 0 otherwise. | |
Advanced initialization structure.
Field Documentation
◆ hwFlowControl
| EUSART_HwFlowControl_TypeDef EUSART_AdvancedInit_TypeDef::hwFlowControl | 
Hardware flow control mode.
◆ collisionDetectEnable
| bool EUSART_AdvancedInit_TypeDef::collisionDetectEnable | 
Enable the collision Detection feature.
Internal (setting loopbackEnable) or external loopback must be done to use this feature.
◆ msbFirst
| bool EUSART_AdvancedInit_TypeDef::msbFirst | 
If true, data will be send with most significant bit first.
◆ invertIO
| EUSART_InvertIO_TypeDef EUSART_AdvancedInit_TypeDef::invertIO | 
Enable inversion of RX and/or TX signals.
◆ dmaWakeUpOnRx
| bool EUSART_AdvancedInit_TypeDef::dmaWakeUpOnRx | 
Enable the automatic wake up from EM2 to EM1 for DMA RX operation.
◆ dmaWakeUpOnTx
| bool EUSART_AdvancedInit_TypeDef::dmaWakeUpOnTx | 
Enable the automatic wake up from EM2 to EM1 for DMA TX operation.
◆ dmaHaltOnError
| bool EUSART_AdvancedInit_TypeDef::dmaHaltOnError | 
Enable DMA requests blocking while framing or parity errors.
◆ startFrame
| uint8_t EUSART_AdvancedInit_TypeDef::startFrame | 
Start frame that will enable RX operation. 0x00 Disable this feature.
◆ txAutoTristate
| bool EUSART_AdvancedInit_TypeDef::txAutoTristate | 
Enable automatic tristating of transmistter output when there is nothing to transmit.
◆ prsRxEnable
| bool EUSART_AdvancedInit_TypeDef::prsRxEnable | 
Enable EUSART capability to use a PRS channel as an input data line for the receiver.
The configured RX GPIO signal won't be routed to the EUSART receiver.
◆ prsRxChannel
| EUSART_PrsChannel_TypeDef EUSART_AdvancedInit_TypeDef::prsRxChannel | 
PRS Channel used to transmit data from PRS to the EUSART.
◆ multiProcessorEnable
| bool EUSART_AdvancedInit_TypeDef::multiProcessorEnable | 
Enable Multiprocessor mode. Address and data filtering using the 9th bit.
◆ multiProcessorAddressBitHigh
| bool EUSART_AdvancedInit_TypeDef::multiProcessorAddressBitHigh | 
Multiprocessor address bit value. If true, 9th bit of address frame must bit 1, 0 otherwise.