SMU - Security Management Unit#

Security Management Unit (SMU) Peripheral API.

SMU forms the control and status/reporting component of bus-level security in EFM32/EFR32 devices.

Peripheral-level protection is provided via the Peripheral Protection Unit (PPU). PPU provides hardware access barrier to any peripheral that is configured to be protected. When an attempt is made to access a peripheral without the required privilege/security level, PPU detects the fault and intercepts the access. No write or read of the peripheral register space occurs, and an all-zero value is returned if the access is a read.

Usage example

// SMU is always clocked, so no call to CMU_ClockEnable() is necessary

// Initialize SMU to prevent access to CMU, EMU, SMU and GPIO
SMU_Init_TypeDef init = SMU_INIT_DEFAULT;
init.ppu.access.privilegedCMU = true;
init.ppu.access.privilegedEMU = true;
init.ppu.access.privilegedSMU = true;
init.ppu.access.privilegedGPIO = true;
SMU_Init(&init);

Modules#

SMU_PrivilegedAccess_TypeDef

SMU_Init_TypeDef

Enumerations#

enum
smuPeripheralEMU = _SMU_PPUPATD0_EMU_SHIFT
smuPeripheralCMU = _SMU_PPUPATD0_CMU_SHIFT
smuPeripheralHFXO = 32 + _SMU_PPUPATD1_HFXO0_SHIFT
smuPeripheralHFRCO0 = _SMU_PPUPATD0_HFRCO0_SHIFT
smuPeripheralFSRCO = _SMU_PPUPATD0_FSRCO_SHIFT
smuPeripheralDPLL0 = _SMU_PPUPATD0_DPLL0_SHIFT
smuPeripheralLFXO = _SMU_PPUPATD0_LFXO_SHIFT
smuPeripheralLFRCO = _SMU_PPUPATD0_LFRCO_SHIFT
smuPeripheralULFRCO = _SMU_PPUPATD0_ULFRCO_SHIFT
smuPeripheralMSC = _SMU_PPUPATD0_MSC_SHIFT
smuPeripheralICACHE0 = _SMU_PPUPATD0_ICACHE0_SHIFT
smuPeripheralPRS = _SMU_PPUPATD0_PRS_SHIFT
smuPeripheralGPIO = _SMU_PPUPATD0_GPIO_SHIFT
smuPeripheralLDMA = _SMU_PPUPATD0_LDMA_SHIFT
smuPeripheralLDMAXBAR = _SMU_PPUPATD0_LDMAXBAR_SHIFT
smuPeripheralTIMER0 = _SMU_PPUPATD0_TIMER0_SHIFT
smuPeripheralTIMER1 = _SMU_PPUPATD0_TIMER1_SHIFT
smuPeripheralTIMER2 = _SMU_PPUPATD0_TIMER2_SHIFT
smuPeripheralTIMER3 = _SMU_PPUPATD0_TIMER3_SHIFT
smuPeripheralTIMER4 = _SMU_PPUPATD0_TIMER4_SHIFT
smuPeripheralUSART0 = _SMU_PPUPATD0_USART0_SHIFT
smuPeripheralBURTC = _SMU_PPUPATD0_BURTC_SHIFT
smuPeripheralI2C1 = _SMU_PPUPATD0_I2C1_SHIFT
smuPeripheralCHIPTESTCTRL = _SMU_PPUPATD0_CHIPTESTCTRL_SHIFT
smuPeripheralSYSCFGCFGNS = _SMU_PPUPATD0_SYSCFGCFGNS_SHIFT
smuPeripheralSYSCFG = _SMU_PPUPATD0_SYSCFG_SHIFT
smuPeripheralBURAM = _SMU_PPUPATD0_BURAM_SHIFT
smuPeripheralGPCRC = _SMU_PPUPATD0_GPCRC_SHIFT
smuPeripheralDCDC = _SMU_PPUPATD0_DCDC_SHIFT
smuPeripheralHOSTMAILBOX = _SMU_PPUPATD0_HOSTMAILBOX_SHIFT
smuPeripheralEUSART0 = 32 + _SMU_PPUPATD1_EUSART0_SHIFT
smuPeripheralEUSART1 = _SMU_PPUPATD0_EUSART1_SHIFT
smuPeripheralEUSART2 = _SMU_PPUPATD0_EUSART2_SHIFT
smuPeripheralSYSRTC = 32 + _SMU_PPUPATD1_SYSRTC_SHIFT
smuPeripheralLCD = 32 + _SMU_PPUPATD1_LCD_SHIFT
smuPeripheralKEYSCAN = 32 + _SMU_PPUPATD1_KEYSCAN_SHIFT
smuPeripheralDMEM = 32 + _SMU_PPUPATD1_DMEM_SHIFT
smuPeripheralLCDRF = 32 + _SMU_PPUPATD1_LCDRF_SHIFT
smuPeripheralPFMXPPRF = 32 + _SMU_PPUPATD1_PFMXPPRF_SHIFT
smuPeripheralVDAC0 = 32 + _SMU_PPUPATD1_VDAC0_SHIFT
smuPeripheralPCNT = 32 + _SMU_PPUPATD1_PCNT_SHIFT
smuPeripheralLESENSE = 32 + _SMU_PPUPATD1_LESENSE_SHIFT
smuPeripheralHFRCO1 = 32 + _SMU_PPUPATD1_HFRCO1_SHIFT
smuPeripheralHFXO0 = 32 + _SMU_PPUPATD1_HFXO0_SHIFT
smuPeripheralLETIMER0 = 32 + _SMU_PPUPATD1_LETIMER0_SHIFT
smuPeripheralIADC0 = 32 + _SMU_PPUPATD1_IADC0_SHIFT
smuPeripheralACMP0 = 32 + _SMU_PPUPATD1_ACMP0_SHIFT
smuPeripheralACMP1 = 32 + _SMU_PPUPATD1_ACMP1_SHIFT
smuPeripheralI2C0 = 32 + _SMU_PPUPATD1_I2C0_SHIFT
smuPeripheralWDOG0 = 32 + _SMU_PPUPATD1_WDOG0_SHIFT
smuPeripheralWDOG1 = 32 + _SMU_PPUPATD1_WDOG1_SHIFT
smuPeripheralAMUXCP0 = 32 + _SMU_PPUPATD1_AMUXCP0_SHIFT
smuPeripheralRADIOAES = 32 + _SMU_PPUPATD1_RADIOAES_SHIFT
smuPeripheralSMU = 32 + _SMU_PPUPATD1_SMU_SHIFT
smuPeripheralSMUCFGNS = 32 + _SMU_PPUPATD1_SMUCFGNS_SHIFT
smuPeripheralAHBRADIO = 32 + _SMU_PPUPATD1_AHBRADIO_SHIFT
smuPeripheralSEMAILBOX = 32 + _SMU_PPUPATD1_SEMAILBOX_SHIFT
smuPeripheralEnd
}

SMU peripheral identifiers.

Functions#

void
SMU_EnablePPU(bool enable)

Enable or disable PPU of SMU.

void
SMU_Init(const SMU_Init_TypeDef *init)

Initialize PPU of SMU.

void
SMU_SetPrivilegedAccess(SMU_Peripheral_TypeDef peripheral, bool privileged)

Change access settings for a peripheral.

Get the ID of the peripheral that caused an access fault.

void
SMU_IntClear(uint32_t flags)

Clear one or more pending SMU interrupts.

void
SMU_IntDisable(uint32_t flags)

Disable one or more SMU interrupts.

void
SMU_IntEnable(uint32_t flags)

Enable one or more SMU interrupts.

uint32_t

Get pending SMU interrupts.

uint32_t

Get enabled and pending SMU interrupt flags.

void
SMU_IntSet(uint32_t flags)

Set one or more pending SMU interrupts from SW.

void

SMU secure IRQ Handler.

Macros#

#define

Default SMU initialization structure settings.

Enumeration Documentation#

SMU_Peripheral_TypeDef#

SMU_Peripheral_TypeDef

SMU peripheral identifiers.

Enumerator
smuPeripheralEMU

SMU peripheral identifier for EMU

smuPeripheralCMU

SMU peripheral identifier for CMU

smuPeripheralHFXO

SMU peripheral identifier for HFXO0

smuPeripheralHFRCO0

SMU peripheral identifier for HFRCO0

smuPeripheralFSRCO

SMU peripheral identifier for FSRCO

smuPeripheralDPLL0

SMU peripheral identifier for DPLL0

smuPeripheralLFXO

SMU peripheral identifier for LFXO

smuPeripheralLFRCO

SMU peripheral identifier for LFRCO

smuPeripheralULFRCO

SMU peripheral identifier for ULFRCO

smuPeripheralMSC

SMU peripheral identifier for MSC

smuPeripheralICACHE0

SMU peripheral identifier for ICACHE0

smuPeripheralPRS

SMU peripheral identifier for PRS

smuPeripheralGPIO

SMU peripheral identifier for GPIO

smuPeripheralLDMA

SMU peripheral identifier for LDMA

smuPeripheralLDMAXBAR

SMU peripheral identifier for LDMAXBAR

smuPeripheralTIMER0

SMU peripheral identifier for TIMER0

smuPeripheralTIMER1

SMU peripheral identifier for TIMER1

smuPeripheralTIMER2

SMU peripheral identifier for TIMER2

smuPeripheralTIMER3

SMU peripheral identifier for TIMER3

smuPeripheralTIMER4

SMU peripheral identifier for TIMER4

smuPeripheralUSART0

SMU peripheral identifier for USART0

smuPeripheralBURTC

SMU peripheral identifier for BURTC

smuPeripheralI2C1

SMU peripheral identifier for I2C1

smuPeripheralCHIPTESTCTRL

SMU peripheral identifier for CHIPTESTCTRL.

smuPeripheralSYSCFGCFGNS

SMU peripheral identifier for SYSCFGCFGNS.

smuPeripheralSYSCFG

SMU peripheral identifier for SYSCFG

smuPeripheralBURAM

SMU peripheral identifier for BURAM

smuPeripheralGPCRC

SMU peripheral identifier for GPCRC

smuPeripheralDCDC

SMU peripheral identifier for DCDC

smuPeripheralHOSTMAILBOX

SMU peripheral identifier for HOSTMAILBOX.

smuPeripheralEUSART0

SMU peripheral identifier for EUSART0

smuPeripheralEUSART1

SMU peripheral identifier for EUSART1

smuPeripheralEUSART2

SMU peripheral identifier for EUSART2

smuPeripheralSYSRTC

SMU peripheral identifier for SYSRTC

smuPeripheralLCD

SMU peripheral identifier for LCD

smuPeripheralKEYSCAN

SMU peripheral identifier for KEYSCAN

smuPeripheralDMEM

SMU peripheral identifier for DMEM

smuPeripheralLCDRF

SMU peripheral identifier for LCDRF

smuPeripheralPFMXPPRF

SMU peripheral identifier for PFMXPPRF

smuPeripheralVDAC0

SMU peripheral identifier for VDAC0

smuPeripheralPCNT

SMU peripheral identifier for PCNT

smuPeripheralLESENSE

SMU peripheral identifier for LESENSE

smuPeripheralHFRCO1

SMU peripheral identifier for HFRCO1

smuPeripheralHFXO0

SMU peripheral identifier for HFXO0

smuPeripheralLETIMER0

SMU peripheral identifier for LETIMER

smuPeripheralIADC0

SMU peripheral identifier for IADC0

smuPeripheralACMP0

SMU peripheral identifier for ACMP0

smuPeripheralACMP1

SMU peripheral identifier for ACMP1

smuPeripheralI2C0

SMU peripheral identifier for I2C0

smuPeripheralWDOG0

SMU peripheral identifier for WDOG0

smuPeripheralWDOG1

SMU peripheral identifier for WDOG1

smuPeripheralAMUXCP0

SMU peripheral identifier for AMUXCP0

smuPeripheralRADIOAES

SMU peripheral identifier for RADIOAES

smuPeripheralSMU

SMU peripheral identifier for SMU

smuPeripheralSMUCFGNS

SMU peripheral identifier for SMUCFGNS

smuPeripheralAHBRADIO

SMU peripheral identifier for AHBRADIO

smuPeripheralSEMAILBOX

SMU peripheral identifier for SEMAILBOX.

smuPeripheralEnd

SMU peripheral end.


Definition at line 72 of file platform/emlib/inc/em_smu.h

Function Documentation#

SMU_EnablePPU#

void SMU_EnablePPU (bool enable)

Enable or disable PPU of SMU.

Parameters
[in]enable

Set to true to enable PPU; set to false otherwise.


Definition at line 1425 of file platform/emlib/inc/em_smu.h

SMU_Init#

void SMU_Init (const SMU_Init_TypeDef *init)

Initialize PPU of SMU.

Parameters
[in]init

Pointer to initialization structure that defines which peripherals should only be accessed from privileged mode, and if PPU should be enabled.


Definition at line 1442 of file platform/emlib/inc/em_smu.h

SMU_SetPrivilegedAccess#

void SMU_SetPrivilegedAccess (SMU_Peripheral_TypeDef peripheral, bool privileged)

Change access settings for a peripheral.

Parameters
[in]peripheral

ID of the peripheral to change access settings for.

[in]privileged

Set to true if the peripheral should only be accessed from privileged mode; set to false otherwise.

Set to limit access of a peripheral from privileged mode.


Definition at line 1475 of file platform/emlib/inc/em_smu.h

SMU_GetFaultingPeripheral#

SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral (void)

Get the ID of the peripheral that caused an access fault.

Parameters
N/A

Note

  • The return value is only valid if SMU_IF_PPUPRIV interrupt flag is set.

Returns

  • ID of the peripheral that caused an access fault.


Definition at line 1519 of file platform/emlib/inc/em_smu.h

SMU_IntClear#

void SMU_IntClear (uint32_t flags)

Clear one or more pending SMU interrupts.

Parameters
[in]flags

Bitwise logic OR of SMU interrupt sources to clear.


Definition at line 1536 of file platform/emlib/inc/em_smu.h

SMU_IntDisable#

void SMU_IntDisable (uint32_t flags)

Disable one or more SMU interrupts.

Parameters
[in]flags

SMU interrupt sources to disable.


Definition at line 1557 of file platform/emlib/inc/em_smu.h

SMU_IntEnable#

void SMU_IntEnable (uint32_t flags)

Enable one or more SMU interrupts.

Parameters
[in]flags

SMU interrupt sources to enable.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using SMU_IntClear() prior to enabling the interrupt.


Definition at line 1583 of file platform/emlib/inc/em_smu.h

SMU_IntGet#

uint32_t SMU_IntGet (void)

Get pending SMU interrupts.

Parameters
N/A

Returns

  • SMU interrupt sources pending.


Definition at line 1604 of file platform/emlib/inc/em_smu.h

SMU_IntGetEnabled#

uint32_t SMU_IntGetEnabled (void)

Get enabled and pending SMU interrupt flags.

Parameters
N/A

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by this function.

Returns

  • Pending and enabled SMU interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in SMU_IEN register and

    • the OR combination of valid interrupt flags in SMU_IF register.


Definition at line 1629 of file platform/emlib/inc/em_smu.h

SMU_IntSet#

void SMU_IntSet (uint32_t flags)

Set one or more pending SMU interrupts from SW.

Parameters
[in]flags

SMU interrupt sources to set to pending.


Definition at line 1658 of file platform/emlib/inc/em_smu.h

SMU_SECURE_IRQHandler#

void SMU_SECURE_IRQHandler (void)

SMU secure IRQ Handler.

Parameters
N/A

When a PPU detects an access to a secure peripheral at its non-secure address or an access to a non-secure peripheral at its secure address, PPUSECIF in SMU_IF is set and the ID of the peripheral being accessed is written to SMU_PPUFS. If PPUSECIEN is set and the SMU's Secure IRQ enabled, the CPU will be interrupted and SMU_SECURE_IRQHandler Will handle the interrupt.


Definition at line 1685 of file platform/emlib/inc/em_smu.h

Macro Definition Documentation#

SMU_INIT_DEFAULT#

#define SMU_INIT_DEFAULT
Value:
{ \
{ { 0 } }, /* No peripherals access protected. */ \
true /* Enable SMU.*/ \
}

Default SMU initialization structure settings.


Definition at line 1409 of file platform/emlib/inc/em_smu.h