TIMER - Timer/Counter#

Timer/Counter (TIMER) Peripheral API.

The timer module consists of three main parts:

  • General timer configuration and enable control.

  • Compare/capture control.

  • Dead time insertion control (may not be available for all timers).

Modules#

TIMER_Init_TypeDef

TIMER_InitCC_TypeDef

TIMER_InitDTI_TypeDef

Enumerations#

enum
timerCCModeOff = _TIMER_CC_CFG_MODE_OFF
timerCCModeCapture = _TIMER_CC_CFG_MODE_INPUTCAPTURE
timerCCModeCompare = _TIMER_CC_CFG_MODE_OUTPUTCOMPARE
timerCCModePWM = _TIMER_CC_CFG_MODE_PWM
}

Timer compare/capture mode.

enum
timerClkSelHFPerClk = _TIMER_CFG_CLKSEL_PRESCEM01GRPACLK
timerClkSelCC1 = _TIMER_CFG_CLKSEL_CC1
timerClkSelCascade = _TIMER_CFG_CLKSEL_TIMEROUF
}

Clock select.

enum
timerEdgeRising = _TIMER_CC_CTRL_ICEDGE_RISING
timerEdgeFalling = _TIMER_CC_CTRL_ICEDGE_FALLING
timerEdgeBoth = _TIMER_CC_CTRL_ICEDGE_BOTH
timerEdgeNone = _TIMER_CC_CTRL_ICEDGE_NONE
}

Input capture edge select.

enum
timerEventEveryEdge = _TIMER_CC_CTRL_ICEVCTRL_EVERYEDGE
timerEventEvery2ndEdge = _TIMER_CC_CTRL_ICEVCTRL_EVERYSECONDEDGE
timerEventRising = _TIMER_CC_CTRL_ICEVCTRL_RISING
timerEventFalling = _TIMER_CC_CTRL_ICEVCTRL_FALLING
}

Input capture event control.

enum
timerInputActionNone = _TIMER_CTRL_FALLA_NONE
timerInputActionStart = _TIMER_CTRL_FALLA_START
timerInputActionStop = _TIMER_CTRL_FALLA_STOP
timerInputActionReloadStart = _TIMER_CTRL_FALLA_RELOADSTART
}

Input edge action.

enum
timerModeUp = _TIMER_CFG_MODE_UP
timerModeDown = _TIMER_CFG_MODE_DOWN
timerModeUpDown = _TIMER_CFG_MODE_UPDOWN
timerModeQDec = _TIMER_CFG_MODE_QDEC
}

Timer mode.

enum
timerOutputActionNone = _TIMER_CC_CTRL_CUFOA_NONE
timerOutputActionToggle = _TIMER_CC_CTRL_CUFOA_TOGGLE
timerOutputActionClear = _TIMER_CC_CTRL_CUFOA_CLEAR
timerOutputActionSet = _TIMER_CC_CTRL_CUFOA_SET
}

Compare/capture output action.

enum
timerPrescale1 = _TIMER_CFG_PRESC_DIV1
timerPrescale2 = _TIMER_CFG_PRESC_DIV2
timerPrescale4 = _TIMER_CFG_PRESC_DIV4
timerPrescale8 = _TIMER_CFG_PRESC_DIV8
timerPrescale16 = _TIMER_CFG_PRESC_DIV16
timerPrescale32 = _TIMER_CFG_PRESC_DIV32
timerPrescale64 = _TIMER_CFG_PRESC_DIV64
timerPrescale128 = _TIMER_CFG_PRESC_DIV128
timerPrescale256 = _TIMER_CFG_PRESC_DIV256
timerPrescale512 = _TIMER_CFG_PRESC_DIV512
timerPrescale1024 = _TIMER_CFG_PRESC_DIV1024
}

Prescaler.

enum
timerPrsInputNone = 0x0
timerPrsInputSync = _TIMER_CC_CFG_INSEL_PRSSYNC
timerPrsInputAsyncLevel = _TIMER_CC_CFG_INSEL_PRSASYNCLEVEL
timerPrsInputAsyncPulse = _TIMER_CC_CFG_INSEL_PRSASYNCPULSE
}

PRS input type.

enum
timerDtiFaultActionNone = _TIMER_DTFCFG_DTFA_NONE
timerDtiFaultActionInactive = _TIMER_DTFCFG_DTFA_INACTIVE
timerDtiFaultActionClear = _TIMER_DTFCFG_DTFA_CLEAR
timerDtiFaultActionTristate = _TIMER_DTFCFG_DTFA_TRISTATE
}

DT (Dead Time) Fault Actions.

enum
timerPrsOutputPulse = 0
timerPrsOutputLevel = 1
timerPrsOutputDefault = timerPrsOutputPulse
}

PRS Output configuration.

Typedefs#

typedef uint8_t

Peripheral Reflex System signal.

Functions#

void
TIMER_Init(TIMER_TypeDef *timer, const TIMER_Init_TypeDef *init)

Initialize TIMER.

void
TIMER_InitCC(TIMER_TypeDef *timer, unsigned int ch, const TIMER_InitCC_TypeDef *init)

Initialize the TIMER compare/capture channel.

void
TIMER_InitDTI(TIMER_TypeDef *timer, const TIMER_InitDTI_TypeDef *init)

Initialize the TIMER DTI unit.

void
TIMER_Reset(TIMER_TypeDef *timer)

Reset the TIMER to the same state that it was in after a hardware reset.

void
TIMER_SyncWait(TIMER_TypeDef *timer)

Wait for pending synchronization to finish.

bool
TIMER_Valid(const TIMER_TypeDef *ref)

Validate the TIMER register block pointer.

bool
TIMER_SupportsDTI(const TIMER_TypeDef *ref)

Check whether the TIMER is valid and supports Dead Timer Insertion (DTI).

uint32_t
TIMER_MaxCount(const TIMER_TypeDef *ref)

Get the Max count of the timer.

uint32_t
TIMER_CaptureGet(TIMER_TypeDef *timer, unsigned int ch)

Get compare/capture value for the compare/capture channel.

uint32_t
TIMER_CaptureBufGet(TIMER_TypeDef *timer, unsigned int ch)

Get the buffered compare/capture value for compare/capture channel.

void
TIMER_CompareBufSet(TIMER_TypeDef *timer, unsigned int ch, uint32_t val)

Set the compare value buffer for the compare/capture channel when operating in compare or PWM mode.

void
TIMER_CompareSet(TIMER_TypeDef *timer, unsigned int ch, uint32_t val)

Set the compare value for compare/capture channel when operating in compare or PWM mode.

uint32_t
TIMER_CounterGet(TIMER_TypeDef *timer)

Get the TIMER counter value.

void
TIMER_CounterSet(TIMER_TypeDef *timer, uint32_t val)

Set the TIMER counter value.

void
TIMER_Enable(TIMER_TypeDef *timer, bool enable)

Start/stop TIMER.

void
TIMER_EnableDTI(TIMER_TypeDef *timer, bool enable)

Enable or disable DTI unit.

uint32_t
TIMER_GetDTIFault(TIMER_TypeDef *timer)

Get DTI fault source flags status.

void
TIMER_ClearDTIFault(TIMER_TypeDef *timer, uint32_t flags)

Clear DTI fault source flags.

void
TIMER_IntClear(TIMER_TypeDef *timer, uint32_t flags)

Clear one or more pending TIMER interrupts.

void
TIMER_IntDisable(TIMER_TypeDef *timer, uint32_t flags)

Disable one or more TIMER interrupts.

void
TIMER_IntEnable(TIMER_TypeDef *timer, uint32_t flags)

Enable one or more TIMER interrupts.

uint32_t
TIMER_IntGet(TIMER_TypeDef *timer)

Get pending TIMER interrupt flags.

uint32_t
TIMER_IntGetEnabled(TIMER_TypeDef *timer)

Get enabled and pending TIMER interrupt flags.

void
TIMER_IntSet(TIMER_TypeDef *timer, uint32_t flags)

Set one or more pending TIMER interrupts from SW.

void
TIMER_TopBufSet(TIMER_TypeDef *timer, uint32_t val)

Set the top value buffer for the timer.

uint32_t
TIMER_TopGet(TIMER_TypeDef *timer)

Get the top value setting for the timer.

void
TIMER_TopSet(TIMER_TypeDef *timer, uint32_t val)

Set the top value for timer.

Macros#

#define
TIMER_INIT_DEFAULT undefined

Default configuration for TIMER initialization structure.

#define
TIMER_INITCC_DEFAULT undefined

Default configuration for TIMER compare/capture initialization structure.

#define
TIMER_INITDTI_DEFAULT undefined

Default configuration for TIMER DTI initialization structure.

Enumeration Documentation#

TIMER_CCMode_TypeDef#

TIMER_CCMode_TypeDef

Timer compare/capture mode.

Enumerator
timerCCModeOff

Channel turned off.

timerCCModeCapture

Input capture.

timerCCModeCompare

Output compare.

timerCCModePWM

Pulse-Width modulation.


TIMER_ClkSel_TypeDef#

TIMER_ClkSel_TypeDef

Clock select.

Enumerator
timerClkSelHFPerClk

Prescaled EM01GRPA clock.

timerClkSelCC1

Compare/Capture Channel 1 Input.

timerClkSelCascade

Cascaded clocked by underflow or overflow by lower numbered timer.


TIMER_Edge_TypeDef#

TIMER_Edge_TypeDef

Input capture edge select.

Enumerator
timerEdgeRising

Rising edges detected.

timerEdgeFalling

Falling edges detected.

timerEdgeBoth

Both edges detected.

timerEdgeNone

No edge detection, leave signal as is.


TIMER_Event_TypeDef#

TIMER_Event_TypeDef

Input capture event control.

Enumerator
timerEventEveryEdge

PRS output pulse, interrupt flag, and DMA request set on every capture.

timerEventEvery2ndEdge

PRS output pulse, interrupt flag, and DMA request set on every second capture.

timerEventRising

PRS output pulse, interrupt flag, and DMA request set on rising edge (if input capture edge = BOTH).

timerEventFalling

PRS output pulse, interrupt flag, and DMA request set on falling edge (if input capture edge = BOTH).


TIMER_InputAction_TypeDef#

TIMER_InputAction_TypeDef

Input edge action.

Enumerator
timerInputActionNone

No action taken.

timerInputActionStart

Start counter without reload.

timerInputActionStop

Stop counter without reload.

timerInputActionReloadStart

Reload and start counter.


TIMER_Mode_TypeDef#

TIMER_Mode_TypeDef

Timer mode.

Enumerator
timerModeUp

Up-counting.

timerModeDown

Down-counting.

timerModeUpDown

Up/down-counting.

timerModeQDec

Quadrature decoder.


TIMER_OutputAction_TypeDef#

TIMER_OutputAction_TypeDef

Compare/capture output action.

Enumerator
timerOutputActionNone

No action.

timerOutputActionToggle

Toggle on event.

timerOutputActionClear

Clear on event.

timerOutputActionSet

Set on event.


TIMER_Prescale_TypeDef#

TIMER_Prescale_TypeDef

Prescaler.

Enumerator
timerPrescale1

Divide by 1.

timerPrescale2

Divide by 2.

timerPrescale4

Divide by 4.

timerPrescale8

Divide by 8.

timerPrescale16

Divide by 16.

timerPrescale32

Divide by 32.

timerPrescale64

Divide by 64.

timerPrescale128

Divide by 128.

timerPrescale256

Divide by 256.

timerPrescale512

Divide by 512.

timerPrescale1024

Divide by 1024.


TIMER_PrsInput_TypeDef#

TIMER_PrsInput_TypeDef

PRS input type.

Enumerator
timerPrsInputNone

No PRS input.

timerPrsInputSync

Synchronous PRS selected.

timerPrsInputAsyncLevel

Asynchronous level PRS selected.

timerPrsInputAsyncPulse

Asynchronous pulse PRS selected.


TIMER_DtiFaultAction_TypeDef#

TIMER_DtiFaultAction_TypeDef

DT (Dead Time) Fault Actions.

Enumerator
timerDtiFaultActionNone

No action on fault.

timerDtiFaultActionInactive

Set outputs inactive.

timerDtiFaultActionClear

Clear outputs.

timerDtiFaultActionTristate

Tristate outputs.


TIMER_PrsOutput_t#

TIMER_PrsOutput_t

PRS Output configuration.

Enumerator
timerPrsOutputPulse

Pulse PRS output from a channel.

timerPrsOutputLevel

PRS output follows CC out level.

timerPrsOutputDefault

Default PRS output behavior.


Typedef Documentation#

TIMER_PRSSEL_TypeDef#

typedef uint8_t TIMER_PRSSEL_TypeDef

Peripheral Reflex System signal.


Function Documentation#

TIMER_Init#

void TIMER_Init (TIMER_TypeDef * timer, const TIMER_Init_TypeDef * init)

Initialize TIMER.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

A pointer to the TIMER peripheral register block.

const TIMER_Init_TypeDef *[in]init

A pointer to the TIMER initialization structure.

Notice that the counter top must be configured separately with, for instance TIMER_TopSet(). In addition, compare/capture and dead-time insertion initialization must be initialized separately if used, which should probably be done prior to using this function if configuring the TIMER to start when initialization is completed.


TIMER_InitCC#

void TIMER_InitCC (TIMER_TypeDef * timer, unsigned int ch, const TIMER_InitCC_TypeDef * init)

Initialize the TIMER compare/capture channel.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

A pointer to the TIMER peripheral register block.

unsigned int[in]ch

A compare/capture channel to initialize for.

const TIMER_InitCC_TypeDef *[in]init

A pointer to the TIMER initialization structure.

Notice that if operating the channel in compare mode, the CCV and CCVB register must be set separately, as required.


TIMER_InitDTI#

void TIMER_InitDTI (TIMER_TypeDef * timer, const TIMER_InitDTI_TypeDef * init)

Initialize the TIMER DTI unit.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

A pointer to the TIMER peripheral register block.

const TIMER_InitDTI_TypeDef *[in]init

A pointer to the TIMER DTI initialization structure.


TIMER_Reset#

void TIMER_Reset (TIMER_TypeDef * timer)

Reset the TIMER to the same state that it was in after a hardware reset.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

A pointer to the TIMER peripheral register block.

Note

  • The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.


TIMER_SyncWait#

void TIMER_SyncWait (TIMER_TypeDef * timer)

Wait for pending synchronization to finish.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

TIMER_Valid#

bool TIMER_Valid (const TIMER_TypeDef * ref)

Validate the TIMER register block pointer.

Parameters
TypeDirectionArgument NameDescription
const TIMER_TypeDef *[in]ref

Pointer to the TIMER peripheral register block.

Returns

  • True if ref points to a valid timer, false otherwise.


TIMER_SupportsDTI#

bool TIMER_SupportsDTI (const TIMER_TypeDef * ref)

Check whether the TIMER is valid and supports Dead Timer Insertion (DTI).

Parameters
TypeDirectionArgument NameDescription
const TIMER_TypeDef *[in]ref

Pointer to the TIMER peripheral register block.

Returns

  • True if ref points to a valid timer that supports DTI, false otherwise.


TIMER_MaxCount#

uint32_t TIMER_MaxCount (const TIMER_TypeDef * ref)

Get the Max count of the timer.

Parameters
TypeDirectionArgument NameDescription
const TIMER_TypeDef *[in]ref

Pointer to the TIMER peripheral register block.

Returns

  • The max count value of the timer. This is 0xFFFF for 16 bit timers and 0xFFFFFFFF for 32 bit timers.


TIMER_CaptureGet#

uint32_t TIMER_CaptureGet (TIMER_TypeDef * timer, unsigned int ch)

Get compare/capture value for the compare/capture channel.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

unsigned int[in]ch

Compare/capture channel to access.

Returns

  • Current capture value.


TIMER_CaptureBufGet#

uint32_t TIMER_CaptureBufGet (TIMER_TypeDef * timer, unsigned int ch)

Get the buffered compare/capture value for compare/capture channel.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

unsigned int[in]ch

Compare/capture channel to access.

Returns

  • Current buffered capture value.


TIMER_CompareBufSet#

void TIMER_CompareBufSet (TIMER_TypeDef * timer, unsigned int ch, uint32_t val)

Set the compare value buffer for the compare/capture channel when operating in compare or PWM mode.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

unsigned int[in]ch

Compare/capture channel to access.

uint32_t[in]val

Value to set in compare value buffer register.

The compare value buffer holds the value which will be written to TIMERn_CCx_CCV on an update event if the buffer has been updated since the last event.


TIMER_CompareSet#

void TIMER_CompareSet (TIMER_TypeDef * timer, unsigned int ch, uint32_t val)

Set the compare value for compare/capture channel when operating in compare or PWM mode.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

unsigned int[in]ch

Compare/capture channel to access.

uint32_t[in]val

Value to set in compare value register.


TIMER_CounterGet#

uint32_t TIMER_CounterGet (TIMER_TypeDef * timer)

Get the TIMER counter value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to TIMER peripheral register block.

Returns

  • Current TIMER counter value.


TIMER_CounterSet#

void TIMER_CounterSet (TIMER_TypeDef * timer, uint32_t val)

Set the TIMER counter value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]val

Value to set counter to.


TIMER_Enable#

void TIMER_Enable (TIMER_TypeDef * timer, bool enable)

Start/stop TIMER.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

bool[in]enable

Set to true to enable counting; set to false otherwise.


TIMER_EnableDTI#

void TIMER_EnableDTI (TIMER_TypeDef * timer, bool enable)

Enable or disable DTI unit.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

bool[in]enable

Set to true to enable DTI unit; set to false otherwise.


TIMER_GetDTIFault#

uint32_t TIMER_GetDTIFault (TIMER_TypeDef * timer)

Get DTI fault source flags status.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Note

  • Event bits are not cleared by this function.

Returns

  • Status of the DTI fault source flags. Returns one or more valid DTI fault source flags (TIMER_DTFAULT_nnn) OR'ed together.


TIMER_ClearDTIFault#

void TIMER_ClearDTIFault (TIMER_TypeDef * timer, uint32_t flags)

Clear DTI fault source flags.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

DTI fault source(s) to clear. Use one or more valid DTI fault source flags (TIMER_DTFAULT_nnn) OR'ed together.


TIMER_IntClear#

void TIMER_IntClear (TIMER_TypeDef * timer, uint32_t flags)

Clear one or more pending TIMER interrupts.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

Pending TIMER interrupt source(s) to clear. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.


TIMER_IntDisable#

void TIMER_IntDisable (TIMER_TypeDef * timer, uint32_t flags)

Disable one or more TIMER interrupts.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

TIMER interrupt source(s) to disable. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.


TIMER_IntEnable#

void TIMER_IntEnable (TIMER_TypeDef * timer, uint32_t flags)

Enable one or more TIMER interrupts.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

TIMER interrupt source(s) to enable. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using TIMER_IntClear() prior to enabling the interrupt.


TIMER_IntGet#

uint32_t TIMER_IntGet (TIMER_TypeDef * timer)

Get pending TIMER interrupt flags.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Note

  • Event bits are not cleared by this function.

Returns

  • TIMER interrupt source(s) pending. Returns one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.


TIMER_IntGetEnabled#

uint32_t TIMER_IntGetEnabled (TIMER_TypeDef * timer)

Get enabled and pending TIMER interrupt flags.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by this function.

Returns

  • Pending and enabled TIMER interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in TIMERx_IEN_nnn register (TIMERx_IEN_nnn) and

    • the OR combination of valid interrupt flags of the TIMER module (TIMERx_IF_nnn).


TIMER_IntSet#

void TIMER_IntSet (TIMER_TypeDef * timer, uint32_t flags)

Set one or more pending TIMER interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

TIMER interrupt source(s) to set to pending. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.


TIMER_TopBufSet#

void TIMER_TopBufSet (TIMER_TypeDef * timer, uint32_t val)

Set the top value buffer for the timer.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]val

Value to set in top value buffer register.

When top value buffer register is updated, value is loaded into top value register at the next wrap around. This feature is useful in order to update top value safely when timer is running.


TIMER_TopGet#

uint32_t TIMER_TopGet (TIMER_TypeDef * timer)

Get the top value setting for the timer.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Returns

  • Current top value.


TIMER_TopSet#

void TIMER_TopSet (TIMER_TypeDef * timer, uint32_t val)

Set the top value for timer.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]val

Value to set in top value register.