You are viewing documentation for version:
SE Command structure to which all commands to the SE must adhere. 
Public Attribute Documentation#
command#
uint32_t SE_Command_t::command
SE Command. 
data_in#
SE_DataTransfer_t* SE_Command_t::data_in
Input data. 
data_out#
SE_DataTransfer_t* SE_Command_t::data_out
Output data. 
parameters#
uint32_t SE_Command_t::parameters[SE_MAX_PARAMETERS]
Parameters. 
num_parameters#
size_t SE_Command_t::num_parameters
Number of parameters.