SE mailbox command context.
This structure defines the common SE mailbox command context used for all SE Manager API functions that execute SE mailbox commands. The members of this context structure should be considered internal to the SE Manager and should not be read or written directly by the user application. For members that are relevant for the user, the user can access them via corresponding set and get API functions, e.g. sl_se_set_yield().
Public Attributes#
SE_Command_t
SE mailbox command struct.
bool
If true, yield the CPU core while waiting for the SE mailbox command to complete.