CLI Commands in RAM#
Support for CLI commands stored in and executed from RAM.
Modules#
Typedefs#
Definition of the CLI storage RAM handle.
Functions#
Clear the command lines stored in ram.
Print the contet of the command lines stored in ram.
Start defining new command lines that will be stored in ram.
Execute command lines stored in ram.
Get the number of command lines stored in ram.
Initialize the cli_storage_ram instance.
Typedef Documentation#
cli_storage_ram_handle_t#
typedef cli_storage_ram_t* cli_storage_ram_handle_t
Definition of the CLI storage RAM handle.
Function Documentation#
sl_cli_storage_ram_clear#
void sl_cli_storage_ram_clear (sl_cli_command_arg_t * arguments)
Clear the command lines stored in ram.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_cli_command_arg_t * | [in] | arguments | A pointer to the command arguments.  | 
This function can be used directly as a cli command handler.
sl_cli_storage_ram_list#
void sl_cli_storage_ram_list (sl_cli_command_arg_t * arguments)
Print the contet of the command lines stored in ram.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_cli_command_arg_t * | [in] | arguments | A pointer to the command arguments.  | 
This function can be used directly as a cli command handler.
sl_cli_storage_ram_define#
void sl_cli_storage_ram_define (sl_cli_command_arg_t * arguments)
Start defining new command lines that will be stored in ram.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_cli_command_arg_t * | [in] | arguments | A pointer to the command arguments.  | 
This function can be used directly as a cli command handler.
sl_cli_storage_ram_execute#
void sl_cli_storage_ram_execute (sl_cli_command_arg_t * arguments)
Execute command lines stored in ram.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_cli_command_arg_t * | [in] | arguments | A pointer to the command arguments.  | 
This function can be used directly as a cli command handler.
Note
The function has a different implementation in a bare-metal vs. kernel configurations. In a bare-metal configuration, this function will signal that stored commands shall be run by the sl_cli_storage_ram_tick function. One stored command is executed for each call to the sl_cli_storage_ram_tick function. In a kernel configuration, all stored commands will be executed before this function returns.
sl_cli_storage_ram_count#
size_t sl_cli_storage_ram_count (sl_cli_handle_t cli_handle)
Get the number of command lines stored in ram.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_cli_handle_t | [in] | cli_handle | Handle to the CLI where the cli_storage_ram component is connected.  | 
Returns
The number of command lines stored in ram.
sl_cli_storage_ram_init#
void sl_cli_storage_ram_init (cli_storage_ram_handle_t handle)
Initialize the cli_storage_ram instance.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| cli_storage_ram_handle_t | [in] | handle | A handle to the cli_storage_ram instance.  |