Public Attributes#

uint8_t

Public Attribute Documentation#

trim_off_1x#

uint8_t sl_hal_system_devinfo_adc_offset_t::trim_off_1x

Definition at line 99 of file platform/peripheral/inc/sl_hal_system_generic.h

trim_off_2x#

uint8_t sl_hal_system_devinfo_adc_offset_t::trim_off_2x

Definition at line 100 of file platform/peripheral/inc/sl_hal_system_generic.h

trim_off_4x#

uint8_t sl_hal_system_devinfo_adc_offset_t::trim_off_4x

Definition at line 101 of file platform/peripheral/inc/sl_hal_system_generic.h

dummy_byte#

uint8_t sl_hal_system_devinfo_adc_offset_t::dummy_byte

Definition at line 102 of file platform/peripheral/inc/sl_hal_system_generic.h