EMU_VmonHystInit_TypeDef Struct ReferenceEMLIB > EMU
VMON Hysteresis initialization structure
Definition at line 687
of file em_emu.h
.
#include <
em_emu.h
>
Data Fields | |
EMU_VmonChannel_TypeDef | channel |
bool | enable |
int | fallThreshold |
bool | fallWakeup |
int | riseThreshold |
bool | riseWakeup |
Field Documentation
EMU_VmonChannel_TypeDef EMU_VmonHystInit_TypeDef::channel |
VMON channel to configure
Definition at line 688
of file em_emu.h
.
Referenced by EMU_VmonHystInit().
bool EMU_VmonHystInit_TypeDef::enable |
int EMU_VmonHystInit_TypeDef::fallThreshold |
bool EMU_VmonHystInit_TypeDef::fallWakeup |
Wake up from EM4H on falling edge
Definition at line 692
of file em_emu.h
.
Referenced by EMU_VmonHystInit().
int EMU_VmonHystInit_TypeDef::riseThreshold |
bool EMU_VmonHystInit_TypeDef::riseWakeup |
Wake up from EM4H on rising edge
Definition at line 691
of file em_emu.h
.
Referenced by EMU_VmonHystInit().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_emu.h