LDMA_CH_TypeDef Struct ReferenceDevicesDevices > | LDMA
LDMA_CH LDMA CH Register
.
Definition at line 47
of file efr32fg1p_ldma_ch.h
.
#include <
efr32fg1p_ldma_ch.h
>
Data Fields | |
__IOM uint32_t | CFG |
__IOM uint32_t | CTRL |
__IOM uint32_t | DST |
__IOM uint32_t | LINK |
__IOM uint32_t | LOOP |
__IOM uint32_t | REQSEL |
uint32_t | RESERVED0 [5] |
__IOM uint32_t | SRC |
Field Documentation
__IOM uint32_t LDMA_CH_TypeDef::CFG |
Channel Configuration Register
Definition at line 49
of file efr32fg1p_ldma_ch.h
.
__IOM uint32_t LDMA_CH_TypeDef::CTRL |
Channel Descriptor Control Word Register
Definition at line 51
of file efr32fg1p_ldma_ch.h
.
__IOM uint32_t LDMA_CH_TypeDef::DST |
Channel Descriptor Destination Data Address Register
Definition at line 53
of file efr32fg1p_ldma_ch.h
.
__IOM uint32_t LDMA_CH_TypeDef::LINK |
Channel Descriptor Link Structure Address Register
Definition at line 54
of file efr32fg1p_ldma_ch.h
.
__IOM uint32_t LDMA_CH_TypeDef::LOOP |
Channel Loop Counter Register
Definition at line 50
of file efr32fg1p_ldma_ch.h
.
__IOM uint32_t LDMA_CH_TypeDef::REQSEL |
Channel Peripheral Request Select Register
Definition at line 48
of file efr32fg1p_ldma_ch.h
.
uint32_t LDMA_CH_TypeDef::RESERVED0[5] |
Reserved future
Definition at line 55
of file efr32fg1p_ldma_ch.h
.
__IOM uint32_t LDMA_CH_TypeDef::SRC |
Channel Descriptor Source Data Address Register
Definition at line 52
of file efr32fg1p_ldma_ch.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32FG1P/Include/
efr32fg1p_ldma_ch.h