touch.c File Reference
EFM32GG_DK3750, Touch panel driver.
- Version
- 5.4.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
touch.c
.
#include <stdlib.h>
#include <string.h>
#include "
em_device.h
"
#include "
em_adc.h
"
#include "
em_gpio.h
"
#include "
em_cmu.h
"
#include "
touch.h
"
#include "calibrate.h"
#include "
bsp.h
"
#include "
i2cspm.h
"
#include "
eeprom.h
"
Macros |
|
#define | ADC_X adcSingleInpCh1 |
#define | ADC_Y adcSingleInpCh4 |
#define | TOUCH_X1_PIN 5 |
#define | TOUCH_X1_PORT gpioPortD |
#define | TOUCH_X2_PIN 4 |
#define | TOUCH_X2_PORT gpioPortD |
#define | TOUCH_Y1_PIN 3 |
#define | TOUCH_Y1_PORT gpioPortD |
#define | TOUCH_Y2_PIN 1 |
#define | TOUCH_Y2_PORT gpioPortD |
Enumerations |
|
enum |
TOUCH_State_TypeDef
{
TOUCH_INIT , TOUCH_CHECK_PRESS , TOUCH_MEASURE_X , TOUCH_MEASURE_Y } |
Functions |
|
void | ADC0_IRQHandler (void) |
Interrupt handler is executed with frequency ~28Hz when panel is not pressed and with frequency ~140Hz when panel is pressed - this will give ~50 readings per second.
|
|
int | TOUCH_CalibrationTable (POINT *displayPtr, POINT *screenPtr) |
Set calibration table.
|
|
void | TOUCH_CallUpcall (void) |
Function that calls registered upcall.
|
|
TOUCH_Pos_TypeDef * | TOUCH_GetPos (void) |
Returns current touch position and state.
|
|
void | TOUCH_Init ( TOUCH_Config_TypeDef *config) |
Initialize touch panel driver.
|
|
int | TOUCH_IsBusy (void) |
Check status of the touch panel.
|
|
void | TOUCH_RecalculatePosition (volatile TOUCH_Pos_TypeDef *pos) |
Convert ADC readings into XY position.
|
|
void | TOUCH_RegisterUpcall ( TOUCH_Upcall_TypeDef *new_upcall) |
Register upcall which will be call every position or state change.
|
|
int | TOUCH_StateChanged (void) |
Check if cursor state changed (down or move)
|
|
Variables |
|
MATRIX | calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } |
Macro Definition Documentation
#define ADC_X adcSingleInpCh1 |
#define ADC_Y adcSingleInpCh4 |
Input channel 4
Definition at line
37
of file
touch.c
.
Referenced by ADC0_IRQHandler() , and TOUCH_Init() .
#define TOUCH_X1_PIN 5 |
#define TOUCH_X1_PORT gpioPortD |
#define TOUCH_X2_PIN 4 |
Pin 4
Definition at line
43
of file
touch.c
.
Referenced by ADC0_IRQHandler() , and TOUCH_IsBusy() .
#define TOUCH_X2_PORT gpioPortD |
Port D
Definition at line
42
of file
touch.c
.
Referenced by ADC0_IRQHandler() , and TOUCH_IsBusy() .
#define TOUCH_Y1_PIN 3 |
#define TOUCH_Y1_PORT gpioPortD |
#define TOUCH_Y2_PIN 1 |
#define TOUCH_Y2_PORT gpioPortD |
Enumeration Type Documentation
enum TOUCH_State_TypeDef |
touch driver states
Definition at line
50
of file
touch.c
.
Function Documentation
void TOUCH_RecalculatePosition | ( | volatile TOUCH_Pos_TypeDef * |
pos
|
) |
Convert ADC readings into XY position.
- Parameters
-
[in] pos
Pointer to position structure
Definition at line
158
of file
touch.c
.
References TOUCH_Pos_TypeDef::adcx , TOUCH_Pos_TypeDef::adcy , calibrationMatrix , TOUCH_Pos_TypeDef::pen , TOUCH_Pos_TypeDef::x , and TOUCH_Pos_TypeDef::y .
Referenced by ADC0_IRQHandler() .
int TOUCH_StateChanged | ( | void |
|
) |
Check if cursor state changed (down or move)
- Returns
- 1 if the cursor state has changed
Definition at line
201
of file
touch.c
.
References TOUCH_Pos_TypeDef::pen , TOUCH_Pos_TypeDef::x , and TOUCH_Pos_TypeDef::y .
Referenced by ADC0_IRQHandler() .
Variable Documentation
MATRIX calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } |
Calibration table
Definition at line
70
of file
touch.c
.
Referenced by TOUCH_CalibrationTable() , and TOUCH_RecalculatePosition() .