Deprecated List

globalScope> Global _SILICON_LABS_32B_PLATFORM
Silicon Labs platform name
globalScope> Global _SILICON_LABS_32B_PLATFORM_1
Silicon Labs platform name
globalScope> Global BSP_TraceSwoSetup (void)
Deprecated function. New code should call BSP_TraceProfilerSetup().
globalScope> Global EMU_MemPwrDown (uint32_t blocks)
This function is deprecated, use EMU_RamPowerDown() instead which maps a user provided memory range into RAM blocks to power down.
globalScope> Global EMU_UpdateOscConfig (void)
Oscillator status is saved in EMU_EnterEM2() and EMU_EnterEM3().
globalScope> Global GPIO_IntConfig (GPIO_Port_TypeDef port, unsigned int pin, bool risingEdge, bool fallingEdge, bool enable)
Deprecated function. New code should use GPIO_ExtIntConfig().
Module INT
These functions are deprecated and marked for removal in a later release. Use the CORE module instead. See Porting from em_int for information on how to convert existing code bases to use CORE.
globalScope> Global INT_Disable (void)
Deprecated and marked for removal in a later release. Use new CORE module instead.
globalScope> Global INT_Enable (void)
Deprecated and marked for removal in a later release. Use the new CORE module instead.
Module NVM
This driver is deprecated and marked for removal in a later release. New code should use NVM3.
globalScope> Global setupSWOForPrint
Use RETARGET_SwoInit instead
globalScope> Global SLEEP_Init (SLEEP_CbFuncPtr_t pSleepCb, SLEEP_CbFuncPtr_t pWakeUpCb)
New code should use the SLEEP_InitEx function for initializing the sleep module.
globalScope> Global UARTDRV_Init (UARTDRV_Handle_t handle, UARTDRV_InitUart_t *initData)
Deprecated; Use UARTDRV_InitUart() instead.
globalScope> Global USART_InitIrDA (const USART_InitIrDA_TypeDef *init)
Deprecated function. New code should use USARTn_InitIrDA(). This function uses DEFAULT_IRDA_USART, which unless otherwise specified, is USART0 on most devices, and USART1 on devices that don't have a USART0.
globalScope> Global WDOG_Enable (bool enable)
Deprecated function. New code should use WDOGn_Enable(). This function uses DEFAULT_WDOG.
globalScope> Global WDOG_Feed (void)
Deprecated function. New code should use WDOGn_Feed(). This function uses DEFAULT_WDOG.
globalScope> Global WDOG_Init (const WDOG_Init_TypeDef *init)
Deprecated function. New code should use WDOGn_Init(). This function uses DEFAULT_WDOG.
globalScope> Global WDOG_Lock (void)
Deprecated function. New code should use WDOGn_Lock(). This function uses DEFAULT_WDOG.