WDOG_TypeDef Struct ReferenceDevices > EFM32WG_WDOG

Definition at line 48 of file efm32wg_wdog.h.

Data Fields

__IOM uint32_t CMD
 
__IOM uint32_t CTRL
 
__IM uint32_t SYNCBUSY
 

Field Documentation

__IOM uint32_t WDOG_TypeDef::CMD

Command Register

Definition at line 50 of file efm32wg_wdog.h.

Referenced by WDOGn_Feed().

__IOM uint32_t WDOG_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32wg_wdog.h.

Referenced by WDOGn_Enable(), WDOGn_Feed(), WDOGn_Init(), and WDOGn_Lock().

__IM uint32_t WDOG_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 52 of file efm32wg_wdog.h.

Referenced by WDOGn_Enable(), WDOGn_Feed(), WDOGn_Init(), and WDOGn_Lock().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/efm32wg_wdog.h