UARTDRV_Buffer_FifoQueue_t Struct ReferenceEMDRV > UARTDRV
Transfer operation FIFO queue typedef.
Definition at line 138
of file uartdrv.h
.
#include <
uartdrv.h
>
Data Fields | |
UARTDRV_Buffer_t | fifo [] |
FIFO of queued data. | |
volatile uint16_t | head |
An index of the next byte to send. | |
const uint16_t | size |
FIFO size. | |
volatile uint16_t | tail |
An index of the location to enqueue the next message. | |
volatile uint16_t | used |
A number of bytes queued. | |
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emdrv/uartdrv/inc/
uartdrv.h