USBD_Callbacks_TypeDef Struct ReferencePlatform Middleware > USB > USB_DEVICE

USB Device stack callback structure.

Callback functions used by the device stack to signal events or query status to/from the application. See USBD_Init_TypeDef. Assign members to NULL if your application don't need a specific callback.

Definition at line 783 of file em_usb.h.

#include <em_usb.h>

Data Fields

const USBD_IsSelfPoweredCb_TypeDef isSelfPowered
 
const USBD_SetupCmdCb_TypeDef setupCmd
 
const USBD_SofIntCb_TypeDef sofInt
 
const USBD_UsbResetCb_TypeDef usbReset
 
const USBD_DeviceStateChangeCb_TypeDef usbStateChange
 

Field Documentation

const USBD_IsSelfPoweredCb_TypeDef USBD_Callbacks_TypeDef::isSelfPowered

Called whenever the device stack needs to query if the device is currently self- or bus-powered. Applies to devices which can operate in both modes.

Definition at line 788 of file em_usb.h.

const USBD_SetupCmdCb_TypeDef USBD_Callbacks_TypeDef::setupCmd

Called on each setup request received from host.

Definition at line 787 of file em_usb.h.

const USBD_SofIntCb_TypeDef USBD_Callbacks_TypeDef::sofInt

Called at each SOF interrupt. If NULL, the device stack will not enable the SOF interrupt.

Definition at line 791 of file em_usb.h.

const USBD_UsbResetCb_TypeDef USBD_Callbacks_TypeDef::usbReset

Called whenever USB reset signalling is detected on the USB port.

Definition at line 784 of file em_usb.h.

Referenced by USBX_init().

const USBD_DeviceStateChangeCb_TypeDef USBD_Callbacks_TypeDef::usbStateChange

Called whenever the device change state.

Definition at line 786 of file em_usb.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/em_usb.h