USBH_Init_TypeDef Struct ReferencePlatform Middleware > USB > USB_HOST
USB Host stack initialization structure.
This structure is passed to USBH_Init() when starting up the device. Max accumulated FIFO size is 2K bytes.
Definition at line 879
of file em_usb.h
.
#include <
em_usb.h
>
Data Fields | |
uint32_t | nptxFifoSize |
uint32_t | ptxFifoSize |
uint32_t | reserved |
uint32_t | rxFifoSize |
Field Documentation
uint32_t USBH_Init_TypeDef::nptxFifoSize |
Number of FIFO bytes set aside for OUT CTRL/BULK endoints.
Definition at line 881
of file em_usb.h
.
Referenced by USBH_Init().
uint32_t USBH_Init_TypeDef::ptxFifoSize |
Number of FIFO bytes set aside for OUT INTR/ISO endoints.
Definition at line 882
of file em_usb.h
.
Referenced by USBH_Init().
uint32_t USBH_Init_TypeDef::reserved |
Reserved for future use.
Definition at line 883
of file em_usb.h
.
uint32_t USBH_Init_TypeDef::rxFifoSize |
Number of FIFO bytes set aside for IN endpoints.
Definition at line 880
of file em_usb.h
.
Referenced by USBH_Init().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/
em_usb.h