operand_t Struct Reference
The fx20_divide and fx20_multiply uses this structure to pass values into it.
       Definition at line
       
        1020
       
       of file
       
        si114x_functions.c
       
       .
      
| Data Fields | |
| uint32_t | op1 | 
| uint32_t | op2 | 
Field Documentation
| uint32_t operand_t::op1 | 
| uint32_t operand_t::op2 | 
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/hardware/kit/common/drivers/
       si114x_functions.c